<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046A 1000Base-KX Mode with Linux Mainline in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-1000Base-KX-Mode-with-Linux-Mainline/m-p/2113822#M15825</link>
    <description>Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180431"&gt;@timsalabim&lt;/a&gt;,&lt;BR /&gt;Unfortunately it is not possible to use it with that release, please use an older release, such the 6.1.55&lt;BR /&gt;</description>
    <pubDate>Tue, 10 Jun 2025 18:51:19 GMT</pubDate>
    <dc:creator>LFGP</dc:creator>
    <dc:date>2025-06-10T18:51:19Z</dc:date>
    <item>
      <title>LS1046A 1000Base-KX Mode with Linux Mainline</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-1000Base-KX-Mode-with-Linux-Mainline/m-p/2113644#M15823</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;one of our customers want to use 1000Base-KX with the LS1046A CPU.&amp;nbsp; When researching I found the following comment in the 6.12.33 Linux Mainline kernel in&amp;nbsp; &amp;nbsp; /tree/drivers/net/ethernet/freescale/fman/fman_memac.c&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class=""&gt;/* TODO: The following interface modes are supported by (some) hardware&lt;/SPAN&gt;
&lt;SPAN class=""&gt;	 * but not by this driver:&lt;/SPAN&gt;
&lt;SPAN class=""&gt;	 * - 1000BASE-KX&lt;/SPAN&gt;
&lt;SPAN class=""&gt;	 * - 10GBASE-KR&lt;/SPAN&gt;
&lt;SPAN class=""&gt;	 * - XAUI/HiGig&lt;/SPAN&gt;
&lt;SPAN class=""&gt;	 */&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&lt;BR /&gt;This comment is missing in the QoriQ Linux kernel repository so I'm wondering if it will be possible to use Linux Mainline kernel with 1000Base-KX.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jun 2025 13:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-1000Base-KX-Mode-with-Linux-Mainline/m-p/2113644#M15823</guid>
      <dc:creator>timsalabim</dc:creator>
      <dc:date>2025-06-10T13:28:51Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A 1000Base-KX Mode with Linux Mainline</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-1000Base-KX-Mode-with-Linux-Mainline/m-p/2113822#M15825</link>
      <description>Dear &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180431"&gt;@timsalabim&lt;/a&gt;,&lt;BR /&gt;Unfortunately it is not possible to use it with that release, please use an older release, such the 6.1.55&lt;BR /&gt;</description>
      <pubDate>Tue, 10 Jun 2025 18:51:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-1000Base-KX-Mode-with-Linux-Mainline/m-p/2113822#M15825</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2025-06-10T18:51:19Z</dc:date>
    </item>
  </channel>
</rss>