<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046ARDB Unable to boot from SD card in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2099281#M15758</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/104291"&gt;@pholden&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;I've seen the same error when I was playing with LS1046AFRWY.&lt;BR /&gt;Look at this line:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;[ 3.092365] Please append a correct "root=" boot option; here are the available partitions:&lt;/LI-CODE&gt;&lt;P&gt;It seems that you didn't specify the `root=` option in u-boot env variable `bootargs`.&lt;BR /&gt;In my case it was&lt;/P&gt;&lt;LI-CODE lang="c"&gt;bootargs "root=/dev/ram0 rw console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 ramdisk_size=0x10000000"&lt;/LI-CODE&gt;&lt;P&gt;but then I forgot to upload the ramdisk via TFTP, and run "boot" command.&lt;BR /&gt;&lt;BR /&gt;The same kernel panic is possible when you point wrong partition number of mmc in "root=" option.&lt;/P&gt;</description>
    <pubDate>Sat, 17 May 2025 14:17:38 GMT</pubDate>
    <dc:creator>valokuvaaja</dc:creator>
    <dc:date>2025-05-17T14:17:38Z</dc:date>
    <item>
      <title>LS1046ARDB Unable to boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2094841#M15718</link>
      <description>&lt;P&gt;I am unable to boot from SD card.&amp;nbsp; I have tried to use the "flex-installer -i auto -m ls1046ardb -d /dev/sdc" and have tried "flex-installer -b boot_LS_arm64_lts_5.10.tgz -r rootfs_lsdk2108_ubuntu_main_arm64.tgz -f firmware_ls1046ardb_sdboot.img -d /dev/sdc" from my build/images directory.&amp;nbsp; They both end in a kernel panic (below).&amp;nbsp; Any suggestions?&lt;/P&gt;&lt;P&gt;debug port output:&lt;/P&gt;&lt;P&gt;[ 2.999330] Waiting for root device PARTUUID=79e0ff00-04...&lt;BR /&gt;[ 3.055507] mmc0: new ultra high speed SDR104 SDHC card at address aaaa&lt;BR /&gt;[ 3.062435] mmcblk0: mmc0:aaaa SD32G 29.7 GiB (ro)&lt;BR /&gt;[ 3.068327] mmcblk0: p1 p2 p3 p4&lt;BR /&gt;[ 3.083392] VFS: Cannot open root device "PARTUUID=79e0ff00-04" or unknown-block(179,4): error -30&lt;BR /&gt;[ 3.092365] Please append a correct "root=" boot option; here are the available partitions:&lt;BR /&gt;[ 3.100725] 0100 4096 ram0&lt;BR /&gt;[ 3.100727] (driver?)&lt;BR /&gt;[ 3.106826] 0101 4096 ram1&lt;BR /&gt;[ 3.106828] (driver?)&lt;BR /&gt;[ 3.112931] 0102 4096 ram2&lt;BR /&gt;[ 3.112933] (driver?)&lt;BR /&gt;[ 3.119032] 0103 4096 ram3&lt;BR /&gt;[ 3.119034] (driver?)&lt;BR /&gt;[ 3.125136] 0104 4096 ram4&lt;BR /&gt;[ 3.125138] (driver?)&lt;BR /&gt;[ 3.131236] 0105 4096 ram5&lt;BR /&gt;[ 3.131238] (driver?)&lt;BR /&gt;[ 3.137341] 0106 4096 ram6&lt;BR /&gt;[ 3.137343] (driver?)&lt;BR /&gt;[ 3.143446] 0107 4096 ram7&lt;BR /&gt;[ 3.143447] (driver?)&lt;BR /&gt;[ 3.149546] 0108 4096 ram8&lt;BR /&gt;[ 3.149548] (driver?)&lt;BR /&gt;[ 3.155650] 0109 4096 ram9&lt;BR /&gt;[ 3.155652] (driver?)&lt;BR /&gt;[ 3.161750] 010a 4096 ram10&lt;BR /&gt;[ 3.161751] (driver?)&lt;BR /&gt;[ 3.167940] 010b 4096 ram11&lt;BR /&gt;[ 3.167942] (driver?)&lt;BR /&gt;[ 3.174128] 010c 4096 ram12&lt;BR /&gt;[ 3.174130] (driver?)&lt;BR /&gt;[ 3.180318] 010d 4096 ram13&lt;BR /&gt;[ 3.180319] (driver?)&lt;BR /&gt;[ 3.186505] 010e 4096 ram14&lt;BR /&gt;[ 3.186506] (driver?)&lt;BR /&gt;[ 3.192695] 010f 4096 ram15&lt;BR /&gt;[ 3.192696] (driver?)&lt;BR /&gt;[ 3.198887] 1f00 524288 mtdblock0&lt;BR /&gt;[ 3.198889] (driver?)&lt;BR /&gt;[ 3.205432] 1f01 65536 mtdblock1&lt;BR /&gt;[ 3.205434] (driver?)&lt;BR /&gt;[ 3.211974] 1f02 65536 mtdblock2&lt;BR /&gt;[ 3.211976] (driver?)&lt;BR /&gt;[ 3.218509] b300 31166976 mmcblk0&lt;BR /&gt;[ 3.218511] driver: mmcblk&lt;BR /&gt;[ 3.225307] b301 131072 mmcblk0p1 79e0ff00-01&lt;BR /&gt;[ 3.225309]&lt;BR /&gt;[ 3.232106] b302 2097152 mmcblk0p2 79e0ff00-02&lt;BR /&gt;[ 3.232108]&lt;BR /&gt;[ 3.238901] b303 5242880 mmcblk0p3 79e0ff00-03&lt;BR /&gt;[ 3.238903]&lt;BR /&gt;[ 3.245697] b304 23623168 mmcblk0p4 79e0ff00-04&lt;BR /&gt;[ 3.245698]&lt;BR /&gt;[ 3.252498] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,4)&lt;BR /&gt;[ 3.260938] CPU: 3 PID: 1 Comm: swapper/0 Not tainted 5.10.35-dirty #15&lt;BR /&gt;[ 3.267550] Hardware name: LS1046A RDB Board (DT)&lt;BR /&gt;[ 3.272248] Call trace:&lt;BR /&gt;[ 3.274696] dump_backtrace+0x0/0x1a8&lt;BR /&gt;[ 3.278353] show_stack+0x18/0x68&lt;BR /&gt;[ 3.281663] dump_stack+0xc8/0x120&lt;BR /&gt;[ 3.285059] panic+0x16c/0x334&lt;BR /&gt;[ 3.288109] mount_block_root+0x1c0/0x250&lt;BR /&gt;[ 3.292112] mount_root+0x10c/0x144&lt;BR /&gt;[ 3.295595] prepare_namespace+0x130/0x170&lt;BR /&gt;[ 3.299687] kernel_init_freeable+0x210/0x23c&lt;BR /&gt;[ 3.304040] kernel_init+0x14/0x114&lt;BR /&gt;[ 3.307523] ret_from_fork+0x10/0x34&lt;BR /&gt;[ 3.311096] SMP: stopping secondary CPUs&lt;BR /&gt;[ 3.315023] Kernel Offset: 0x520644c00000 from 0xffff800010000000&lt;BR /&gt;[ 3.321113] PHYS_OFFSET: 0xffffdee980000000&lt;BR /&gt;[ 3.325291] CPU features: 0x0040022,21806000&lt;BR /&gt;[ 3.329555] Memory Limit: none&lt;BR /&gt;[ 3.332608] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,4) ]---&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 20:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2094841#M15718</guid>
      <dc:creator>pholden</dc:creator>
      <dc:date>2025-05-09T20:51:34Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB Unable to boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2097493#M15745</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Are you able to boot from the emmc nor flash?&amp;nbsp;If the board is configured with the default switch settings and power is supplied to the board, then the boot loader (U-Boot) image&lt;BR /&gt;located in QSPI NOR flash virtual bank 0 runs.&lt;/P&gt;
&lt;P&gt;After confirming it boots please review again your switch configuration and try again using the pre-build images.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LS1046ARDBGSG" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=LS1046ARDBGSG&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Wed, 14 May 2025 18:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2097493#M15745</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-05-14T18:41:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB Unable to boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2097561#M15746</link>
      <description>&lt;P&gt;Of course it booted with the default settings.&amp;nbsp; I then switched the boot config switches to allow for sd-boot (as defined in the LS1046ARDB user guide), and this is what I got with both my slightly modified image AND the pre-built image.&lt;/P&gt;</description>
      <pubDate>Wed, 14 May 2025 21:38:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2097561#M15746</guid>
      <dc:creator>pholden</dc:creator>
      <dc:date>2025-05-14T21:38:46Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB Unable to boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2099281#M15758</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/104291"&gt;@pholden&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;I've seen the same error when I was playing with LS1046AFRWY.&lt;BR /&gt;Look at this line:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;[ 3.092365] Please append a correct "root=" boot option; here are the available partitions:&lt;/LI-CODE&gt;&lt;P&gt;It seems that you didn't specify the `root=` option in u-boot env variable `bootargs`.&lt;BR /&gt;In my case it was&lt;/P&gt;&lt;LI-CODE lang="c"&gt;bootargs "root=/dev/ram0 rw console=ttyS0,115200 earlycon=uart8250,mmio,0x21c0500 ramdisk_size=0x10000000"&lt;/LI-CODE&gt;&lt;P&gt;but then I forgot to upload the ramdisk via TFTP, and run "boot" command.&lt;BR /&gt;&lt;BR /&gt;The same kernel panic is possible when you point wrong partition number of mmc in "root=" option.&lt;/P&gt;</description>
      <pubDate>Sat, 17 May 2025 14:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2099281#M15758</guid>
      <dc:creator>valokuvaaja</dc:creator>
      <dc:date>2025-05-17T14:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB Unable to boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2100112#M15764</link>
      <description>&lt;P&gt;This is what my bootargs looks like:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;bootargs=console=ttyS0,115200 root=/dev/ram0 earlycon=uart8250,mmio,0x21c0500 mtdparts=1550000.spi-0:1m(rcw),15m(u-boot),48m(kernel.itb);7e800000.flash:16m(nand_uboot),48m(nand_kernel),448m(nand_free)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;What should it look like for sdcard?&amp;nbsp; Do I just change root to mmcblk0p1?&amp;nbsp; I'm not about the rest.&amp;nbsp; It doesn't look right either for SD card boot.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 May 2025 21:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2100112#M15764</guid>
      <dc:creator>pholden</dc:creator>
      <dc:date>2025-05-19T21:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB Unable to boot from SD card</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2104776#M15794</link>
      <description>&lt;P&gt;Did you download the flex-installer tool following the LSDK2108UG? , please try to flash only the firmware and test the image, also try with a diferent SD card and share screenshots of the process you followed.&lt;/P&gt;</description>
      <pubDate>Tue, 27 May 2025 04:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-Unable-to-boot-from-SD-card/m-p/2104776#M15794</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-05-27T04:05:01Z</dc:date>
    </item>
  </channel>
</rss>