<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDRC Timeout while waiting for DEBUG_2 on LS1046A in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/DDRC-Timeout-while-waiting-for-DEBUG-2-on-LS1046A/m-p/2093514#M15708</link>
    <description>&lt;P&gt;1. In target initialization File, in function "run_init_file", please comment line "Init_DDRC(DDR_freq)".&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. No this configuration.&lt;/P&gt;
&lt;P&gt;3. Please refer to the following document.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/DDR-Bringing-up-and-validation-with-QCVS-DDRv-Tool/ta-p/1167315?attachment-id=102669" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/DDR-Bringing-up-and-validation-with-QCVS-DDRv-Tool/ta-p/1167315?attachment-id=102669&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;4. It means there is problem with DDR controller initialization.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 08 May 2025 09:01:43 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2025-05-08T09:01:43Z</dc:date>
    <item>
      <title>DDRC Timeout while waiting for DEBUG_2 on LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/DDRC-Timeout-while-waiting-for-DEBUG-2-on-LS1046A/m-p/2091670#M15695</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using an LS1046A on a custom carrier board. We have these boards shipping and running in the field, however there are some lingering manufacturing issues I am looking into.&lt;/P&gt;&lt;P&gt;On a number of boards (more than we are willing to tolerate) we get some failures which were originally attributed to bad eMMC devices. However, upon looking deeper into the issue, I can now say that I believe these failures are due to something related to the DDR4 bus between the LS1046A and the DDR4 devices. The specific error message is:&lt;/P&gt;&lt;P&gt;DDRC: Timeout while waiting for DEBUG_2&lt;/P&gt;&lt;P&gt;On CCS the error message I get is:&lt;/P&gt;&lt;P&gt;Cortex-A72: Core not responding&lt;/P&gt;&lt;P&gt;This seems to be related to the erratum A009803 as found in the target initialization file.&lt;/P&gt;&lt;P&gt;In order to debug this, using a good board (GB) I confirmed that I am able to read/write to internal and external memory using the CCS tool. Then I made the following changes:&lt;/P&gt;&lt;P&gt;1. removed the eMMC device&lt;/P&gt;&lt;P&gt;2. removed one of the 4x DDR4 mem devices&lt;/P&gt;&lt;P&gt;After rework 1 above, I am still able to initialize the board and read/write to internal and external memory as expected via CCS tool.&lt;/P&gt;&lt;P&gt;After rework 2 above, I am now able to induce the same failure message as seen on the bad boards. And now, I get the "Core not responding message" and I am unable to talk to the device.&lt;/P&gt;&lt;P&gt;Questions I have / would like some help with:&lt;/P&gt;&lt;P&gt;1. Is there a way to bypass the DDRC init so that I can still talk to the LS1046A via JTAG to assess health status?&lt;/P&gt;&lt;P&gt;2. Is there a way to configure the DDRC to only talk to 3 out of 4 devices i.e. in essence ignore one or more DDR4 devices during init?&lt;/P&gt;&lt;P&gt;3. what are some status/error register I can look at to assess health of the LS1046A, DDRC, and DDR4 devices?&lt;/P&gt;&lt;P&gt;4. why does the Diagnose Connection inside the CW IDE check the marks the "Run target initialization script" step with a green checkmark, when it actually reports a Timeout? Is this the expected behaviour?&lt;/P&gt;&lt;P&gt;Any suggestions or ideas would be much appreciated.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Axel&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 05 May 2025 19:56:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDRC-Timeout-while-waiting-for-DEBUG-2-on-LS1046A/m-p/2091670#M15695</guid>
      <dc:creator>axegar</dc:creator>
      <dc:date>2025-05-05T19:56:16Z</dc:date>
    </item>
    <item>
      <title>Re: DDRC Timeout while waiting for DEBUG_2 on LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/DDRC-Timeout-while-waiting-for-DEBUG-2-on-LS1046A/m-p/2093514#M15708</link>
      <description>&lt;P&gt;1. In target initialization File, in function "run_init_file", please comment line "Init_DDRC(DDR_freq)".&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2. No this configuration.&lt;/P&gt;
&lt;P&gt;3. Please refer to the following document.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/DDR-Bringing-up-and-validation-with-QCVS-DDRv-Tool/ta-p/1167315?attachment-id=102669" target="_blank"&gt;https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/DDR-Bringing-up-and-validation-with-QCVS-DDRv-Tool/ta-p/1167315?attachment-id=102669&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;4. It means there is problem with DDR controller initialization.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 09:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDRC-Timeout-while-waiting-for-DEBUG-2-on-LS1046A/m-p/2093514#M15708</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-05-08T09:01:43Z</dc:date>
    </item>
    <item>
      <title>Re: DDRC Timeout while waiting for DEBUG_2 on LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/DDRC-Timeout-while-waiting-for-DEBUG-2-on-LS1046A/m-p/2101027#M15778</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Thanks for your help. You were absolutely right, it seems to have been a configuration issue only at the 1600MT/s DDR speed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In other word, during boot up when we have to use the default DDR configuration, we had some timing issue. I have now fixed this and things seem much more stable now.&lt;/P&gt;&lt;P&gt;Running through a number of files at the factory to truly validate the fix.&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;Axel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 May 2025 01:35:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/DDRC-Timeout-while-waiting-for-DEBUG-2-on-LS1046A/m-p/2101027#M15778</guid>
      <dc:creator>axegar</dc:creator>
      <dc:date>2025-05-21T01:35:44Z</dc:date>
    </item>
  </channel>
</rss>