<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Help me understand how MSI interrupts work on the LS1046A</title>
    <link>https://community.nxp.com/t5/Layerscape/Help-me-understand-how-MSI-interrupts-work-on-the-LS1046A/m-p/2087591#M15665</link>
    <description>&lt;P&gt;We have a custom board that uses the LS1046A connected to a Switchtek PM40036 PCIe switch to allow connecting 20 PCIe devices.&amp;nbsp; As we needed to use features that are only available in the version 6 kernel, we have upgraded to kernel 6.1.&lt;/P&gt;&lt;P&gt;This has exposed an issue that I am struggling to understand. We get an error during boot that does a stack_dump(), and after some searching, it was found this was caused by enabling legacy_interrupts. Since 5.13 (&lt;A href="https://lore.kernel.org/linux-pci/5b3f3544-b7a5-c338-d53a-c6d7ff3ac8e0@nvidia.com/T/" target="_blank"&gt;https://lore.kernel.org/linux-pci/5b3f3544-b7a5-c338-d53a-c6d7ff3ac8e0@nvidia.com/T/&lt;/A&gt;) the Arm64 architecture no longer supports this feature. In our case,&amp;nbsp; this error has the side effect of rendering inoperable the first PCIe port processed (the one that generated this error.)&lt;/P&gt;&lt;P&gt;While I understand what is happening, I don't under why it is this way. The documentation clearly shows the LS1046A supports MSI interrupts, but the Linux drivers don't seem to be using them.&lt;/P&gt;&lt;P&gt;Is there a patch I need to apply to the mainline Linux kernel to make this work?&lt;/P&gt;&lt;P&gt;When I look at /proc/interrupts, I see the following:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@localhost:~# cat /proc/interrupts
           CPU0       CPU1       CPU2       CPU3       
  9:          0          0          0          0     GICv2  25 Level     vgic
 11:     267302     353977     340076     422853     GICv2  30 Level     arch_timer
 12:          0          0          0          0     GICv2  27 Level     kvm guest vtimer
 14:          0          0          0          0     GICv2  98 Level     gpio-cascade
 15:          0          0          0          0     GICv2  99 Level     gpio-cascade
 16:          3          0          0          0     GICv2 100 Level     gpio-cascade
 17:          0          0          0          0     GICv2 166 Level     gpio-cascade
 18:      32023          0          0          0     GICv2  88 Level     2180000.i2c
 19:      31997          0          0          0     GICv2  89 Level     2190000.i2c
 20:      76999          0          0          0     GICv2  90 Level     21a0000.i2c
 21:        259          0          0          0     GICv2  91 Level     21b0000.i2c
 22:      28997          0          0          0     GICv2  75 Level     fsl-ifc
 23:          0          0          0          0     GICv2 138 Level     arm-pmu
 24:          0          0          0          0     GICv2 139 Level     arm-pmu
 25:          0          0          0          0     GICv2 127 Level     arm-pmu
 26:          0          0          0          0     GICv2 129 Level     arm-pmu
 27:      32960          0          0          0     GICv2  86 Level     ttyS0
 28:          5          0          0          0     GICv2 131 Level     1550000.spi
 29:          3          0          0          0  mpc8xxx-gpio  15 Edge      gt911
 30:    3915558          0          0          0     GICv2  96 Level     2100000.spi
 31:          0          0          0          0     GICv2 174 Level     arm-smmu global fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault
 32:          0          0          0          0     GICv2 175 Level     arm-smmu global fault
 33:          0          0          0          0     GICv2 185 Level     qDMA error
 34:          0          0          0          0     GICv2  71 Level     qDMA queue
 35:          0          0          0          0     GICv2  92 Level     xhci-hcd:usb1
 36:       1011          0          0          0     GICv2  93 Level     dwc3
 38:      41544          0          0          0     GICv2 142 Level     xhci-hcd:usb3, xhci-hcd:usb5, xhci-hcd:usb7, xhci-hcd:usb9, xhci-hcd:usb11, xhci-hcd:usb13, xhci-hcd:usb15, xhci-hcd:usb17, xhci-hcd:usb19, 5
IPI0:      3248       3790       3688       3986       Rescheduling interrupts
IPI1:     25151      98589      77808      55638       Function call interrupts
IPI2:         0          0          0          0       CPU stop interrupts
IPI3:         0          0          0          0       CPU stop (for crash dump) interrupts
IPI4:         0          0          0          0       Timer broadcast interrupts
IPI5:         0          0          0          0       IRQ work interrupts
IPI6:         0          0          0          0       CPU wake-up interrupts
Err:          0
root@localhost:~#&lt;/LI-CODE&gt;&lt;P&gt;All the xhci-hcd controllers are actually PCIe devices. I expect to see them indicated as PCI-MSI, not assigned to GICv2 142.&amp;nbsp; So I've reached the extent of my understanding of the problem. If the LS1046a supports MSI, why are these being configured as legacy interrupts?&lt;/P&gt;&lt;P&gt;Is there a special driver or a configuration that I need to include, that I am not?&lt;/P&gt;&lt;P&gt;How do I get the PCIe host controller to support MSI?&lt;/P&gt;&lt;P&gt;Any advice appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sat, 26 Apr 2025 12:43:17 GMT</pubDate>
    <dc:creator>AbelianMeme</dc:creator>
    <dc:date>2025-04-26T12:43:17Z</dc:date>
    <item>
      <title>Help me understand how MSI interrupts work on the LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Help-me-understand-how-MSI-interrupts-work-on-the-LS1046A/m-p/2087591#M15665</link>
      <description>&lt;P&gt;We have a custom board that uses the LS1046A connected to a Switchtek PM40036 PCIe switch to allow connecting 20 PCIe devices.&amp;nbsp; As we needed to use features that are only available in the version 6 kernel, we have upgraded to kernel 6.1.&lt;/P&gt;&lt;P&gt;This has exposed an issue that I am struggling to understand. We get an error during boot that does a stack_dump(), and after some searching, it was found this was caused by enabling legacy_interrupts. Since 5.13 (&lt;A href="https://lore.kernel.org/linux-pci/5b3f3544-b7a5-c338-d53a-c6d7ff3ac8e0@nvidia.com/T/" target="_blank"&gt;https://lore.kernel.org/linux-pci/5b3f3544-b7a5-c338-d53a-c6d7ff3ac8e0@nvidia.com/T/&lt;/A&gt;) the Arm64 architecture no longer supports this feature. In our case,&amp;nbsp; this error has the side effect of rendering inoperable the first PCIe port processed (the one that generated this error.)&lt;/P&gt;&lt;P&gt;While I understand what is happening, I don't under why it is this way. The documentation clearly shows the LS1046A supports MSI interrupts, but the Linux drivers don't seem to be using them.&lt;/P&gt;&lt;P&gt;Is there a patch I need to apply to the mainline Linux kernel to make this work?&lt;/P&gt;&lt;P&gt;When I look at /proc/interrupts, I see the following:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@localhost:~# cat /proc/interrupts
           CPU0       CPU1       CPU2       CPU3       
  9:          0          0          0          0     GICv2  25 Level     vgic
 11:     267302     353977     340076     422853     GICv2  30 Level     arch_timer
 12:          0          0          0          0     GICv2  27 Level     kvm guest vtimer
 14:          0          0          0          0     GICv2  98 Level     gpio-cascade
 15:          0          0          0          0     GICv2  99 Level     gpio-cascade
 16:          3          0          0          0     GICv2 100 Level     gpio-cascade
 17:          0          0          0          0     GICv2 166 Level     gpio-cascade
 18:      32023          0          0          0     GICv2  88 Level     2180000.i2c
 19:      31997          0          0          0     GICv2  89 Level     2190000.i2c
 20:      76999          0          0          0     GICv2  90 Level     21a0000.i2c
 21:        259          0          0          0     GICv2  91 Level     21b0000.i2c
 22:      28997          0          0          0     GICv2  75 Level     fsl-ifc
 23:          0          0          0          0     GICv2 138 Level     arm-pmu
 24:          0          0          0          0     GICv2 139 Level     arm-pmu
 25:          0          0          0          0     GICv2 127 Level     arm-pmu
 26:          0          0          0          0     GICv2 129 Level     arm-pmu
 27:      32960          0          0          0     GICv2  86 Level     ttyS0
 28:          5          0          0          0     GICv2 131 Level     1550000.spi
 29:          3          0          0          0  mpc8xxx-gpio  15 Edge      gt911
 30:    3915558          0          0          0     GICv2  96 Level     2100000.spi
 31:          0          0          0          0     GICv2 174 Level     arm-smmu global fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault, arm-smmu-context-fault
 32:          0          0          0          0     GICv2 175 Level     arm-smmu global fault
 33:          0          0          0          0     GICv2 185 Level     qDMA error
 34:          0          0          0          0     GICv2  71 Level     qDMA queue
 35:          0          0          0          0     GICv2  92 Level     xhci-hcd:usb1
 36:       1011          0          0          0     GICv2  93 Level     dwc3
 38:      41544          0          0          0     GICv2 142 Level     xhci-hcd:usb3, xhci-hcd:usb5, xhci-hcd:usb7, xhci-hcd:usb9, xhci-hcd:usb11, xhci-hcd:usb13, xhci-hcd:usb15, xhci-hcd:usb17, xhci-hcd:usb19, 5
IPI0:      3248       3790       3688       3986       Rescheduling interrupts
IPI1:     25151      98589      77808      55638       Function call interrupts
IPI2:         0          0          0          0       CPU stop interrupts
IPI3:         0          0          0          0       CPU stop (for crash dump) interrupts
IPI4:         0          0          0          0       Timer broadcast interrupts
IPI5:         0          0          0          0       IRQ work interrupts
IPI6:         0          0          0          0       CPU wake-up interrupts
Err:          0
root@localhost:~#&lt;/LI-CODE&gt;&lt;P&gt;All the xhci-hcd controllers are actually PCIe devices. I expect to see them indicated as PCI-MSI, not assigned to GICv2 142.&amp;nbsp; So I've reached the extent of my understanding of the problem. If the LS1046a supports MSI, why are these being configured as legacy interrupts?&lt;/P&gt;&lt;P&gt;Is there a special driver or a configuration that I need to include, that I am not?&lt;/P&gt;&lt;P&gt;How do I get the PCIe host controller to support MSI?&lt;/P&gt;&lt;P&gt;Any advice appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 26 Apr 2025 12:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Help-me-understand-how-MSI-interrupts-work-on-the-LS1046A/m-p/2087591#M15665</guid>
      <dc:creator>AbelianMeme</dc:creator>
      <dc:date>2025-04-26T12:43:17Z</dc:date>
    </item>
    <item>
      <title>Re: Help me understand how MSI interrupts work on the LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Help-me-understand-how-MSI-interrupts-work-on-the-LS1046A/m-p/2093242#M15706</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Suggest using the following kernel version instead of the mentioned mainline Linux kernel 6.1. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MSI works well in the lf-6.1.55-2.2.0, please refer to the attached logs for details.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://github.com/nxp-qoriq/linux/tree/lf-6.1.55-2.2.0" target="_blank"&gt;https://github.com/nxp-qoriq/linux/tree/lf-6.1.55-2.2.0&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 May 2025 02:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Help-me-understand-how-MSI-interrupts-work-on-the-LS1046A/m-p/2093242#M15706</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-05-08T02:53:29Z</dc:date>
    </item>
  </channel>
</rss>