<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SD Card not working on Custom board in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/SD-Card-not-working-on-Custom-board/m-p/2086323#M15661</link>
    <description>&lt;DIV class=""&gt;Hi,&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;PFA SD card schematics of our hardware. Pls have a look and provide feedback. our observations are as follows:&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;1. R352 and R1071 are mounted, R 1072 and Q24 are not mounted - SDHC1_CD_B signal is low when card is inserted.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;2. DAT0, DAT1, DAT2, DAT3 and CMD lines are pulled up with 10K resistors to P3V3 from Resistors R346, R347,R348, R351, R354 through jumper wires.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;3. All the data lines and CMD line is continuously high to 3.3V from the power-up of the board.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;4. There is clock available on CLK pin of SD card connector.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Issue: There should be some toggling waveform at DAT0 pin after the Power-on to show the transaction of data but this is not happening.&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Kindly help to resolve the issue at the earliest.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Thanks,&lt;/DIV&gt;&lt;DIV class=""&gt;Shruti&lt;/DIV&gt;</description>
    <pubDate>Thu, 24 Apr 2025 07:09:09 GMT</pubDate>
    <dc:creator>shrutishrivastava</dc:creator>
    <dc:date>2025-04-24T07:09:09Z</dc:date>
    <item>
      <title>SD Card not working on Custom board</title>
      <link>https://community.nxp.com/t5/Layerscape/SD-Card-not-working-on-Custom-board/m-p/2086323#M15661</link>
      <description>&lt;DIV class=""&gt;Hi,&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;PFA SD card schematics of our hardware. Pls have a look and provide feedback. our observations are as follows:&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;1. R352 and R1071 are mounted, R 1072 and Q24 are not mounted - SDHC1_CD_B signal is low when card is inserted.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;2. DAT0, DAT1, DAT2, DAT3 and CMD lines are pulled up with 10K resistors to P3V3 from Resistors R346, R347,R348, R351, R354 through jumper wires.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;3. All the data lines and CMD line is continuously high to 3.3V from the power-up of the board.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;4. There is clock available on CLK pin of SD card connector.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Issue: There should be some toggling waveform at DAT0 pin after the Power-on to show the transaction of data but this is not happening.&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Kindly help to resolve the issue at the earliest.&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;Thanks,&lt;/DIV&gt;&lt;DIV class=""&gt;Shruti&lt;/DIV&gt;</description>
      <pubDate>Thu, 24 Apr 2025 07:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/SD-Card-not-working-on-Custom-board/m-p/2086323#M15661</guid>
      <dc:creator>shrutishrivastava</dc:creator>
      <dc:date>2025-04-24T07:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: SD Card not working on Custom board</title>
      <link>https://community.nxp.com/t5/Layerscape/SD-Card-not-working-on-Custom-board/m-p/2089171#M15669</link>
      <description>&lt;P&gt;Discussing with the AE team.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 08:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/SD-Card-not-working-on-Custom-board/m-p/2089171#M15669</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-04-29T08:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: SD Card not working on Custom board</title>
      <link>https://community.nxp.com/t5/Layerscape/SD-Card-not-working-on-Custom-board/m-p/2091744#M15696</link>
      <description>&lt;DIV id="b0p1o74i0i2r1" class="fm-textarea iwps_edit_box -iwps_edit_box fm_object_74 -fm_object_74 v-has-width v-has-height fm-inactive"&gt;
&lt;DIV class="inner_border"&gt;
&lt;DIV class="text" tabindex="0"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;DIV id="b0p1o78i0i2r1" class="fm-textarea iwps_text_area -iwps_text_area fm_object_78 -fm_object_78 show-scrollbars -show-scrollbars v-has-width v-has-height fm-inactive"&gt;
&lt;DIV class="inner_border"&gt;
&lt;DIV class="text" tabindex="0"&gt;Last time we discussed there were pull ups inside the voltage translator and on board translators were to be removed and voltage levels to be measured at both ends.&lt;/DIV&gt;
&lt;DIV class="text" tabindex="0"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV class="text" tabindex="0"&gt;&lt;SPAN&gt;Please note that this issue on LX2160A &lt;/SPAN&gt;&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Tue, 06 May 2025 01:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/SD-Card-not-working-on-Custom-board/m-p/2091744#M15696</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-05-06T01:16:55Z</dc:date>
    </item>
  </channel>
</rss>