<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1043A Custom Board codewarrior JTAG Diagnose Error</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-Custom-Board-codewarrior-JTAG-Diagnose-Error/m-p/2074787#M15579</link>
    <description>&lt;P&gt;Hi~Expert!&lt;/P&gt;&lt;P&gt;We are developing a custom board using the LS1043A processor.&lt;BR /&gt;Referring to LS1043ARDB, we replaced CPLD with FPGA and controlled PORESET_B to confirm that HRESET_B is normally ASSERTed and then DE-ASSERTed. At this time, RCW_SRC[0:8] was set to 0x9F. (Only DIFF_SYSCLK 100MHz is used.)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The next step is to connect to the device using CodeWarrior. However, when we click Diagnose Connection to check, an error occurs as shown below at the "&lt;STRONG&gt;Run target Initialization script&lt;/STRONG&gt;" stage and we cannot proceed any further.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jmsong_0-1744001569451.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/331534i1EA7D24E264819CC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jmsong_0-1744001569451.png" alt="jmsong_0-1744001569451.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;At this time, the Scan IDCODE is as follows.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;* Device 0&amp;nbsp; IDCODE: 5BA00477 Device: ARM DAP rev 5.x&lt;/P&gt;&lt;P&gt;* Device 1&amp;nbsp; IDCODE: 06B1201D&amp;nbsp; &amp;nbsp;Device: Unmapped NXP Device&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the initialization script file, USE_SAFE_RCW = True and BOOT_CHIP_SELECT = 2 are set.&lt;/P&gt;&lt;P&gt;and TA.rcw.set_source(0x9F)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I don't know if an error occurs when entering the internal register writing stage for DDR4 settings. (It's the same even if I change the address)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;def Init_DDRC_PD():&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080110, 0x450C0000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080000, 0x0000007F)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080008, 0x00000000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080010, 0x00000000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; .....&lt;/P&gt;</description>
    <pubDate>Mon, 07 Apr 2025 04:58:20 GMT</pubDate>
    <dc:creator>jmsong</dc:creator>
    <dc:date>2025-04-07T04:58:20Z</dc:date>
    <item>
      <title>LS1043A Custom Board codewarrior JTAG Diagnose Error</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Custom-Board-codewarrior-JTAG-Diagnose-Error/m-p/2074787#M15579</link>
      <description>&lt;P&gt;Hi~Expert!&lt;/P&gt;&lt;P&gt;We are developing a custom board using the LS1043A processor.&lt;BR /&gt;Referring to LS1043ARDB, we replaced CPLD with FPGA and controlled PORESET_B to confirm that HRESET_B is normally ASSERTed and then DE-ASSERTed. At this time, RCW_SRC[0:8] was set to 0x9F. (Only DIFF_SYSCLK 100MHz is used.)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The next step is to connect to the device using CodeWarrior. However, when we click Diagnose Connection to check, an error occurs as shown below at the "&lt;STRONG&gt;Run target Initialization script&lt;/STRONG&gt;" stage and we cannot proceed any further.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jmsong_0-1744001569451.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/331534i1EA7D24E264819CC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jmsong_0-1744001569451.png" alt="jmsong_0-1744001569451.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;At this time, the Scan IDCODE is as follows.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;* Device 0&amp;nbsp; IDCODE: 5BA00477 Device: ARM DAP rev 5.x&lt;/P&gt;&lt;P&gt;* Device 1&amp;nbsp; IDCODE: 06B1201D&amp;nbsp; &amp;nbsp;Device: Unmapped NXP Device&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;In the initialization script file, USE_SAFE_RCW = True and BOOT_CHIP_SELECT = 2 are set.&lt;/P&gt;&lt;P&gt;and TA.rcw.set_source(0x9F)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I don't know if an error occurs when entering the internal register writing stage for DDR4 settings. (It's the same even if I change the address)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;def Init_DDRC_PD():&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080110, 0x450C0000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080000, 0x0000007F)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080008, 0x00000000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;CCSR_BE_M(0x01080010, 0x00000000)&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; .....&lt;/P&gt;</description>
      <pubDate>Mon, 07 Apr 2025 04:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Custom-Board-codewarrior-JTAG-Diagnose-Error/m-p/2074787#M15579</guid>
      <dc:creator>jmsong</dc:creator>
      <dc:date>2025-04-07T04:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A Custom Board codewarrior JTAG Diagnose Error</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-Custom-Board-codewarrior-JTAG-Diagnose-Error/m-p/2075980#M15592</link>
      <description>&lt;P&gt;&lt;SPAN&gt;My CWTAP IP address: &lt;/SPAN&gt;&lt;SPAN&gt;10.193.20.23&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Please refer the command below to debug your environment.&lt;/P&gt;
&lt;P&gt;In the CCS, run command below:&lt;/P&gt;
&lt;P&gt;(bin) 1 % delete all&lt;/P&gt;
&lt;P&gt;(bin) 2 % config cc cwtap:10.193.20.23&lt;/P&gt;
&lt;P&gt;(bin) 3 % show cc&lt;/P&gt;
&lt;P&gt;0: CodeWarrior TAP (cwtap:10.193.20.23) CC software ver. {0.0}&lt;/P&gt;
&lt;P&gt;(bin) 4 % ccs::config_chain {ls1043a dap sap2}&lt;/P&gt;
&lt;P&gt;(bin) 5 % display ::ccs::get_config_chain&lt;/P&gt;
&lt;P&gt;Chain Position 0: LS1043A&lt;/P&gt;
&lt;P&gt;Chain Position 1: CoreSight ATB Funnel&lt;/P&gt;
&lt;P&gt;Chain Position 2: CoreSight ATB Funnel&lt;/P&gt;
&lt;P&gt;Chain Position 3: CoreSight TMC&lt;/P&gt;
&lt;P&gt;Chain Position 4: CoreSight TMC&lt;/P&gt;
&lt;P&gt;Chain Position 5: CoreSight ATB Funnel&lt;/P&gt;
&lt;P&gt;Chain Position 6: CoreSight STM&lt;/P&gt;
&lt;P&gt;Chain Position 7: CoreSight TMC&lt;/P&gt;
&lt;P&gt;Chain Position 8: CoreSight ATB Funnel&lt;/P&gt;
&lt;P&gt;Chain Position 9: CoreSight ATB Funnel&lt;/P&gt;
&lt;P&gt;Chain Position 10: CoreSight TMC&lt;/P&gt;
&lt;P&gt;Chain Position 11: CoreSight TMC&lt;/P&gt;
&lt;P&gt;Chain Position 12: CoreSight TMC&lt;/P&gt;
&lt;P&gt;Chain Position 13: CoreSight CTI&lt;/P&gt;
&lt;P&gt;Chain Position 14: CoreSight CTI&lt;/P&gt;
&lt;P&gt;Chain Position 15: CoreSight CTI&lt;/P&gt;
&lt;P&gt;Chain Position 16: Cortex-A53&lt;/P&gt;
&lt;P&gt;Chain Position 17: CoreSight CTI&lt;/P&gt;
&lt;P&gt;Chain Position 18: Cortex-A53 PMU&lt;/P&gt;
&lt;P&gt;Chain Position 19: Cortex-A53 ETM&lt;/P&gt;
&lt;P&gt;Chain Position 20: Cortex-A53&lt;/P&gt;
&lt;P&gt;Chain Position 21: CoreSight CTI&lt;/P&gt;
&lt;P&gt;Chain Position 22: Cortex-A53 PMU&lt;/P&gt;
&lt;P&gt;Chain Position 23: Cortex-A53 ETM&lt;/P&gt;
&lt;P&gt;Chain Position 24: Cortex-A53&lt;/P&gt;
&lt;P&gt;Chain Position 25: CoreSight CTI&lt;/P&gt;
&lt;P&gt;Chain Position 26: Cortex-A53 PMU&lt;/P&gt;
&lt;P&gt;Chain Position 27: Cortex-A53 ETM&lt;/P&gt;
&lt;P&gt;Chain Position 28: Cortex-A53&lt;/P&gt;
&lt;P&gt;Chain Position 29: CoreSight CTI&lt;/P&gt;
&lt;P&gt;Chain Position 30: Cortex-A53 PMU&lt;/P&gt;
&lt;P&gt;Chain Position 31: Cortex-A53 ETM&lt;/P&gt;
&lt;P&gt;Chain Position 32: DAP&lt;/P&gt;
&lt;P&gt;Chain Position 33: SAP2&lt;/P&gt;
&lt;P&gt;(bin) 6 % ccs::display_mem 32 0x1080000 4 0 4&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +C&lt;/P&gt;
&lt;P&gt;[0x01080000] 0000007F 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;(bin) 7 % ccs::display_mem 32 0x1080000 4 0 40&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +4&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +8&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; +C&lt;/P&gt;
&lt;P&gt;[0x01080000] 0000007F 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080010] 00000000 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080020] 00000000 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080030] 00000000 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080040] 00000000 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080050] 00000000 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080060] 00000000 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080070] 00000000 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080080] 80040322 00000000 00000000 00000000&lt;/P&gt;
&lt;P&gt;[0x01080090] 00000000 00000000 00000000 00000000&lt;/P&gt;</description>
      <pubDate>Tue, 08 Apr 2025 09:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-Custom-Board-codewarrior-JTAG-Diagnose-Error/m-p/2075980#M15592</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2025-04-08T09:16:36Z</dc:date>
    </item>
  </channel>
</rss>