<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Issue with LS1046A Custom Board Under Temperature Stress Test in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Issue-with-LS1046A-Custom-Board-Under-Temperature-Stress-Test/m-p/2063292#M15513</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have designed a custom board using the LS1046A processor and conducted a temperature chamber test. However, when the board temperature reaches around 55°C and the CPU core temperature is approximately 70°C, the board's ASLEEP LED blinks periodically at about 0.5-second intervals, and the system stops functioning.&lt;/P&gt;&lt;P&gt;Additionally, when I connect a console cable, it appears that the system is attempting to reboot repeatedly, as shown in the log below. However, when the temperature decreases, the system resumes normal operation.&lt;/P&gt;&lt;P&gt;I used the LS1046A chip with the highest available temperature rating and referenced the FRWY board for my design.&lt;/P&gt;&lt;P&gt;Are there any debugging steps you would recommend?&lt;/P&gt;&lt;P&gt;(Log attached below)&lt;BR /&gt;&lt;BR /&gt;[2025-03-17 11:39:33.155] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:33.592]&lt;BR /&gt;[2025-03-17 11:39:33.592] NOTICE: 4 GB DDR4, 64-bit, CL=15, ECC on&lt;BR /&gt;[2025-03-17 11:39:33.592] NOTICE: BL2: v1.5(release):LSDK-20.12-dirty&lt;BR /&gt;[2025-03-17 11:39:33.592] NOTICE: BL2: Built : 10:47:11, Feb 7 2023&lt;BR /&gt;[2025-03-17 11:39:33.867] NOTICE: BL2: Booting BL31NOTICE: BL31: v1.5(release):LSDK-20.12-dirty&lt;BR /&gt;[2025-03-17 11:39:33.867] NOTICE: BL31: Built : 10:47:11, Feb 7 2023&lt;BR /&gt;[2025-03-17 11:39:33.867] NOTICE: Welcome to LS1046 BL31 Phase&lt;BR /&gt;[2025-03-17 11:39:33.867]&lt;BR /&gt;[2025-03-17 11:39:33.867]&lt;BR /&gt;[2025-03-17 11:39:33.867] U-Boot 2020.04-dirty (Feb 06 2023 - 22:20:05 +0900)&lt;BR /&gt;[2025-03-17 11:39:33.946]&lt;BR /&gt;[2025-03-17 11:39:33.946] SoC: LS1046A Rev1.0 (0x87070110)&lt;BR /&gt;[2025-03-17 11:39:33.946] Clock Configuration:&lt;BR /&gt;[2025-03-17 11:39:33.946] CPU0(A72):1600 MHz CPU1(A72):1600 MHz CPU2(A72):1600 MHz&lt;BR /&gt;[2025-03-17 11:39:33.946] CPU3(A72):1600 MHz&lt;BR /&gt;[2025-03-17 11:39:33.946] Bus: 600 MHz DDR: 2100 MT/s FMAN: 700 MHz&lt;BR /&gt;[2025-03-17 11:39:33.946] Reset Configuration Word (RCW):&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000000: 0c150010 0e000000 00000000 00000000&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000010: 11338888 00400016 40025000 c1000000&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000020: 00000000 00000000 00000000 00038800&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000030: 20044100 24003000 00000096 00000001&lt;BR /&gt;[2025-03-17 11:39:33.946] Model: LS1046A FRWY Board&lt;BR /&gt;[2025-03-17 11:39:33.946] Board: LS1046AFRWY-SATURN-HURA, Rev: B, boot from QSPI&lt;BR /&gt;[2025-03-17 11:39:33.946] SD1_CLK1 = 100.00MHZ, SD1_CLK2 = 100.00MHZ&lt;BR /&gt;[2025-03-17 11:39:33.946] DRAM: 3.9 GiB (DDR4, 64-bit, CL=15, ECC on)&lt;BR /&gt;[2025-03-17 11:39:33.955] SEC0: RNG instantiated&lt;BR /&gt;[2025-03-17 11:39:34.016] select_i2c_ch_pca9547: Cannot find udev for a bus 0&lt;BR /&gt;[2025-03-17 11:39:34.016] Using SERDES1 Protocol: 4403 (0x1133)&lt;BR /&gt;[2025-03-17 11:39:34.016] Using SERDES2 Protocol: 34952 (0x8888)&lt;BR /&gt;[2025-03-17 11:39:34.016] NAND: 0 MiB&lt;BR /&gt;[2025-03-17 11:39:34.016] MMC: FSL_SDHC: 0&lt;BR /&gt;[2025-03-17 11:39:34.016] Loading Environment from SPI Flash... SF: Detected mt25qu512a with page size 256 Bytes, erase size 64 KiB, total 64 MiB&lt;BR /&gt;[2025-03-17 11:39:34.016] OK&lt;BR /&gt;[2025-03-17 11:39:34.016] EEPROM: Read failed.&lt;BR /&gt;[2025-03-17 11:39:34.016] In: serial&lt;BR /&gt;[2025-03-17 11:39:34.016] Out: serial&lt;BR /&gt;[2025-03-17 11:39:34.016] Err: serial&lt;BR /&gt;[2025-03-17 11:39:34.016] Net: SF: Detected mt25qu512a with page size 256 Bytes, erase size 64 KiB, total 64 MiB&lt;BR /&gt;[2025-03-17 11:39:34.016] Fman1: Uploading microcode version 106.4.18&lt;BR /&gt;[2025-03-17 11:39:34.088] PCIe1: pcie@3400000 Root Complex: no link&lt;BR /&gt;[2025-03-17 11:39:34.088] PCIe2: pcie@3500000 disabled&lt;BR /&gt;[2025-03-17 11:39:34.088] PCIe3: pcie@3600000 disabled&lt;BR /&gt;[2025-03-17 11:39:34.088] FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1&lt;BR /&gt;[2025-03-17 11:39:34.088] Error: FM1@TGEC1 address not set.&lt;BR /&gt;[2025-03-17 11:39:34.088] , FM1@TGEC2&lt;BR /&gt;[2025-03-17 11:39:34.088] Error: FM1@TGEC2 address not set.&lt;BR /&gt;[2025-03-17 11:39:34.088]&lt;BR /&gt;[2025-03-17 11:39:34.088] Hit any key to stop autoboot: 3 2 1 0&lt;BR /&gt;[2025-03-17 11:39:37.144] switch to partitions #0, OK&lt;BR /&gt;[2025-03-17 11:39:37.160] mmc0(part 0) is current device&lt;BR /&gt;[2025-03-17 11:39:37.176] Scanning mmc 0:1...&lt;BR /&gt;[2025-03-17 11:39:37.326] Scanning mmc 0:2...&lt;BR /&gt;[2025-03-17 11:39:37.367] Found U-Boot script /ls1046afrwy_boot.scr&lt;BR /&gt;[2025-03-17 11:39:38.551] 17635632 bytes read in 1159 ms (14.5 MiB/s)&lt;BR /&gt;[2025-03-17 11:39:38.551] do_fpgaload: fpga_load 17635632 bytes in 2591 ms&lt;BR /&gt;[2025-03-17 11:39:41.181] 968 bytes read in 17 ms (54.7 KiB/s)&lt;BR /&gt;[2025-03-17 11:39:41.181] ## Executing script at 80000000&lt;BR /&gt;[2025-03-17 11:39:43.519] 35828224 bytes read in 2333 ms (14.6 MiB/s)&lt;BR /&gt;[2025-03-17 11:39:43.558] 31419 bytes read in 17 ms (1.8 MiB/s)&lt;BR /&gt;[2025-03-17 11:39:43.798] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:44.095] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:44.451] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:44.861] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:45.243] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:45.658] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:46.047] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:46.464] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:46.878] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:47.282] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:47.704] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:48.103] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:48.530] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:48.939] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:49.346] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:49.754] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:50.162] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:50.575] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:50.991] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:51.415] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:51.825] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:31.984] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:32.374] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:32.780] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:33.190] NOTICE: Fixed DDR on board&lt;/P&gt;</description>
    <pubDate>Mon, 17 Mar 2025 23:55:46 GMT</pubDate>
    <dc:creator>hyeonbin</dc:creator>
    <dc:date>2025-03-17T23:55:46Z</dc:date>
    <item>
      <title>Issue with LS1046A Custom Board Under Temperature Stress Test</title>
      <link>https://community.nxp.com/t5/Layerscape/Issue-with-LS1046A-Custom-Board-Under-Temperature-Stress-Test/m-p/2063292#M15513</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have designed a custom board using the LS1046A processor and conducted a temperature chamber test. However, when the board temperature reaches around 55°C and the CPU core temperature is approximately 70°C, the board's ASLEEP LED blinks periodically at about 0.5-second intervals, and the system stops functioning.&lt;/P&gt;&lt;P&gt;Additionally, when I connect a console cable, it appears that the system is attempting to reboot repeatedly, as shown in the log below. However, when the temperature decreases, the system resumes normal operation.&lt;/P&gt;&lt;P&gt;I used the LS1046A chip with the highest available temperature rating and referenced the FRWY board for my design.&lt;/P&gt;&lt;P&gt;Are there any debugging steps you would recommend?&lt;/P&gt;&lt;P&gt;(Log attached below)&lt;BR /&gt;&lt;BR /&gt;[2025-03-17 11:39:33.155] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:33.592]&lt;BR /&gt;[2025-03-17 11:39:33.592] NOTICE: 4 GB DDR4, 64-bit, CL=15, ECC on&lt;BR /&gt;[2025-03-17 11:39:33.592] NOTICE: BL2: v1.5(release):LSDK-20.12-dirty&lt;BR /&gt;[2025-03-17 11:39:33.592] NOTICE: BL2: Built : 10:47:11, Feb 7 2023&lt;BR /&gt;[2025-03-17 11:39:33.867] NOTICE: BL2: Booting BL31NOTICE: BL31: v1.5(release):LSDK-20.12-dirty&lt;BR /&gt;[2025-03-17 11:39:33.867] NOTICE: BL31: Built : 10:47:11, Feb 7 2023&lt;BR /&gt;[2025-03-17 11:39:33.867] NOTICE: Welcome to LS1046 BL31 Phase&lt;BR /&gt;[2025-03-17 11:39:33.867]&lt;BR /&gt;[2025-03-17 11:39:33.867]&lt;BR /&gt;[2025-03-17 11:39:33.867] U-Boot 2020.04-dirty (Feb 06 2023 - 22:20:05 +0900)&lt;BR /&gt;[2025-03-17 11:39:33.946]&lt;BR /&gt;[2025-03-17 11:39:33.946] SoC: LS1046A Rev1.0 (0x87070110)&lt;BR /&gt;[2025-03-17 11:39:33.946] Clock Configuration:&lt;BR /&gt;[2025-03-17 11:39:33.946] CPU0(A72):1600 MHz CPU1(A72):1600 MHz CPU2(A72):1600 MHz&lt;BR /&gt;[2025-03-17 11:39:33.946] CPU3(A72):1600 MHz&lt;BR /&gt;[2025-03-17 11:39:33.946] Bus: 600 MHz DDR: 2100 MT/s FMAN: 700 MHz&lt;BR /&gt;[2025-03-17 11:39:33.946] Reset Configuration Word (RCW):&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000000: 0c150010 0e000000 00000000 00000000&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000010: 11338888 00400016 40025000 c1000000&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000020: 00000000 00000000 00000000 00038800&lt;BR /&gt;[2025-03-17 11:39:33.946] 00000030: 20044100 24003000 00000096 00000001&lt;BR /&gt;[2025-03-17 11:39:33.946] Model: LS1046A FRWY Board&lt;BR /&gt;[2025-03-17 11:39:33.946] Board: LS1046AFRWY-SATURN-HURA, Rev: B, boot from QSPI&lt;BR /&gt;[2025-03-17 11:39:33.946] SD1_CLK1 = 100.00MHZ, SD1_CLK2 = 100.00MHZ&lt;BR /&gt;[2025-03-17 11:39:33.946] DRAM: 3.9 GiB (DDR4, 64-bit, CL=15, ECC on)&lt;BR /&gt;[2025-03-17 11:39:33.955] SEC0: RNG instantiated&lt;BR /&gt;[2025-03-17 11:39:34.016] select_i2c_ch_pca9547: Cannot find udev for a bus 0&lt;BR /&gt;[2025-03-17 11:39:34.016] Using SERDES1 Protocol: 4403 (0x1133)&lt;BR /&gt;[2025-03-17 11:39:34.016] Using SERDES2 Protocol: 34952 (0x8888)&lt;BR /&gt;[2025-03-17 11:39:34.016] NAND: 0 MiB&lt;BR /&gt;[2025-03-17 11:39:34.016] MMC: FSL_SDHC: 0&lt;BR /&gt;[2025-03-17 11:39:34.016] Loading Environment from SPI Flash... SF: Detected mt25qu512a with page size 256 Bytes, erase size 64 KiB, total 64 MiB&lt;BR /&gt;[2025-03-17 11:39:34.016] OK&lt;BR /&gt;[2025-03-17 11:39:34.016] EEPROM: Read failed.&lt;BR /&gt;[2025-03-17 11:39:34.016] In: serial&lt;BR /&gt;[2025-03-17 11:39:34.016] Out: serial&lt;BR /&gt;[2025-03-17 11:39:34.016] Err: serial&lt;BR /&gt;[2025-03-17 11:39:34.016] Net: SF: Detected mt25qu512a with page size 256 Bytes, erase size 64 KiB, total 64 MiB&lt;BR /&gt;[2025-03-17 11:39:34.016] Fman1: Uploading microcode version 106.4.18&lt;BR /&gt;[2025-03-17 11:39:34.088] PCIe1: pcie@3400000 Root Complex: no link&lt;BR /&gt;[2025-03-17 11:39:34.088] PCIe2: pcie@3500000 disabled&lt;BR /&gt;[2025-03-17 11:39:34.088] PCIe3: pcie@3600000 disabled&lt;BR /&gt;[2025-03-17 11:39:34.088] FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1&lt;BR /&gt;[2025-03-17 11:39:34.088] Error: FM1@TGEC1 address not set.&lt;BR /&gt;[2025-03-17 11:39:34.088] , FM1@TGEC2&lt;BR /&gt;[2025-03-17 11:39:34.088] Error: FM1@TGEC2 address not set.&lt;BR /&gt;[2025-03-17 11:39:34.088]&lt;BR /&gt;[2025-03-17 11:39:34.088] Hit any key to stop autoboot: 3 2 1 0&lt;BR /&gt;[2025-03-17 11:39:37.144] switch to partitions #0, OK&lt;BR /&gt;[2025-03-17 11:39:37.160] mmc0(part 0) is current device&lt;BR /&gt;[2025-03-17 11:39:37.176] Scanning mmc 0:1...&lt;BR /&gt;[2025-03-17 11:39:37.326] Scanning mmc 0:2...&lt;BR /&gt;[2025-03-17 11:39:37.367] Found U-Boot script /ls1046afrwy_boot.scr&lt;BR /&gt;[2025-03-17 11:39:38.551] 17635632 bytes read in 1159 ms (14.5 MiB/s)&lt;BR /&gt;[2025-03-17 11:39:38.551] do_fpgaload: fpga_load 17635632 bytes in 2591 ms&lt;BR /&gt;[2025-03-17 11:39:41.181] 968 bytes read in 17 ms (54.7 KiB/s)&lt;BR /&gt;[2025-03-17 11:39:41.181] ## Executing script at 80000000&lt;BR /&gt;[2025-03-17 11:39:43.519] 35828224 bytes read in 2333 ms (14.6 MiB/s)&lt;BR /&gt;[2025-03-17 11:39:43.558] 31419 bytes read in 17 ms (1.8 MiB/s)&lt;BR /&gt;[2025-03-17 11:39:43.798] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:44.095] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:44.451] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:44.861] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:45.243] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:45.658] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:46.047] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:46.464] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:46.878] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:47.282] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:47.704] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:48.103] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:48.530] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:48.939] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:49.346] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:49.754] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:50.162] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:50.575] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:50.991] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:51.415] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:39:51.825] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:31.984] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:32.374] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:32.780] NOTICE: Fixed DDR on board&lt;BR /&gt;[2025-03-17 11:40:33.190] NOTICE: Fixed DDR on board&lt;/P&gt;</description>
      <pubDate>Mon, 17 Mar 2025 23:55:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issue-with-LS1046A-Custom-Board-Under-Temperature-Stress-Test/m-p/2063292#M15513</guid>
      <dc:creator>hyeonbin</dc:creator>
      <dc:date>2025-03-17T23:55:46Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with LS1046A Custom Board Under Temperature Stress Test</title>
      <link>https://community.nxp.com/t5/Layerscape/Issue-with-LS1046A-Custom-Board-Under-Temperature-Stress-Test/m-p/2064423#M15521</link>
      <description>&lt;P&gt;The thermal management function is based on TMU (Thermal Monitoring Unit).&lt;BR /&gt;The driver sets two thresholds for management function. If the CPU temperature crosses the first one (75 C for LS2080. 85&lt;BR /&gt;C for other platforms), the driver will trigger CPU frequency limitation auto-scaling according to the temperature trend; If the&lt;BR /&gt;CPU temperature crosses the second one (85 C for LS2080, 95 C for other platforms, critical for core) the driver will shut down the system.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Mar 2025 07:02:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Issue-with-LS1046A-Custom-Board-Under-Temperature-Stress-Test/m-p/2064423#M15521</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-03-19T07:02:53Z</dc:date>
    </item>
  </channel>
</rss>