<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1028A TFA problems</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028A-TFA-problems/m-p/2055920#M15468</link>
    <description>&lt;P&gt;1. Please use QCVS DDRv tool to do DDR optimization and validation.&lt;/P&gt;
&lt;P&gt;2. Please refer to the following document to debug ATF.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/Debugging-ATF-and-u-boot-with-CodeWarrior-for-ARMv8/ta-p/1684233" target="_blank"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/Debugging-ATF-and-u-boot-with-CodeWarrior-for-ARMv8/ta-p/1684233&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 05 Mar 2025 03:52:04 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2025-03-05T03:52:04Z</dc:date>
    <item>
      <title>LS1028A TFA problems</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-TFA-problems/m-p/2055133#M15464</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;SPAN&gt;When burning the system via an SD card on my 1028A board, I encountered issues during the&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;BL2 phase of TFA&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;(Trusted Firmware-A). Sometimes it fails at loading&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;image 4&lt;/STRONG&gt;&lt;SPAN&gt;&amp;nbsp;during the BL2 stage, and other times it fails at loading&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;image 5&lt;/STRONG&gt;&lt;SPAN&gt;. The specific issues are as follows. How can I resolve this problem? thank you！&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: RCW BOOT SRC is SD&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: SoC workaround for DDR Errata A009803 was applied&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: SoC workaround for DDR Errata A009942 was applied&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: SoC workaround for DDR Errata A010165 was applied&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: time base 0 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: Fixed DDR on board&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Time after parsing SPD 4 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Time before programming controller 8 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Time used by DDR driver 18 ms&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: RCW BOOT SRC is SD&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: esdhc_emmc_init&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Card detected successfully&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: init done:&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: BL2: Built : 11:17:14, Feb 28 2025&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Configuring TrustZone Controller&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: ******* image_id: 3 ********&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: image_base: 4225761280;image_size: 0;image_max_size: 2097152;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: type: 1;version: 2;size: 24;attr: 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: ******* image_id: 4 ********&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: image_base: 4227858432;image_size: 0;image_max_size: 67108864;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: type: 1;version: 2;size: 24;attr: 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: ******* image_id: 5 ********&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: image_base: 2181038080;image_size: 0;image_max_size: 2044723200;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: type: 1;version: 2;size: 24;attr: 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: BL2: Doing platform setup&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start bl2_load_images id 3&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: BL2: Loading image id 3&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Loading image id=3 at address 0xfbe00000&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Image id=3 loaded: 0xfbe00000 - 0xfbe0d23d&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: load_auth_image_internal: 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start post_image_load id 3&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start bl2_load_images id 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: BL2: Loading image id 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;WARNING: Firmware Image Package header check failed. id=0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;WARNING: Failed to obtain reference to image id=4 (-2)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: load_auth_image_internal: -2&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;ERROR: BL2: Failed to load image id 4 (-2)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Authentication failure&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class=""&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: image_base: 4225761280;image_size: 0;image_max_size: 2097152;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: type: 1;version: 2;size: 24;attr: 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: ******* image_id: 4 ********&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: image_base: 4227858432;image_size: 0;image_max_size: 67108864;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: type: 1;version: 2;size: 24;attr: 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: ******* image_id: 5 ********&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: image_base: 2181038080;image_size: 0;image_max_size: 2044723200;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: type: 1;version: 2;size: 24;attr: 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: BL2: Doing platform setup&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start bl2_load_images id 3&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: BL2: Loading image id 3&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Loading image id=3 at address 0xfbe00000&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Image id=3 loaded: 0xfbe00000 - 0xfbe0d23d&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: load_auth_image_internal: 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start post_image_load id 3&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start bl2_load_images id 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: BL2: Loading image id 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Loading image id=4 at address 0xfc000000&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: Image id=4 loaded: 0xfc000000 - 0xfc07bdc0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: load_auth_image_internal: 0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start post_image_load id 4&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;NOTICE: start bl2_load_images id 5&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: BL2: Loading image id 5&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;WARNING: Firmware Image Package header check failed. id=0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;WARNING: Failed to obtain reference to image id=5 (-2)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;INFO: load_auth_image_internal: -2&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;ERROR: BL2: Failed to load image id 5 (-2)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Authentication failure&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Mar 2025 02:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-TFA-problems/m-p/2055133#M15464</guid>
      <dc:creator>barce</dc:creator>
      <dc:date>2025-03-04T02:36:31Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A TFA problems</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-TFA-problems/m-p/2055920#M15468</link>
      <description>&lt;P&gt;1. Please use QCVS DDRv tool to do DDR optimization and validation.&lt;/P&gt;
&lt;P&gt;2. Please refer to the following document to debug ATF.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/Debugging-ATF-and-u-boot-with-CodeWarrior-for-ARMv8/ta-p/1684233" target="_blank"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/Debugging-ATF-and-u-boot-with-CodeWarrior-for-ARMv8/ta-p/1684233&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Mar 2025 03:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-TFA-problems/m-p/2055920#M15468</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-03-05T03:52:04Z</dc:date>
    </item>
  </channel>
</rss>