<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピックls1012afrwy boot issue</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1012afrwy-boot-issue/m-p/2033387#M15307</link>
    <description>&lt;P&gt;I am attempting to build a linux image for an ls1012afrwy board, but am having trouble getting the board to boot with the image. I properly setup my environment for the ls1012afrwy board (using the setup environment script) and used the "bitbake fsl-image-networking" command to build the image. I then partitioned a micro SD card with a boot partition and a root file system partition. and attached the following images in the following partitions:&lt;BR /&gt;&lt;BR /&gt;boot&lt;BR /&gt;&amp;nbsp; &amp;nbsp;Image&lt;BR /&gt;&amp;nbsp; &amp;nbsp;Image.gz&lt;BR /&gt;&amp;nbsp; &amp;nbsp;fsl-ls1012a-frwy.dtb&lt;BR /&gt;root&lt;BR /&gt;&amp;nbsp; &amp;nbsp;core-image-minimal-ls1012afrwy.rootfs.ext4&lt;BR /&gt;&lt;BR /&gt;I have also tried using "uImage" rather than "Image" in the boot partition, and I have tried to expand the file system in the root partition as well. When I try entering u-boot and loading the kernel using the command "load mmc 0:1 0x42000000 Image", I receive the error "Error reading cluster. Unable to read file Image". Similarly, I am unable to read the .dtb file. U boot is able to see the files in the boot partition, as it successfully notes them when I use the "fatls" command. Any help is greatly appreciated!&lt;/P&gt;</description>
    <pubDate>Thu, 23 Jan 2025 18:51:00 GMT</pubDate>
    <dc:creator>AC7</dc:creator>
    <dc:date>2025-01-23T18:51:00Z</dc:date>
    <item>
      <title>ls1012afrwy boot issue</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1012afrwy-boot-issue/m-p/2033387#M15307</link>
      <description>&lt;P&gt;I am attempting to build a linux image for an ls1012afrwy board, but am having trouble getting the board to boot with the image. I properly setup my environment for the ls1012afrwy board (using the setup environment script) and used the "bitbake fsl-image-networking" command to build the image. I then partitioned a micro SD card with a boot partition and a root file system partition. and attached the following images in the following partitions:&lt;BR /&gt;&lt;BR /&gt;boot&lt;BR /&gt;&amp;nbsp; &amp;nbsp;Image&lt;BR /&gt;&amp;nbsp; &amp;nbsp;Image.gz&lt;BR /&gt;&amp;nbsp; &amp;nbsp;fsl-ls1012a-frwy.dtb&lt;BR /&gt;root&lt;BR /&gt;&amp;nbsp; &amp;nbsp;core-image-minimal-ls1012afrwy.rootfs.ext4&lt;BR /&gt;&lt;BR /&gt;I have also tried using "uImage" rather than "Image" in the boot partition, and I have tried to expand the file system in the root partition as well. When I try entering u-boot and loading the kernel using the command "load mmc 0:1 0x42000000 Image", I receive the error "Error reading cluster. Unable to read file Image". Similarly, I am unable to read the .dtb file. U boot is able to see the files in the boot partition, as it successfully notes them when I use the "fatls" command. Any help is greatly appreciated!&lt;/P&gt;</description>
      <pubDate>Thu, 23 Jan 2025 18:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1012afrwy-boot-issue/m-p/2033387#M15307</guid>
      <dc:creator>AC7</dc:creator>
      <dc:date>2025-01-23T18:51:00Z</dc:date>
    </item>
    <item>
      <title>Re: ls1012afrwy boot issue</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1012afrwy-boot-issue/m-p/2036732#M15335</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You can try with the pre-build image available in&amp;nbsp;&lt;A href="https://lsdk.github.io/components.html" target="_blank"&gt;https://lsdk.github.io/components.html&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Fri, 31 Jan 2025 19:09:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1012afrwy-boot-issue/m-p/2036732#M15335</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-01-31T19:09:15Z</dc:date>
    </item>
  </channel>
</rss>