<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Loading multiple vpps causes network disruption in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Loading-multiple-vpps-causes-network-disruption/m-p/2032149#M15299</link>
    <description>&lt;P&gt;The creation of dpmac.5 is based on disconnecting and reconnecting .&lt;BR /&gt;And when tcpdump data from eth0 find another error:&lt;/P&gt;&lt;P&gt;fsl_dpaa2_eth dpni.0 eth0:Could not add mcast MAC 01:00:5e:00:00:01 to the filtering table(err -110).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 22 Jan 2025 08:21:39 GMT</pubDate>
    <dc:creator>linxs</dc:creator>
    <dc:date>2025-01-22T08:21:39Z</dc:date>
    <item>
      <title>Loading multiple vpps causes network disruption</title>
      <link>https://community.nxp.com/t5/Layerscape/Loading-multiple-vpps-causes-network-disruption/m-p/2030982#M15291</link>
      <description>&lt;P&gt;&lt;SPAN&gt;U&lt;/SPAN&gt;&lt;SPAN&gt;sing the LX2160 chip under the Linux system&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;restool -v&lt;BR /&gt;restool v2.4 (10.30.0 compatible)&lt;/P&gt;&lt;P&gt;restool -m&lt;BR /&gt;MC firmware version: 10.36.0&lt;/P&gt;&lt;P&gt;ls-listni&lt;/P&gt;&lt;P&gt;dprc.1/dpni.0 (interface: eth0, end point: dpsw.0.1)&lt;BR /&gt;dprc.1/dprc.4/dpni.4 (end point: dpmac.9)&lt;BR /&gt;dprc.1/dprc.3/dpni.3 (end point: dpmac.7)&lt;BR /&gt;dprc.1/dprc.2/dpni.2 (end point: dpmac.6)&lt;BR /&gt;dprc.1/dprc.2/dpni.1 (end point: dpmac.5)&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I start vpp1 using dprc.3 and vpp2 using dprc.4, everything boots up normally, and the interface corresponding to dpni.0 works fine. However, when I start another PHY program using dprc.2, dpni.0 experiences abnormalities.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;vpp1 and vpp2 allocated resources are&amp;nbsp;DPCON_COUNT=8、DPBP_COUNT=16、DPMCP_COUNT=3、&lt;/SPAN&gt;&lt;SPAN&gt;DPSECI_COUNT=16、DPIO_COUNT=4、DPCI_COUNT=4、DPDMAI_COUNT=4&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;phy program&amp;nbsp;allocated resources are&amp;nbsp;DPCON_COUNT=8、DPBP_COUNT=16、DPMCP_COUNT=3、DPSECI_COUNT=16、DPIO_COUNT=34、DPCI_COUNT=4、DPDMAI_COUNT=4&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;cat /dev/fsl_mc_console&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;[E, qbman_nrec_isr:421, QBMAN] QBMAN non-recoverable event 0x10&lt;BR /&gt;[E, enq_deq:68, CTLU] ifp_mng_cmd_try_dequeue() returned -EBUSY at each 1000 tries&lt;BR /&gt;[E, enq_deq:68, CTLU] ifp_mng_cmd_try_dequeue() returned -EBUSY at each 1000 tries&lt;BR /&gt;[E, enq_deq:68, CTLU] ifp_mng_cmd_try_dequeue() returned -EBUSY at each 1000 tries&lt;BR /&gt;[E, enq_deq:68, CTLU] ifp_mng_cmd_try_dequeue() returned -EBUSY at each 1000 tries&lt;BR /&gt;[E, dpni_add_mac_addr:10686, DPNI] ID[4]: Failed to add address&lt;BR /&gt;[E, ifp_mng_cmd_enqueue:1755, CTLU] Busy: No available Management command descriptor&lt;BR /&gt;[E, ifp_mng_cmd_enqueue:1755, CTLU] Busy: No available Management command descriptor&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, there are no issues when only one vpp and the PHY program are started. Why is that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there any way to solve the problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for advice from experienced experts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards！&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Jan 2025 02:21:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Loading-multiple-vpps-causes-network-disruption/m-p/2030982#M15291</guid>
      <dc:creator>linxs</dc:creator>
      <dc:date>2025-01-21T02:21:23Z</dc:date>
    </item>
    <item>
      <title>Re: Loading multiple vpps causes network disruption</title>
      <link>https://community.nxp.com/t5/Layerscape/Loading-multiple-vpps-causes-network-disruption/m-p/2031937#M15298</link>
      <description>the issue you are facing due that the dpmac.5 is connected to the dpni.0 by default.&lt;BR /&gt;you can unbind it and then reassign it to other dpni.&lt;BR /&gt;please move out the dprc.4 ,3 and 2 from dprc.1   &lt;BR /&gt;In order to get a better grasp review the subject "3.7.8.5 Bringing up DPAA2 network interfaces" in the LLDP reference manual</description>
      <pubDate>Wed, 22 Jan 2025 03:36:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Loading-multiple-vpps-causes-network-disruption/m-p/2031937#M15298</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2025-01-22T03:36:24Z</dc:date>
    </item>
    <item>
      <title>Re: Loading multiple vpps causes network disruption</title>
      <link>https://community.nxp.com/t5/Layerscape/Loading-multiple-vpps-causes-network-disruption/m-p/2032149#M15299</link>
      <description>&lt;P&gt;The creation of dpmac.5 is based on disconnecting and reconnecting .&lt;BR /&gt;And when tcpdump data from eth0 find another error:&lt;/P&gt;&lt;P&gt;fsl_dpaa2_eth dpni.0 eth0:Could not add mcast MAC 01:00:5e:00:00:01 to the filtering table(err -110).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Jan 2025 08:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Loading-multiple-vpps-causes-network-disruption/m-p/2032149#M15299</guid>
      <dc:creator>linxs</dc:creator>
      <dc:date>2025-01-22T08:21:39Z</dc:date>
    </item>
  </channel>
</rss>