<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1088ardb send data over UART in U-boot during boot</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1088ardb-send-data-over-UART-in-U-boot-during-boot/m-p/2029761#M15283</link>
    <description>&lt;P&gt;Hello dear experts,&lt;/P&gt;&lt;P&gt;I need your support and suggestions for a problem I have. We have custom boards with several versions based on ls1088a-rdb.&amp;nbsp;In one of these versions, we have SD/eMMC connection switched via mux from cpld, designed on the same line.&amp;nbsp;If I activate the eMMC line from cpld before powering on the device, I can successfully see it in the "/dev/mmcblk0" path when I type "fdisk -l" in the user space.&amp;nbsp;But I want to use the SD card for booting and then activate the eMMC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried this in user space and switched the eMMC line by sending a command to CPLD from the ls1088 UART3(/dev/ttyS2) line.&amp;nbsp;However, when I say "fdisk -l" I don't see any active mmc lines. When I examine the kernel output with dmesg I get this error: "&lt;/P&gt;&lt;PRE&gt;/dev/mmcblk0: Can't open blockdev&lt;BR /&gt;mmcblk0: error -110 requesting status&lt;BR /&gt;mmcblk0: recovery failed!&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;My first question here is, is it possible to activate emmc after uboot and kernel initialization?&lt;/P&gt;&lt;P&gt;Second question is can I send data to CPLD via UART later during the flexbuild u-boot boot phase? UART1(ttyS0) is console, UART3 connected to CPLD.&amp;nbsp;Is it possible to send data via UART3 line in U-boot?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 17 Jan 2025 12:38:37 GMT</pubDate>
    <dc:creator>zeroqruel</dc:creator>
    <dc:date>2025-01-17T12:38:37Z</dc:date>
    <item>
      <title>LS1088ardb send data over UART in U-boot during boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088ardb-send-data-over-UART-in-U-boot-during-boot/m-p/2029761#M15283</link>
      <description>&lt;P&gt;Hello dear experts,&lt;/P&gt;&lt;P&gt;I need your support and suggestions for a problem I have. We have custom boards with several versions based on ls1088a-rdb.&amp;nbsp;In one of these versions, we have SD/eMMC connection switched via mux from cpld, designed on the same line.&amp;nbsp;If I activate the eMMC line from cpld before powering on the device, I can successfully see it in the "/dev/mmcblk0" path when I type "fdisk -l" in the user space.&amp;nbsp;But I want to use the SD card for booting and then activate the eMMC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried this in user space and switched the eMMC line by sending a command to CPLD from the ls1088 UART3(/dev/ttyS2) line.&amp;nbsp;However, when I say "fdisk -l" I don't see any active mmc lines. When I examine the kernel output with dmesg I get this error: "&lt;/P&gt;&lt;PRE&gt;/dev/mmcblk0: Can't open blockdev&lt;BR /&gt;mmcblk0: error -110 requesting status&lt;BR /&gt;mmcblk0: recovery failed!&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;My first question here is, is it possible to activate emmc after uboot and kernel initialization?&lt;/P&gt;&lt;P&gt;Second question is can I send data to CPLD via UART later during the flexbuild u-boot boot phase? UART1(ttyS0) is console, UART3 connected to CPLD.&amp;nbsp;Is it possible to send data via UART3 line in U-boot?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 17 Jan 2025 12:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088ardb-send-data-over-UART-in-U-boot-during-boot/m-p/2029761#M15283</guid>
      <dc:creator>zeroqruel</dc:creator>
      <dc:date>2025-01-17T12:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088ardb send data over UART in U-boot during boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088ardb-send-data-over-UART-in-U-boot-during-boot/m-p/2035858#M15325</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please explain more about the process you follow to "select" emmc instead of sd card and share the complete log file in .txt file to review it.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jan 2025 20:57:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088ardb-send-data-over-UART-in-U-boot-during-boot/m-p/2035858#M15325</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2025-01-29T20:57:59Z</dc:date>
    </item>
  </channel>
</rss>