<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Kernel-panic-not-syncing-Attempted-to-kill-init-exitcode/m-p/2028941#M15276</link>
    <description>&lt;P&gt;hi.&lt;/P&gt;&lt;P&gt;I am trying to &lt;SPAN class=""&gt;compile&lt;/SPAN&gt; the system for OK1046A-C2 board.&lt;/P&gt;&lt;P&gt;U-Boot version: U-Boot 2018.03&lt;BR /&gt;Kernel version: Linux 4.14&lt;/P&gt;&lt;P&gt;Compilation completed without any issues, but an error occurred during flashing with USB.&lt;/P&gt;&lt;P&gt;The printed information is as follows.&lt;/P&gt;&lt;P&gt;How can this problem be resolved?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 16 Jan 2025 10:14:40 GMT</pubDate>
    <dc:creator>fayeting</dc:creator>
    <dc:date>2025-01-16T10:14:40Z</dc:date>
    <item>
      <title>Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b</title>
      <link>https://community.nxp.com/t5/Layerscape/Kernel-panic-not-syncing-Attempted-to-kill-init-exitcode/m-p/2028941#M15276</link>
      <description>&lt;P&gt;hi.&lt;/P&gt;&lt;P&gt;I am trying to &lt;SPAN class=""&gt;compile&lt;/SPAN&gt; the system for OK1046A-C2 board.&lt;/P&gt;&lt;P&gt;U-Boot version: U-Boot 2018.03&lt;BR /&gt;Kernel version: Linux 4.14&lt;/P&gt;&lt;P&gt;Compilation completed without any issues, but an error occurred during flashing with USB.&lt;/P&gt;&lt;P&gt;The printed information is as follows.&lt;/P&gt;&lt;P&gt;How can this problem be resolved?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 10:14:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Kernel-panic-not-syncing-Attempted-to-kill-init-exitcode/m-p/2028941#M15276</guid>
      <dc:creator>fayeting</dc:creator>
      <dc:date>2025-01-16T10:14:40Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b</title>
      <link>https://community.nxp.com/t5/Layerscape/Kernel-panic-not-syncing-Attempted-to-kill-init-exitcode/m-p/2029070#M15277</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Something happens that the usb is disconnected and connected again in the midle of transfer data, I just try to burn again the BSP with the latest kernel to avoid this error.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jan 2025 13:47:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Kernel-panic-not-syncing-Attempted-to-kill-init-exitcode/m-p/2029070#M15277</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-01-16T13:47:06Z</dc:date>
    </item>
  </channel>
</rss>