<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ls1046a kernel panic in xhci_irq. How do I parse NXP custom ISS field in esr_el1? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1046a-kernel-panic-in-xhci-irq-How-do-I-parse-NXP-custom-ISS/m-p/2026231#M15270</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Refer to the doc of "ARM Cortex-A72 MPCore Processor" for the interpretation of "ISS" filed in SError exception.&lt;BR /&gt;&lt;BR /&gt;ISS=2 means "Slave Error". It might related to a PCIe Error.&lt;BR /&gt;&lt;BR /&gt;Please comment out "ls_pcie_fix_error_response" in "drivers/pci/controller/dwc/pci-layerscape.c" and run the test again, then share the crash log&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 13 Jan 2025 00:54:06 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2025-01-13T00:54:06Z</dc:date>
    <item>
      <title>ls1046a kernel panic in xhci_irq. How do I parse NXP custom ISS field in esr_el1?</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1046a-kernel-panic-in-xhci-irq-How-do-I-parse-NXP-custom-ISS/m-p/2020164#M15232</link>
      <description>&lt;P&gt;I am trying to resolve a problem I'm having with a kernel panic on the LS1046a. Our custom board has a PCIe switch and 12 PCIe slots, with each PCIe slot containing an ASM3142 dual USB host controller.&lt;/P&gt;&lt;P&gt;Intermittently, I receive kernel panics from routines related to the Linux XHCI implementation. These always seem to occur in 1 of 2 places. Either in the xhci_irq routine, or the xhci_handshake routine, but in either location, the panic always occurs on the instruction:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;dmb oshld&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This is a data memory barrier instruction, and the panic is caused by an SError (shown below).&amp;nbsp; I have no idea what could possibly cause an SError at this instruction, as there were no obvious illegal memory accesses prior to this. I am hoping the ESR_EL1 register may offer some clues, but I don't know how to parse it.&lt;/P&gt;&lt;P&gt;According to the AArch64-Registers document on developer.arm.com, the ESR_EL1 register value 0xbf000002 can be parsed as:&lt;/P&gt;&lt;P&gt;(bits 31:26) ESR_ESL1.EC = 0b101111&amp;nbsp;&amp;nbsp; ==&amp;gt;&amp;nbsp; SErrror&lt;/P&gt;&lt;P&gt;(bit 25)&amp;nbsp; ESR_ESL1.IL = 0b1 (32 bit instruction)&lt;/P&gt;&lt;P&gt;(bit 24)&amp;nbsp; ESR_ESL1. = 0b1 (Implementation defined)&lt;/P&gt;&lt;P&gt;Then, ISS bits 23:0 are an implementation defined value and I can't find any documentation that explains NXP's custom codes for the arm64 implementation in the LS1046a.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know how to interpret the ISS value 0x000002 on an SError exception for&amp;nbsp; the LS1046a? Or where I can download something that documents this? Importantly, does this offer any assistance at all in figuring out why a data memory barrier command would generate such an exception?&lt;/P&gt;&lt;P&gt;Alternatively, does anyone have any clue at all what might be happening here?&amp;nbsp; I'm stumped on what could be the problem.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any assistance is appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;------------------------------&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446849] SError Interrupt on CPU0, code 0x00000000bf000002 -- SError&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446857] CPU: 0 PID: 185 Comm: kworker/0:3 Tainted: G O 6.1.41-devel #49&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446862] Hardware name: LS1046A Copier Board (DT)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446864] Workqueue: events xhci_handle_command_timeout&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446873] pstate: 600000c5 (nZCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446877] pc : xhci_handshake+0x68/0x110&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446884] lr : xhci_handshake+0x60/0x110&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446887] sp : ffffffc00adf3b40&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446889] x29: ffffffc00adf3b40 x28: 0000000000000000 x27: 0000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446895] x26: 0000000000000000 x25: ffffffc00b379210 x24: 0000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446899] x23: 0000000000000000 x22: 0000000000000008 x21: ffffffc00b360038&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446904] x20: 00000053693ee8a8 x19: 00000000004c4b40 x18: ffffffc00e463c88&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446909] x17: 0000000000000000 x16: 0000000000000000 x15: 0000000000000001&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446913] x14: 00000000000003bb x13: 0000000000000000 x12: 0000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446917] x11: 0000000000000000 x10: 00000000000009e0 x9 : ffffffc00adf3d70&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446922] x8 : ffffff8801c7fb40 x7 : fefefefefefefeff x6 : 000000023074d81b&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446926] x5 : 00ffffffffffffff x4 : 002e7ddb00000000 x3 : 0000000000000018&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446931] x2 : 0000000000000000 x1 : ffffffc00adf3b00 x0 : 0000000000000000&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446936] Kernel panic - not syncing: Asynchronous SError Interrupt&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446938] CPU: 0 PID: 185 Comm: kworker/0:3 Tainted: G O 6.1.41-devel ##4&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446942] Hardware name: LS1046A Copier Board (DT)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446943] Workqueue: events xhci_handle_command_timeout&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446947] Call trace:&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446948] dump_backtrace+0xf0/0x130&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446955] show_stack+0x18/0x28&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446959] dump_stack_lvl+0x68/0x84&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446965] dump_stack+0x18/0x34&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446970] panic+0x1a0/0x998&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446974] nmi_panic+0xac/0xb0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446979] arm64_serror_panic+0x64/0x78&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446982] do_serror+0x34/0x80&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446984] el1h_64_error_handler+0x34/0x50&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446987] el1h_64_error+0x64/0x68&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446990] xhci_handshake+0x68/0x110&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446994] xhci_handle_command_timeout+0x180/0x5c0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.446997] process_one_work+0x1fc/0x350&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.447001] worker_thread+0x44/0x440&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.447004] kthread+0xf8/0x110&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier" size="2"&gt;[ 353.447007] ret_from_fork+0x10/0x20&lt;/FONT&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 28 Dec 2024 21:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1046a-kernel-panic-in-xhci-irq-How-do-I-parse-NXP-custom-ISS/m-p/2020164#M15232</guid>
      <dc:creator>AbelianMeme</dc:creator>
      <dc:date>2024-12-28T21:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: ls1046a kernel panic in xhci_irq. How do I parse NXP custom ISS field in esr_el1?</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1046a-kernel-panic-in-xhci-irq-How-do-I-parse-NXP-custom-ISS/m-p/2023140#M15251</link>
      <description>&lt;P&gt;Discussing with the AE team, will provide more update later.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jan 2025 09:12:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1046a-kernel-panic-in-xhci-irq-How-do-I-parse-NXP-custom-ISS/m-p/2023140#M15251</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-01-07T09:12:17Z</dc:date>
    </item>
    <item>
      <title>Re: ls1046a kernel panic in xhci_irq. How do I parse NXP custom ISS field in esr_el1?</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1046a-kernel-panic-in-xhci-irq-How-do-I-parse-NXP-custom-ISS/m-p/2026231#M15270</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Refer to the doc of "ARM Cortex-A72 MPCore Processor" for the interpretation of "ISS" filed in SError exception.&lt;BR /&gt;&lt;BR /&gt;ISS=2 means "Slave Error". It might related to a PCIe Error.&lt;BR /&gt;&lt;BR /&gt;Please comment out "ls_pcie_fix_error_response" in "drivers/pci/controller/dwc/pci-layerscape.c" and run the test again, then share the crash log&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 00:54:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1046a-kernel-panic-in-xhci-irq-How-do-I-parse-NXP-custom-ISS/m-p/2026231#M15270</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-01-13T00:54:06Z</dc:date>
    </item>
  </channel>
</rss>