<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1028 SPI 3-wire configuration and GPIO usage for CS in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028-SPI-3-wire-configuration-and-GPIO-usage-for-CS/m-p/1992987#M15093</link>
    <description>dear AntoNico10,&lt;BR /&gt;yes it is posible to configure SPI with 3-wire and it's necessary  to connect MISO and MOSI.&lt;BR /&gt;You can uso a GPIO pins as ChipSelect but keep in mind that you have to program the functionality as CS to them.</description>
    <pubDate>Tue, 12 Nov 2024 17:32:19 GMT</pubDate>
    <dc:creator>LFGP</dc:creator>
    <dc:date>2024-11-12T17:32:19Z</dc:date>
    <item>
      <title>LS1028 SPI 3-wire configuration and GPIO usage for CS</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-SPI-3-wire-configuration-and-GPIO-usage-for-CS/m-p/1992139#M15087</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am design a custom board with the LS1028 processor, and I have a couple of questions regarding SPI configuration:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Is it possible to configure SPI in 3-wire mode, or do I need to physically connect MISO and MOSI to achieve this setup?&lt;/LI&gt;&lt;LI&gt;Is it feasible to use other GPIO pins as Chip Select (CS) lines? For example, on SPI 3, I am already using CS1 and CS2 for USB power management, so I would like to assign another GPIO as a CS pin ( I need 2 CS pin ).&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Thank you for any guidance you can provide.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Nov 2024 17:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-SPI-3-wire-configuration-and-GPIO-usage-for-CS/m-p/1992139#M15087</guid>
      <dc:creator>AntoNico10</dc:creator>
      <dc:date>2024-11-11T17:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 SPI 3-wire configuration and GPIO usage for CS</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-SPI-3-wire-configuration-and-GPIO-usage-for-CS/m-p/1992987#M15093</link>
      <description>dear AntoNico10,&lt;BR /&gt;yes it is posible to configure SPI with 3-wire and it's necessary  to connect MISO and MOSI.&lt;BR /&gt;You can uso a GPIO pins as ChipSelect but keep in mind that you have to program the functionality as CS to them.</description>
      <pubDate>Tue, 12 Nov 2024 17:32:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-SPI-3-wire-configuration-and-GPIO-usage-for-CS/m-p/1992987#M15093</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2024-11-12T17:32:19Z</dc:date>
    </item>
  </channel>
</rss>