<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックPPS output on LS1028ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/PPS-output-on-LS1028ARDB/m-p/1991186#M15084</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using an LS1028ARDB with Real time edge to perform some synchronization tests on a bunch of devices.&lt;/P&gt;&lt;P&gt;In my configuration, the LS1028ARDB is the gPTP master, while the devices are slaves.&lt;/P&gt;&lt;P&gt;The devices are connected to swp0...3.&lt;/P&gt;&lt;P&gt;I need to measure the real synchronization accuracy by comparing the PPS output of the switch and the devices.&lt;/P&gt;&lt;P&gt;From my understanding, the switch should be able to generate the PPS on connector J12 (the SMA one). However, as it is now, I don't see any signal on such a connector (nor on J11 or J13).&lt;/P&gt;&lt;P&gt;Now, to me is not clear if there are any procedures to enable it. I don't see any specific reference on the Real-time Edge Software User Guide.&lt;/P&gt;&lt;P&gt;The only reference I found is in the Layerscape Software Development Kit User Guide Section 8.7.7.1 PPS signal. I followed the PPS interrupt verification, and everything went smoothly. I would have expected the PPS on J12 when the sync on eno0 is enabled, but nothing.&lt;/P&gt;&lt;P&gt;I also tried "Section 8.7.7.3 Programmable PTP pins" to enable the PPS output from swp0 but I don't get any signal from the SWTICH_1588_DAT0 on J13.&lt;/P&gt;&lt;P&gt;Am I missing something? Is there any procedure for enabling the PPS output synchronized with swp0...3? A PPS output synced with eno0 would be also ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
    <pubDate>Fri, 08 Nov 2024 16:13:26 GMT</pubDate>
    <dc:creator>Almor</dc:creator>
    <dc:date>2024-11-08T16:13:26Z</dc:date>
    <item>
      <title>PPS output on LS1028ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/PPS-output-on-LS1028ARDB/m-p/1991186#M15084</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using an LS1028ARDB with Real time edge to perform some synchronization tests on a bunch of devices.&lt;/P&gt;&lt;P&gt;In my configuration, the LS1028ARDB is the gPTP master, while the devices are slaves.&lt;/P&gt;&lt;P&gt;The devices are connected to swp0...3.&lt;/P&gt;&lt;P&gt;I need to measure the real synchronization accuracy by comparing the PPS output of the switch and the devices.&lt;/P&gt;&lt;P&gt;From my understanding, the switch should be able to generate the PPS on connector J12 (the SMA one). However, as it is now, I don't see any signal on such a connector (nor on J11 or J13).&lt;/P&gt;&lt;P&gt;Now, to me is not clear if there are any procedures to enable it. I don't see any specific reference on the Real-time Edge Software User Guide.&lt;/P&gt;&lt;P&gt;The only reference I found is in the Layerscape Software Development Kit User Guide Section 8.7.7.1 PPS signal. I followed the PPS interrupt verification, and everything went smoothly. I would have expected the PPS on J12 when the sync on eno0 is enabled, but nothing.&lt;/P&gt;&lt;P&gt;I also tried "Section 8.7.7.3 Programmable PTP pins" to enable the PPS output from swp0 but I don't get any signal from the SWTICH_1588_DAT0 on J13.&lt;/P&gt;&lt;P&gt;Am I missing something? Is there any procedure for enabling the PPS output synchronized with swp0...3? A PPS output synced with eno0 would be also ok.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alberto&lt;/P&gt;</description>
      <pubDate>Fri, 08 Nov 2024 16:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PPS-output-on-LS1028ARDB/m-p/1991186#M15084</guid>
      <dc:creator>Almor</dc:creator>
      <dc:date>2024-11-08T16:13:26Z</dc:date>
    </item>
  </channel>
</rss>