<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: IPSec Demo in LX2160ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1982432#M15020</link>
    <description>I run iperf3** sending packets from GE1 to GE0. When I do that, EP1 ipsec-secgw crash with segmentation fault.</description>
    <pubDate>Sat, 26 Oct 2024 19:57:11 GMT</pubDate>
    <dc:creator>lucasgm</dc:creator>
    <dc:date>2024-10-26T19:57:11Z</dc:date>
    <item>
      <title>IPSec Demo in LX2160ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1836629#M14135</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have acquired two LX2160ARDB dev board and I'm trying to setup an IPSec demo, following the instruction in `Running IPSec gateway application with 16 Cores on LX2 platform` section in this guide:&amp;nbsp;&lt;A href="https://docs.nxp.com/bundle/GUID-1441E561-3EAD-47FD-A50D-72E1A4E4D69E/page/GUID-9B14728A-B012-48BC-8F97-D11F6850B233.html" target="_self"&gt;https://docs.nxp.com/bundle/GUID-1441E561-3EAD-47FD-A50D-72E1A4E4D69E/page/GUID-9B14728A-B012-48BC-8F97-D11F6850B233.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;However, when I run the following command:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;dpdk-ipsec-secgw -c 0xFFFF -n 1 -- -p 0xf -P -u 0xa --config="(0,0,0),(0,1,1),(0,2,2),(0,3,3),(1,0,4),(1,1,5),(1,2,6),(1,3,7),(2,0,8),(2,1,9),(2,2,10),(2,3,11),(3,0,12),(3,1,13),(3,2,14),(3,3,15)" -f /usr/local/dpdk/ipsec/ep0_64X64_sha256_proto.cfg&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I get the following error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;EAL: Detected 16 lcore(s)
EAL: Detected 1 NUMA nodes
EAL: Detected static linkage of DPDK
EAL: Multi-process socket /var/run/dpdk/rte/mp_socket
EAL: Selected IOVA mode 'VA'
EAL: No available hugepages reported in hugepages-32768kB
EAL: No available hugepages reported in hugepages-64kB
EAL: No available hugepages reported in hugepages-1048576kB
EAL: Probing VFIO support...
EAL: VFIO support initialized
EAL: No legacy callbacks, legacy socket not created
Promiscuous mode selected
librte_ipsec usage: disabled
replay window size: 0
ESN: disabled
SA flags: 0
Frag TTL: 10000000000 ns
port 0 is not present on the board
EAL: Error - exiting with code: 1
Cause: check_poll_mode_params failed&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I also tried to use the DPDK test example that comes in the DPDK repository, here:&amp;nbsp;&lt;A href="https://github.com/nxp-qoriq/dpdk/tree/LSDK-21.08/examples/ipsec-secgw/test" target="_self"&gt;https://github.com/nxp-qoriq/dpdk/tree/LSDK-21.08/examples/ipsec-secgw/test&lt;/A&gt;&lt;BR /&gt;In that case, I get the following error:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;+ stdbuf -o0 /usr/local/bin/dpdk-ipsec-secgw --lcores=0 -n 4 --vdev=crypto_aesni_mb0 --vdev=net_tap0,mac=fixed eth0 -- -p 0x3 -u 1 -P '--config=(0,0,0),(1,0,0)' -f /tmp/tmp.kPgZZI7hsi
EAL: Detected 16 lcore(s)
EAL: Detected 1 NUMA nodes
EAL: Detected static linkage of DPDK
EAL: failed to parse device "crypto_aesni_mb0"
EAL: Unable to parse device 'crypto_aesni_mb0'
EAL: Error - exiting with code: 1
Cause: Invalid EAL parameters&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have found out in the DPDK documentation (here&amp;nbsp;&lt;A href="https://doc.dpdk.org/guides/cryptodevs/aesni_mb.html" target="_self"&gt;https://doc.dpdk.org/guides/cryptodevs/aesni_mb.html&lt;/A&gt;), section 2.5, that it requires intel code:&amp;nbsp;&lt;A href="https://github.com/intel/intel-ipsec-mb" target="_self"&gt;https://github.com/intel/intel-ipsec-mb&lt;/A&gt;&amp;nbsp;which I was not able to build for ARM64.&lt;/P&gt;&lt;P&gt;I tried to change the `CRYPTO_DEV` environment variable to `crypto_openssl` or `crypto_null`, but without success. In that case, I get the same erros as the first example.&lt;/P&gt;&lt;P&gt;Someone have any idea how to setup this demo?&lt;/P&gt;&lt;P&gt;I'm using LSDK 21.08 and the kernel config is attached.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 17:44:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1836629#M14135</guid>
      <dc:creator>lucasgm</dc:creator>
      <dc:date>2024-03-27T17:44:19Z</dc:date>
    </item>
    <item>
      <title>Re: IPSec Demo in LX2160ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1838268#M14139</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Linux CAAM driver has been built as a kernel module, it must be loaded with command "insmod caam_jr.ko" in kernel before running DPDK application.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Apr 2024 02:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1838268#M14139</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-04-01T02:42:56Z</dc:date>
    </item>
    <item>
      <title>Re: IPSec Demo in LX2160ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1982430#M15019</link>
      <description>&lt;P&gt;I've rebuild the LX2160ARDB image using the SDK 21.08 flexbuild, including only the dpdk package and leaving all other default configurations.&lt;/P&gt;&lt;P&gt;Following the PoC Userguide and other manuals, I was able to run the dpdk-ipsec-secgw in both boards . However, I cant find how to generate the traffic to test the performance.&lt;/P&gt;&lt;P&gt;My setup is the following:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;| GE0 | --- | EP0 | --- | EP1 | --- | GE1 |&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;GE are traffic generators, and EP are LX2160 ARDB baords. GE0 and GE1 are connected to EP0 and EP1 port 2 (10 Gbps, dpmac.4). EP0 and EP1 are connect through port 0 (40 Gbps, dpmac.2)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The script I'm using to setup EP0 and EP1 is the following (using the correct cfg file for ep0 and ep1):&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;sudo su

# Ubind eth0/dpni.1/dpmac.2 interface from fsl_dpaa2_eth network driver
echo dpni.1 &amp;gt; /sys/bus/fsl-mc/drivers/fsl_dpaa2_eth/unbind
restool dpni destroy dpni.1

# Bind dpmac.2,3,4,5,6 to dpni.1, dpni.2,3,4,5,6
chmod +x /usr/local/dpdk/dpaa2/dynamic_dpl.sh
source /usr/local/dpdk/dpaa2/dynamic_dpl.sh dpmac.2 dpmac.3 dpmac.4 dpmac.5 dpmac.6
dpdk-ipsec-secgw -c 0xFFFF -n 1 -- -p 0x5 -P -u 0x1 --config="(0,0,0),(0,1,1),(0,2,2),(0,3,3),(0,4,4),(0,5,5),(0,6,6),(0,7,7),(2,0,8),(2,1,9),(2,2,10),(2,3,11),(2,4,12),(2,5,13),(2,6,14),(2,7,15)" -f /usr/local/dpdk/ipsec/ep0_64X64_sha256_proto.cfg&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The ipsec-secgw runs without errors on both endpoints, showing both interfaces as "UP".&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I've set the IP&amp;nbsp;192.168.102.2/24 for GE0 and IP&amp;nbsp;192.168.2.2 for GE1. I've also set the corresponding MAC addresses in the ARP table (mapping GE1 in GE0 and vice-versa). Then, I run ipsec sending packets from GE1 to GE0. When I do that, &lt;STRONG&gt;EP1 ipsec-secgw crash with segmentation fault.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I know the packages are going from GE to EP because if I try to ping GE1 from GE0 without setting the MAC address, I see a message in EP0 ipsec-secgw saying the packet has an unsupported protocol (I believe it is the ARP messages).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm missing something? How can I debug this?&lt;/P&gt;</description>
      <pubDate>Sat, 26 Oct 2024 16:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1982430#M15019</guid>
      <dc:creator>lucasgm</dc:creator>
      <dc:date>2024-10-26T16:43:20Z</dc:date>
    </item>
    <item>
      <title>Re: IPSec Demo in LX2160ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1982432#M15020</link>
      <description>I run iperf3** sending packets from GE1 to GE0. When I do that, EP1 ipsec-secgw crash with segmentation fault.</description>
      <pubDate>Sat, 26 Oct 2024 19:57:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IPSec-Demo-in-LX2160ARDB/m-p/1982432#M15020</guid>
      <dc:creator>lucasgm</dc:creator>
      <dc:date>2024-10-26T19:57:11Z</dc:date>
    </item>
  </channel>
</rss>