<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: The 10G network can send data but cannot receive data</title>
    <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1972103#M14982</link>
    <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuweilai_0-1728641187952.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304210iF75854480331BBC8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xuweilai_0-1728641187952.jpeg" alt="xuweilai_0-1728641187952.jpeg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuweilai_1-1728641197535.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304211iDB26B8C3AE01EDCB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xuweilai_1-1728641197535.jpeg" alt="xuweilai_1-1728641197535.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp; I am trapped with this bus for a long time,could you help me ?&lt;BR /&gt;dpmac increase with rx frags when host pinging 2160, but dpni could not get data from dpmac.17&lt;/P&gt;</description>
    <pubDate>Fri, 11 Oct 2024 10:10:48 GMT</pubDate>
    <dc:creator>xuweilai</dc:creator>
    <dc:date>2024-10-11T10:10:48Z</dc:date>
    <item>
      <title>The 10G network can send data but cannot receive data</title>
      <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1353936#M9077</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The network can send data but cannot receive data.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;we used the marvell 88x3310 phy device.&amp;nbsp;&lt;SPAN class="tgt"&gt;I have checked the PHY checklist and there is no problem. &lt;SPAN&gt;The PHY drivers have been loaded successfully.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="tgt"&gt;Usxgmii is used for THE PHY and DPMAC14, and 10GBase-T mode is used for the outside of the PHY.&lt;/SPAN&gt;&lt;SPAN class="tgt"&gt;Currently, ping the target device under the kernel, the target device can receive data, and also responded, but our LX2160 can not receive data&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="tgt"&gt;&lt;SPAN&gt;Can you give me some debugging advice?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="tgt"&gt;&lt;SPAN&gt;root@localhost:~# &lt;FONT color="#FF6600"&gt;ls-listni&lt;/FONT&gt;&lt;BR /&gt;dprc.1/dpni.2 (interface: eth0, end point: dpmac.17)&lt;BR /&gt;dprc.1/dpni.1 (interface: eth1, end point: dpmac.14)&lt;BR /&gt;dprc.1/dpni.0 (interface: eth2, end point: dpmac.13)&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;root@localhost:~# &lt;FONT face="andale mono,times" color="#FF6600"&gt;ifconfig eth1&lt;/FONT&gt;&lt;BR /&gt;eth1: flags=4355&amp;lt;UP,BROADCAST,PROMISC,MULTICAST&amp;gt; mtu 1500&lt;BR /&gt;inet 10.0.1.111 netmask 255.0.0.0 broadcast 10.255.255.255&lt;BR /&gt;inet6 fe80::94ae:91ff:fea5:9ce prefixlen 64 scopeid 0x20&amp;lt;link&amp;gt;&lt;BR /&gt;ether 96:ae:91:a5:09:ce txqueuelen 1000 (Ethernet)&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;RX packets 0 bytes 0 (0.0 B)&lt;/FONT&gt;&lt;BR /&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;TX packets 21 bytes 1314 (1.3 KB)&lt;/FONT&gt;&lt;BR /&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/P&gt;&lt;P&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~# ethtool eth1&lt;BR /&gt;Settings for eth1:&lt;BR /&gt;Supported ports: [ ]&lt;BR /&gt;Supported link modes: 10baseT/Full&lt;BR /&gt;100baseT/Full&lt;BR /&gt;1000baseT/Full&lt;BR /&gt;10000baseT/Full&lt;BR /&gt;2500baseT/Full&lt;BR /&gt;Supported pause frame use: No&lt;BR /&gt;Supports auto-negotiation: Yes&lt;BR /&gt;Supported FEC modes: Not reported&lt;BR /&gt;Advertised link modes: 10baseT/Full&lt;BR /&gt;100baseT/Full&lt;BR /&gt;1000baseT/Full&lt;BR /&gt;10000baseT/Full&lt;BR /&gt;2500baseT/Full&lt;BR /&gt;Advertised pause frame use: No&lt;BR /&gt;Advertised auto-negotiation: Yes&lt;BR /&gt;Advertised FEC modes: Not reported&lt;BR /&gt;&lt;FONT color="#FF6600"&gt;Speed: 1000Mb/s&lt;/FONT&gt;&lt;BR /&gt;Duplex: Full&lt;BR /&gt;Port: Twisted Pair&lt;BR /&gt;PHYAD: 0&lt;BR /&gt;Transceiver: internal&lt;BR /&gt;Auto-negotiation: on&lt;BR /&gt;MDI-X: Unknown&lt;BR /&gt;Link detected: no&lt;BR /&gt;&lt;BR /&gt;root@localhost:~#&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 12 Oct 2021 06:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1353936#M9077</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2021-10-12T06:34:07Z</dc:date>
    </item>
    <item>
      <title>Re: The 10G network can send data but cannot receive data</title>
      <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1357130#M9113</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Please run icmp ping for a while and then stop it.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Then share us the output of following commands - &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;restool dpmac info dpmac.14&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;restool dpni info dpni.1&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Also give us the full boot logs, right from u-boot to linux shell &lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Oct 2021 10:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1357130#M9113</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-10-18T10:02:54Z</dc:date>
    </item>
    <item>
      <title>Re: The 10G network can send data but cannot receive data</title>
      <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1357151#M9114</link>
      <description>&lt;P&gt;thanks ur reply.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The log file is attached 。i can not see any problem form follow information.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;root@localhost:~# ls-listni&lt;BR /&gt;dprc.1/dpni.2 (interface: eth0, end point: dpmac.17)&lt;BR /&gt;dprc.1/dpni.1 (interface: eth1, end point: dpmac.14)&lt;BR /&gt;dprc.1/dpni.0 (interface: eth2, end point: dpmac.13)&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~# ifconfig eth1 10.0.1.111&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~# ping 10.0.1.222&lt;BR /&gt;PING 10.0.1.222 (10.0.1.222) 56(84) bytes of data.&lt;BR /&gt;From 10.0.1.111 icmp_seq=1 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=2 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=3 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=4 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=5 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=6 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=7 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=8 Destination Host Unreachable&lt;BR /&gt;From 10.0.1.111 icmp_seq=9 Destination Host Unreachable&lt;BR /&gt;^C&lt;BR /&gt;--- 10.0.1.222 ping statistics ---&lt;BR /&gt;10 packets transmitted, 0 received, +9 errors, 100% packet loss, time 9204ms&lt;BR /&gt;pipe 4&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~# restool dpmac info dpmac.14&lt;BR /&gt;dpmac version: 4.7&lt;BR /&gt;dpmac object id/portal id: 14&lt;BR /&gt;plugged state: plugged&lt;BR /&gt;endpoint state: 1&lt;BR /&gt;endpoint: dpni.1, link is up&lt;BR /&gt;DPMAC link type: DPMAC_LINK_TYPE_PHY&lt;BR /&gt;DPMAC ethernet interface: DPMAC_ETH_IF_USXGMII&lt;BR /&gt;MAC address: 36:ab:e6:e4:da:4d&lt;BR /&gt;maximum supported rate 10000 Mbps&lt;BR /&gt;Counters:&lt;BR /&gt;rx all frames: 0&lt;BR /&gt;rx frames ok: 0&lt;BR /&gt;rx frame errors: 0&lt;BR /&gt;rx frame discards: 0&lt;BR /&gt;rx u-cast: 0&lt;BR /&gt;rx b-cast: 0&lt;BR /&gt;rx m-cast: 0&lt;BR /&gt;rx 64 bytes: 0&lt;BR /&gt;rx 65-127 bytes: 0&lt;BR /&gt;rx 128-255 bytes: 0&lt;BR /&gt;rx 256-511 bytes: 0&lt;BR /&gt;rx 512-1023 bytes: 0&lt;BR /&gt;rx 1024-1518 bytes: 0&lt;BR /&gt;rx 1519-max bytes: 0&lt;BR /&gt;rx frags: 0&lt;BR /&gt;rx jabber: 0&lt;BR /&gt;rx align errors: 0&lt;BR /&gt;rx oversized: 0&lt;BR /&gt;rx pause: 0&lt;BR /&gt;rx bytes: 0&lt;BR /&gt;tx frames ok: 22&lt;BR /&gt;tx u-cast: 0&lt;BR /&gt;tx m-cast: 10&lt;BR /&gt;tx b-cast: 12&lt;BR /&gt;tx frame errors: 0&lt;BR /&gt;tx undersized: 0&lt;BR /&gt;tx b-pause: 0&lt;BR /&gt;tx bytes: 1604&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~#&lt;BR /&gt;root@localhost:~# restool dpni info dpni.1&lt;BR /&gt;dpni version: 7.16&lt;BR /&gt;dpni id: 1&lt;BR /&gt;plugged state: plugged&lt;BR /&gt;endpoint state: 1&lt;BR /&gt;endpoint: dpmac.14, link is up&lt;BR /&gt;link status: 1 - up&lt;BR /&gt;mac address: 36:ab:e6:e4:da:4d&lt;BR /&gt;dpni_attr.options value is: 0&lt;BR /&gt;num_queues: 16&lt;BR /&gt;num_cgs: 1&lt;BR /&gt;num_rx_tcs: 1&lt;BR /&gt;num_tx_tcs: 1&lt;BR /&gt;mac_entries: 16&lt;BR /&gt;vlan_entries: 0&lt;BR /&gt;qos_entries: 0&lt;BR /&gt;fs_entries: 64&lt;BR /&gt;qos_key_size: 0&lt;BR /&gt;fs_key_size: 56&lt;BR /&gt;ingress_all_frames: 0&lt;BR /&gt;ingress_all_bytes: 0&lt;BR /&gt;ingress_multicast_frames: 0&lt;BR /&gt;ingress_multicast_bytes: 0&lt;BR /&gt;ingress_broadcast_frames: 0&lt;BR /&gt;ingress_broadcast_bytes: 0&lt;BR /&gt;egress_all_frames: 22&lt;BR /&gt;egress_all_bytes: 1300&lt;BR /&gt;egress_multicast_frames: 10&lt;BR /&gt;egress_multicast_bytes: 796&lt;BR /&gt;egress_broadcast_frames: 12&lt;BR /&gt;egress_broadcast_bytes: 504&lt;BR /&gt;ingress_filtered_frames: 0&lt;BR /&gt;ingress_discarded_frames: 0&lt;BR /&gt;ingress_nobuffer_discards: 0&lt;BR /&gt;egress_discarded_frames: 0&lt;BR /&gt;egress_confirmed_frames: 22&lt;BR /&gt;root@localhost:~#&lt;/P&gt;</description>
      <pubDate>Mon, 18 Oct 2021 10:38:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1357151#M9114</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2021-10-18T10:38:51Z</dc:date>
    </item>
    <item>
      <title>Re: The 10G network can send data but cannot receive data</title>
      <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1358310#M9134</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Are you using generic PHY driver or specific PHY driver say - drivers/net/phy/marvell10g.c ?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In case you are using specific PHY driver, then Can you use generic driver once and see if your problem still persists.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 05:25:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1358310#M9134</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-10-20T05:25:27Z</dc:date>
    </item>
    <item>
      <title>Re: The 10G network can send data but cannot receive data</title>
      <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1358399#M9136</link>
      <description>&lt;P&gt;&lt;SPAN&gt;generic PHY driver and specific PHY driver ---- drivers/net/phy/marvell10g.c&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I've tested them all, are the same prolem.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 07:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1358399#M9136</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2021-10-20T07:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: The 10G network can send data but cannot receive data</title>
      <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1358445#M9137</link>
      <description>&lt;P&gt;the problem is resolved.it is a hardware problem&lt;/P&gt;</description>
      <pubDate>Wed, 20 Oct 2021 07:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1358445#M9137</guid>
      <dc:creator>muaxi8</dc:creator>
      <dc:date>2021-10-20T07:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: The 10G network can send data but cannot receive data</title>
      <link>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1972103#M14982</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuweilai_0-1728641187952.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304210iF75854480331BBC8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xuweilai_0-1728641187952.jpeg" alt="xuweilai_0-1728641187952.jpeg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xuweilai_1-1728641197535.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/304211iDB26B8C3AE01EDCB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xuweilai_1-1728641197535.jpeg" alt="xuweilai_1-1728641197535.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp; I am trapped with this bus for a long time,could you help me ?&lt;BR /&gt;dpmac increase with rx frags when host pinging 2160, but dpni could not get data from dpmac.17&lt;/P&gt;</description>
      <pubDate>Fri, 11 Oct 2024 10:10:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-10G-network-can-send-data-but-cannot-receive-data/m-p/1972103#M14982</guid>
      <dc:creator>xuweilai</dc:creator>
      <dc:date>2024-10-11T10:10:48Z</dc:date>
    </item>
  </channel>
</rss>