<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1088A DDR Size in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1971226#M14978</link>
    <description>&lt;P&gt;Thank for reply.&lt;BR /&gt;If I delete "mcmemsize" will network performance decrease?&lt;/P&gt;</description>
    <pubDate>Thu, 10 Oct 2024 09:13:22 GMT</pubDate>
    <dc:creator>cuongkelvin</dc:creator>
    <dc:date>2024-10-10T09:13:22Z</dc:date>
    <item>
      <title>LS1088A DDR Size</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1969396#M14974</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we are having a DDR4 size problem on LS1088a platform.&amp;nbsp; We have 4GB DDR4 on the board. When u-boot starts it is confirmed that board has 4GB DDR4. But when we checked on kernel with free commands, it shows that RAM is 2GB.&amp;nbsp; I was&amp;nbsp;&lt;SPAN&gt;delete the "mcmemsize" variable from my U-Boot configuration.&amp;nbsp;&lt;/SPAN&gt;Do you have any idea why are we having mismatch DDR size in u-boot and kernel ?&lt;/P&gt;&lt;P&gt;Attached photos you can see the differences.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2024-10-09 09-21-15.png" style="width: 408px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/303563iEC4BDF2B8FA0DE7C/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2024-10-09 09-21-15.png" alt="Screenshot from 2024-10-09 09-21-15.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2024-10-09 09-21-15.png&lt;/span&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2024-10-09 09-18-52.png" style="width: 504px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/303564i7E3489CC69731D35/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2024-10-09 09-18-52.png" alt="Screenshot from 2024-10-09 09-18-52.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Screenshot from 2024-10-09 09-18-52.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 02:29:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1969396#M14974</guid>
      <dc:creator>cuongkelvin</dc:creator>
      <dc:date>2024-10-09T02:29:31Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088A DDR Size</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1969724#M14975</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The lost DDR can be divided into 2 parts.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;1) DDR used by NXP specific software, firmware components&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2) DDR used by various segments of kernel.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For the first part,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;1) u-boot uses memory till it is used, but once kernel boots, u-boot is swapped out of memory.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2) 66 MB is used by TF-A&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;3) MC can use anywhere between 512M to 2G (it depends on u-boot comandline argument 'mcmemsize'). The parameter mcmemsize defines amount of system DDR to be used by the Management Complex. If this variable is not defined, the compile-time value 0x70000000 or 1.75GB will be the default. Normally, users do not need to set this variable because the default is acceptable.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;TF-A+MC is about 1.8G&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;kernel reserved=(18620K kernel code, 2476K rwdata, 8844K rodata, 5888K init, 993K bss, 406712K reserved, 327680K cma-reserved) = 771213K=0.7G&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;MemTotal in /proc/meminfo is 14232028 kB, the lost memory is about 16-13.6=2.4G(TF-A+MC+kernel reserved)&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;root@TinyLinux:~# cat /proc/meminfo&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;MemTotal:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 14232028 kB&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;MemFree:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 13596760 kB&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;MemAvailable:&amp;nbsp;&amp;nbsp; 13478276 kB&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Oct 2024 08:21:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1969724#M14975</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-10-09T08:21:58Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088A DDR Size</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1971226#M14978</link>
      <description>&lt;P&gt;Thank for reply.&lt;BR /&gt;If I delete "mcmemsize" will network performance decrease?&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 09:13:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1971226#M14978</guid>
      <dc:creator>cuongkelvin</dc:creator>
      <dc:date>2024-10-10T09:13:22Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088A DDR Size</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1971229#M14979</link>
      <description>&lt;P&gt;Yes, it will.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Oct 2024 09:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088A-DDR-Size/m-p/1971229#M14979</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-10-10T09:15:32Z</dc:date>
    </item>
  </channel>
</rss>