<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AW-XM458MA-PUR Module Not Detected via PCIe on NXP LA1224 Reference Board in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/AW-XM458MA-PUR-Module-Not-Detected-via-PCIe-on-NXP-LA1224/m-p/1964252#M14942</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi Team,&lt;BR /&gt;We have connected the AW-XM458MA-PUR module to the NXP LA1224-rdb Reference Design Board using the PCIe M.2 Key E connector on the J7 slot.&lt;BR /&gt;In the system image, we have configured the SERDES protocol as follows:&lt;BR /&gt;SRDS_PLL_PD_PLL5=1&lt;BR /&gt;SRDS_PRTCL_S1=19&lt;BR /&gt;SRDS_PRTCL_S2=5&lt;BR /&gt;SRDS_PRTCL_S3=2&lt;BR /&gt;SRDS_PLL_REF_CLK_SEL_S1=2&lt;BR /&gt;SRDS_DIV_PEX_S1=1&lt;BR /&gt;SRDS_DIV_PEX_S2=1&lt;BR /&gt;SRDS_DIV_PEX_S3=1&lt;BR /&gt;Additionally, PCIe support has been enabled in the Linux kernel, and we have attached the corresponding configuration file&amp;nbsp; and pin mapping for reference.&lt;BR /&gt;However, we are encountering an issue where the module is not being detected when running the lspci command—no module appears in the PCIe device list.&lt;BR /&gt;Could you please provide guidance or troubleshooting steps to resolve this issue and get the module detected correctly?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 30 Sep 2024 07:22:29 GMT</pubDate>
    <dc:creator>Anitha1</dc:creator>
    <dc:date>2024-09-30T07:22:29Z</dc:date>
    <item>
      <title>AW-XM458MA-PUR Module Not Detected via PCIe on NXP LA1224 Reference Board</title>
      <link>https://community.nxp.com/t5/Layerscape/AW-XM458MA-PUR-Module-Not-Detected-via-PCIe-on-NXP-LA1224/m-p/1964252#M14942</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Team,&lt;BR /&gt;We have connected the AW-XM458MA-PUR module to the NXP LA1224-rdb Reference Design Board using the PCIe M.2 Key E connector on the J7 slot.&lt;BR /&gt;In the system image, we have configured the SERDES protocol as follows:&lt;BR /&gt;SRDS_PLL_PD_PLL5=1&lt;BR /&gt;SRDS_PRTCL_S1=19&lt;BR /&gt;SRDS_PRTCL_S2=5&lt;BR /&gt;SRDS_PRTCL_S3=2&lt;BR /&gt;SRDS_PLL_REF_CLK_SEL_S1=2&lt;BR /&gt;SRDS_DIV_PEX_S1=1&lt;BR /&gt;SRDS_DIV_PEX_S2=1&lt;BR /&gt;SRDS_DIV_PEX_S3=1&lt;BR /&gt;Additionally, PCIe support has been enabled in the Linux kernel, and we have attached the corresponding configuration file&amp;nbsp; and pin mapping for reference.&lt;BR /&gt;However, we are encountering an issue where the module is not being detected when running the lspci command—no module appears in the PCIe device list.&lt;BR /&gt;Could you please provide guidance or troubleshooting steps to resolve this issue and get the module detected correctly?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Sep 2024 07:22:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/AW-XM458MA-PUR-Module-Not-Detected-via-PCIe-on-NXP-LA1224/m-p/1964252#M14942</guid>
      <dc:creator>Anitha1</dc:creator>
      <dc:date>2024-09-30T07:22:29Z</dc:date>
    </item>
  </channel>
</rss>