<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Testing 802.1 Qav on ls1028a switch in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Testing-802-1-Qav-on-ls1028a-switch/m-p/1958724#M14904</link>
    <description>&lt;P&gt;I am using mickledore branch of &lt;A href="https://github.com/nxp-qoriq/yocto-sdk.git" target="_blank" rel="noopener"&gt;https://github.com/nxp-qoriq/yocto-sdk.git&amp;nbsp;&lt;/A&gt;on the ls1028a-rdb.&lt;/P&gt;&lt;P&gt;And indeed with cut-through disabled it works as expected.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Fri, 20 Sep 2024 10:26:39 GMT</pubDate>
    <dc:creator>_mkl</dc:creator>
    <dc:date>2024-09-20T10:26:39Z</dc:date>
    <item>
      <title>Testing 802.1 Qav on ls1028a switch</title>
      <link>https://community.nxp.com/t5/Layerscape/Testing-802-1-Qav-on-ls1028a-switch/m-p/1943076#M14835</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am following the TSN tests on ls1028ardb in 4.1.4 of the Real-time Edge Software User Guide, but I am unable to get Qav on the switch to work. The switch always forwards the full transmission rate.&lt;/P&gt;&lt;P&gt;I have configured enetc2 as DSA port and enetc3 as standard port and send traffic with class 5 from enetc3 to swp5. On swp0 a second ls1028ardb is connected to capture the frames. If I configure Qav on the enetc3 port the rate is limited as expected, but not if i configure it on swp0:&lt;/P&gt;&lt;P&gt;$ sudo tsntool cbsset --device swp0 --tc 5 --percentage 10&lt;/P&gt;&lt;P&gt;In the manual two streams are mentioned, does the switch only rate limit with interferring streams? On enetc I had to configure also the upper traffic classes, does this apply to the switch as well?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Aug 2024 05:55:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Testing-802-1-Qav-on-ls1028a-switch/m-p/1943076#M14835</guid>
      <dc:creator>_mkl</dc:creator>
      <dc:date>2024-08-29T05:55:23Z</dc:date>
    </item>
    <item>
      <title>Re: Testing 802.1 Qav on ls1028a switch</title>
      <link>https://community.nxp.com/t5/Layerscape/Testing-802-1-Qav-on-ls1028a-switch/m-p/1950832#M14861</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Which version of RTedge are you using? LS1028ARDB board?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In default configuration of LS1028ARDB dts, if eno3 is disabled, eno2 is used DSA port, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if eno3 is enabled, eno3 will be used DSA port in default.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;About Qav, customer should disable cut through mode using below command before running cbsset:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;tsntool ctset --device swp0 --queue_stat 0x0&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 08:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Testing-802-1-Qav-on-ls1028a-switch/m-p/1950832#M14861</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-09-10T08:11:21Z</dc:date>
    </item>
    <item>
      <title>Re: Testing 802.1 Qav on ls1028a switch</title>
      <link>https://community.nxp.com/t5/Layerscape/Testing-802-1-Qav-on-ls1028a-switch/m-p/1958724#M14904</link>
      <description>&lt;P&gt;I am using mickledore branch of &lt;A href="https://github.com/nxp-qoriq/yocto-sdk.git" target="_blank" rel="noopener"&gt;https://github.com/nxp-qoriq/yocto-sdk.git&amp;nbsp;&lt;/A&gt;on the ls1028a-rdb.&lt;/P&gt;&lt;P&gt;And indeed with cut-through disabled it works as expected.&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Fri, 20 Sep 2024 10:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Testing-802-1-Qav-on-ls1028a-switch/m-p/1958724#M14904</guid>
      <dc:creator>_mkl</dc:creator>
      <dc:date>2024-09-20T10:26:39Z</dc:date>
    </item>
  </channel>
</rss>