<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Add RS485 mode on ls1028 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Add-RS485-mode-on-ls1028/m-p/1958200#M14901</link>
    <description>&lt;P&gt;Hi：&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How do I configure Duart to operate in half-duplex RS485 mode? Currently, I am using the duart1 port, and the default configuration is as follows:&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;      duart1: serial@21c0600 {
                        compatible = "fsl,ns16550", "ns16550a";
                        reg = &amp;lt;0x00 0x21c0600 0x0 0x100&amp;gt;;
                        interrupts = &amp;lt;GIC_SPI 32 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
                        clocks = &amp;lt;&amp;amp;clockgen 4 1&amp;gt;;
                        status = "disabled";
                };&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 20 Sep 2024 02:16:35 GMT</pubDate>
    <dc:creator>Eddy1</dc:creator>
    <dc:date>2024-09-20T02:16:35Z</dc:date>
    <item>
      <title>Add RS485 mode on ls1028</title>
      <link>https://community.nxp.com/t5/Layerscape/Add-RS485-mode-on-ls1028/m-p/1958200#M14901</link>
      <description>&lt;P&gt;Hi：&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;How do I configure Duart to operate in half-duplex RS485 mode? Currently, I am using the duart1 port, and the default configuration is as follows:&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;      duart1: serial@21c0600 {
                        compatible = "fsl,ns16550", "ns16550a";
                        reg = &amp;lt;0x00 0x21c0600 0x0 0x100&amp;gt;;
                        interrupts = &amp;lt;GIC_SPI 32 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
                        clocks = &amp;lt;&amp;amp;clockgen 4 1&amp;gt;;
                        status = "disabled";
                };&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Sep 2024 02:16:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Add-RS485-mode-on-ls1028/m-p/1958200#M14901</guid>
      <dc:creator>Eddy1</dc:creator>
      <dc:date>2024-09-20T02:16:35Z</dc:date>
    </item>
    <item>
      <title>Re: Add RS485 mode on ls1028</title>
      <link>https://community.nxp.com/t5/Layerscape/Add-RS485-mode-on-ls1028/m-p/1959336#M14909</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;First, you should confirm the customer HW mode of UART in RS485.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;If the direction of the RS485 is controlled by the extra signal, you should add it in the DTS, and modify the SW driver.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;If the direction of the RS485 is controlled by the RTS, I don't think it needs extra modification.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Sep 2024 01:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Add-RS485-mode-on-ls1028/m-p/1959336#M14909</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2024-09-23T01:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: Add RS485 mode on ls1028</title>
      <link>https://community.nxp.com/t5/Layerscape/Add-RS485-mode-on-ls1028/m-p/1961174#M14918</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi：&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thank you for your reply. I have modified the SW driver, and it can now send and receive&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Sep 2024 01:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Add-RS485-mode-on-ls1028/m-p/1961174#M14918</guid>
      <dc:creator>Eddy1</dc:creator>
      <dc:date>2024-09-25T01:41:31Z</dc:date>
    </item>
  </channel>
</rss>