<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Custom board based on LS1028 DDR Bring-up procedure guide</title>
    <link>https://community.nxp.com/t5/Layerscape/Custom-board-based-on-LS1028-DDR-Bring-up-procedure-guide/m-p/1952203#M14869</link>
    <description>regarding your questions:&lt;BR /&gt;Each platform needs to define a function _init_ddr which is in a board-specific file, &lt;BR /&gt;The _init_ddr function calls dram_init which calls the NXP DDR drivers initialization/training routine.&lt;BR /&gt;This function can also be used to apply DDR errata, which needs to be applied post DDR configuration.&lt;BR /&gt;It is the same concept for LX2 platforms but they use a binary image file according to the TFA version.&lt;BR /&gt;</description>
    <pubDate>Wed, 11 Sep 2024 14:38:57 GMT</pubDate>
    <dc:creator>LFGP</dc:creator>
    <dc:date>2024-09-11T14:38:57Z</dc:date>
    <item>
      <title>Custom board based on LS1028 DDR Bring-up procedure guide</title>
      <link>https://community.nxp.com/t5/Layerscape/Custom-board-based-on-LS1028-DDR-Bring-up-procedure-guide/m-p/1950919#M14863</link>
      <description>&lt;P&gt;Hi, is there any guide on how to bring up custom DDR memory on LS1028A SoC based device?&lt;/P&gt;&lt;P&gt;I was googling but haven't found anything related to LS1028A. One more question - why does LX2160a NXP need something like fip-ddr? What's the purpose of this? Is it used to DDR training phase? Is it required on LS1028A?&lt;/P&gt;</description>
      <pubDate>Tue, 10 Sep 2024 09:18:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Custom-board-based-on-LS1028-DDR-Bring-up-procedure-guide/m-p/1950919#M14863</guid>
      <dc:creator>pb3</dc:creator>
      <dc:date>2024-09-10T09:18:08Z</dc:date>
    </item>
    <item>
      <title>Re: Custom board based on LS1028 DDR Bring-up procedure guide</title>
      <link>https://community.nxp.com/t5/Layerscape/Custom-board-based-on-LS1028-DDR-Bring-up-procedure-guide/m-p/1952186#M14868</link>
      <description>&lt;P&gt;Dear Patryk,&lt;/P&gt;
&lt;P&gt;You could manually modify the ddr_init.c file , please read the chapter " &lt;SPAN class="fontstyle0"&gt;4.2.1.1 TF-A DDR Driver&lt;/SPAN&gt;" into the LLDP_6.1.55 user guide,&lt;/P&gt;
&lt;P&gt;or you could use QCVS tool to get the respected file, please follow to the next link&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/QCVS_DDR_User_Guide.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/QCVS_DDR_User_Guide.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Sep 2024 14:26:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Custom-board-based-on-LS1028-DDR-Bring-up-procedure-guide/m-p/1952186#M14868</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2024-09-11T14:26:34Z</dc:date>
    </item>
    <item>
      <title>Re: Custom board based on LS1028 DDR Bring-up procedure guide</title>
      <link>https://community.nxp.com/t5/Layerscape/Custom-board-based-on-LS1028-DDR-Bring-up-procedure-guide/m-p/1952203#M14869</link>
      <description>regarding your questions:&lt;BR /&gt;Each platform needs to define a function _init_ddr which is in a board-specific file, &lt;BR /&gt;The _init_ddr function calls dram_init which calls the NXP DDR drivers initialization/training routine.&lt;BR /&gt;This function can also be used to apply DDR errata, which needs to be applied post DDR configuration.&lt;BR /&gt;It is the same concept for LX2 platforms but they use a binary image file according to the TFA version.&lt;BR /&gt;</description>
      <pubDate>Wed, 11 Sep 2024 14:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Custom-board-based-on-LS1028-DDR-Bring-up-procedure-guide/m-p/1952203#M14869</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2024-09-11T14:38:57Z</dc:date>
    </item>
  </channel>
</rss>