<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 25G Link Detection Issue on LA1224-RDB-BLS with LX2160ARDB Rev2 Image in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/25G-Link-Detection-Issue-on-LA1224-RDB-BLS-with-LX2160ARDB-Rev2/m-p/1941039#M14824</link>
    <description>&lt;P&gt;Same reply, LX2160ARDB-rev2 and&amp;nbsp; LA1224-RDB-B, the Retimers on the both boards are different, Inphi IN112525 on the LX2160ARDB-rev2, and TI “DS250DF230" on the LA1224-RDB-B. The driver would be different.&lt;/P&gt;
&lt;P&gt;If you use LSDK LX2160ARDB-rve2 on the LA1224-RDB-B, it could not work.&lt;/P&gt;
&lt;P&gt;Please use the LA1224 SDK on the LA1224-RDB-B to realize your development, if you don't have SW source in hand, please contact NXP local support for the LA1224-RDB-B.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;A href="https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS#INDIA" target="_blank"&gt;https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS#INDIA&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;LSDK2108 could not support LA1224-RDB-B.&lt;/P&gt;</description>
    <pubDate>Tue, 27 Aug 2024 07:39:51 GMT</pubDate>
    <dc:creator>June_Lu</dc:creator>
    <dc:date>2024-08-27T07:39:51Z</dc:date>
    <item>
      <title>25G Link Detection Issue on LA1224-RDB-BLS with LX2160ARDB Rev2 Image</title>
      <link>https://community.nxp.com/t5/Layerscape/25G-Link-Detection-Issue-on-LA1224-RDB-BLS-with-LX2160ARDB-Rev2/m-p/1940390#M14819</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;BR /&gt;&lt;BR /&gt;I would like to provide an update regarding the issue we’re facing with the 25G link detection on the LA1224-RDB-BLS board.&lt;/P&gt;&lt;H3&gt;Current Status:&lt;/H3&gt;&lt;P&gt;&lt;STRONG&gt;Working Configuration&lt;/STRONG&gt;: Our custom image, based on the LSDK21.08, is working correctly on the LX2160ARDB board, including 25G link detection. The interfaces are coming up as expected, and we can establish a connection without issues.&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;NXP Provided Image&lt;/STRONG&gt;: The NXP-provided image for the LA1224RDB-BLS board works fine, including 25G link functionality, which suggests that the hardware is in good condition and capable of supporting the 25G link.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Problematic Configuration&lt;/STRONG&gt;: However, when using the same custom image with a basic SDK bring-up of the LX2160ARDB Rev2 build on the LA1224-RDB-BLS board, the 25G link does not come up. The interface mapping appears correct, but we are unable to establish a connection, and the link remains inactive.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="harisankar2001_0-1724672219744.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/295296i2A01C78E6FE6C71C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="harisankar2001_0-1724672219744.png" alt="harisankar2001_0-1724672219744.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;harisankar2001_0-1724672219744.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Are there any specific configurations or errata that need to be applied for the LA1224RDB-BLS board when using an image built for the LX2160ARDB Rev2?&lt;BR /&gt;&lt;BR /&gt;Your expertise and guidance in resolving this issue would be greatly appreciated, as it is critical for our project timeline.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Aug 2024 11:48:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/25G-Link-Detection-Issue-on-LA1224-RDB-BLS-with-LX2160ARDB-Rev2/m-p/1940390#M14819</guid>
      <dc:creator>harisankar2001</dc:creator>
      <dc:date>2024-08-26T11:48:14Z</dc:date>
    </item>
    <item>
      <title>Re: 25G Link Detection Issue on LA1224-RDB-BLS with LX2160ARDB Rev2 Image</title>
      <link>https://community.nxp.com/t5/Layerscape/25G-Link-Detection-Issue-on-LA1224-RDB-BLS-with-LX2160ARDB-Rev2/m-p/1941039#M14824</link>
      <description>&lt;P&gt;Same reply, LX2160ARDB-rev2 and&amp;nbsp; LA1224-RDB-B, the Retimers on the both boards are different, Inphi IN112525 on the LX2160ARDB-rev2, and TI “DS250DF230" on the LA1224-RDB-B. The driver would be different.&lt;/P&gt;
&lt;P&gt;If you use LSDK LX2160ARDB-rve2 on the LA1224-RDB-B, it could not work.&lt;/P&gt;
&lt;P&gt;Please use the LA1224 SDK on the LA1224-RDB-B to realize your development, if you don't have SW source in hand, please contact NXP local support for the LA1224-RDB-B.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;A href="https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS#INDIA" target="_blank"&gt;https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS#INDIA&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;LSDK2108 could not support LA1224-RDB-B.&lt;/P&gt;</description>
      <pubDate>Tue, 27 Aug 2024 07:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/25G-Link-Detection-Issue-on-LA1224-RDB-BLS-with-LX2160ARDB-Rev2/m-p/1941039#M14824</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2024-08-27T07:39:51Z</dc:date>
    </item>
  </channel>
</rss>