<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックMini PCIe not detected on LS1043ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1930966#M14731</link>
    <description>&lt;P&gt;I have been unable to resolve the issue I posted &lt;A href="https://support.nxp.com/s/case/5002p00002zpFsh/sierra-wireless-airprime-on-minipcie-connector?tabset-d5929500=2" target="_self"&gt;here&lt;/A&gt;. Trying to use Sierra Modem EM9191 (also Telit FN990A) on&amp;nbsp;LS1043ARDB.&lt;/P&gt;&lt;P&gt;Using M.2 to Mini PCIe adapter board (&lt;A href="https://techship.com/product/techship-4g-5g-m2-key-b-to-mpcie-usb2-pcie/?variant=002" target="_self"&gt;Techship MP301-ES&lt;/A&gt;) and u-boot does not detect the device on the PCI bus (see console output below).&lt;/P&gt;&lt;P&gt;I can successfully detect and run WiFi module 920NGW on this PCI bus (of course with different adapter board)&lt;/P&gt;&lt;P&gt;Please let me know if this is expected to work with the default configuration of nxp-qoriq build or if there are any changes that I can try on the configuration (e.g. RCW).&lt;/P&gt;&lt;P&gt;----------------&lt;/P&gt;&lt;P&gt;Using SERDES1 Protocol: 5205 (0x1455)&lt;BR /&gt;PCIe1: pcie@3400000 disabled&lt;BR /&gt;PCIe2: pcie@3500000 Root Complex: no link&lt;BR /&gt;PCIe3: pcie@3600000 Root Complex: no link&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Tue, 13 Aug 2024 08:47:08 GMT</pubDate>
    <dc:creator>mehdi-cubic</dc:creator>
    <dc:date>2024-08-13T08:47:08Z</dc:date>
    <item>
      <title>Mini PCIe not detected on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1930966#M14731</link>
      <description>&lt;P&gt;I have been unable to resolve the issue I posted &lt;A href="https://support.nxp.com/s/case/5002p00002zpFsh/sierra-wireless-airprime-on-minipcie-connector?tabset-d5929500=2" target="_self"&gt;here&lt;/A&gt;. Trying to use Sierra Modem EM9191 (also Telit FN990A) on&amp;nbsp;LS1043ARDB.&lt;/P&gt;&lt;P&gt;Using M.2 to Mini PCIe adapter board (&lt;A href="https://techship.com/product/techship-4g-5g-m2-key-b-to-mpcie-usb2-pcie/?variant=002" target="_self"&gt;Techship MP301-ES&lt;/A&gt;) and u-boot does not detect the device on the PCI bus (see console output below).&lt;/P&gt;&lt;P&gt;I can successfully detect and run WiFi module 920NGW on this PCI bus (of course with different adapter board)&lt;/P&gt;&lt;P&gt;Please let me know if this is expected to work with the default configuration of nxp-qoriq build or if there are any changes that I can try on the configuration (e.g. RCW).&lt;/P&gt;&lt;P&gt;----------------&lt;/P&gt;&lt;P&gt;Using SERDES1 Protocol: 5205 (0x1455)&lt;BR /&gt;PCIe1: pcie@3400000 disabled&lt;BR /&gt;PCIe2: pcie@3500000 Root Complex: no link&lt;BR /&gt;PCIe3: pcie@3600000 Root Complex: no link&lt;/P&gt;&lt;P&gt;------------------&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Aug 2024 08:47:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1930966#M14731</guid>
      <dc:creator>mehdi-cubic</dc:creator>
      <dc:date>2024-08-13T08:47:08Z</dc:date>
    </item>
    <item>
      <title>Re: Mini PCIe not detected on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1933509#M14752</link>
      <description>&lt;P&gt;Discussing with the AE team.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Aug 2024 07:48:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1933509#M14752</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-08-16T07:48:01Z</dc:date>
    </item>
    <item>
      <title>Re: Mini PCIe not detected on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1936220#M14778</link>
      <description>&lt;P&gt;I assume there has been no progress on this topic?&lt;/P&gt;</description>
      <pubDate>Tue, 20 Aug 2024 11:08:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1936220#M14778</guid>
      <dc:creator>mehdi-cubic</dc:creator>
      <dc:date>2024-08-20T11:08:07Z</dc:date>
    </item>
    <item>
      <title>Re: Mini PCIe not detected on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1937050#M14785</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Can you check and tell us the PCIe LTSSM state[from PCI Express Link Control Register] at Uboot when you are connecting the Telit FN990A via M.2 to Mini PCIe adapter board ?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Aug 2024 06:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1937050#M14785</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-08-21T06:39:22Z</dc:date>
    </item>
    <item>
      <title>Re: Mini PCIe not detected on LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1937385#M14791</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;Thanks for the update.&amp;nbsp;&lt;BR /&gt;Yes sure, I will extract the value in this register and post it ASAP.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Aug 2024 11:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Mini-PCIe-not-detected-on-LS1043ARDB/m-p/1937385#M14791</guid>
      <dc:creator>mehdi-cubic</dc:creator>
      <dc:date>2024-08-21T11:12:52Z</dc:date>
    </item>
  </channel>
</rss>