<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピックls1027 reduce static power consumption</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1027-reduce-static-power-consumption/m-p/1930126#M14725</link>
    <description>&lt;P&gt;Our LS1027A board is using way more static power than we anticipated. The LS1027A is using about 4W of static power when idle.&lt;/P&gt;&lt;P&gt;The CPU frequency is lowered to 300MHz and Linux is entering the low-power states, as we can see in /sys/devices/cpu...&lt;/P&gt;&lt;P&gt;Changing the frequency (while idle) to 1500 MHz doesn't have much effect on the power consumption (about 30mW or so), which, to me, confirms that the low-power WFI states are doing their work.&lt;/P&gt;&lt;P&gt;We have no clue where the LS1027A is spending all this static power.&lt;/P&gt;&lt;P&gt;We're not using the networking components. We disabled everything we're not using in the device-tree.&lt;/P&gt;&lt;P&gt;I also tried disabling more of the network components by setting "ENETC_RCW=0" in the RCW, but saw no noticable effect.&lt;/P&gt;&lt;P&gt;Putting the CPU in suspend-to-RAM mode reduced the power a bit, but still about 3W remains, which is excessively large (compared to other systems I've worked with, where the CPU would go far below 1W while suspended).&lt;/P&gt;&lt;P&gt;What's using all that static power? And how can we diagnose and reduce it?&lt;/P&gt;</description>
    <pubDate>Mon, 12 Aug 2024 10:05:19 GMT</pubDate>
    <dc:creator>mikelooijmans</dc:creator>
    <dc:date>2024-08-12T10:05:19Z</dc:date>
    <item>
      <title>ls1027 reduce static power consumption</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1027-reduce-static-power-consumption/m-p/1930126#M14725</link>
      <description>&lt;P&gt;Our LS1027A board is using way more static power than we anticipated. The LS1027A is using about 4W of static power when idle.&lt;/P&gt;&lt;P&gt;The CPU frequency is lowered to 300MHz and Linux is entering the low-power states, as we can see in /sys/devices/cpu...&lt;/P&gt;&lt;P&gt;Changing the frequency (while idle) to 1500 MHz doesn't have much effect on the power consumption (about 30mW or so), which, to me, confirms that the low-power WFI states are doing their work.&lt;/P&gt;&lt;P&gt;We have no clue where the LS1027A is spending all this static power.&lt;/P&gt;&lt;P&gt;We're not using the networking components. We disabled everything we're not using in the device-tree.&lt;/P&gt;&lt;P&gt;I also tried disabling more of the network components by setting "ENETC_RCW=0" in the RCW, but saw no noticable effect.&lt;/P&gt;&lt;P&gt;Putting the CPU in suspend-to-RAM mode reduced the power a bit, but still about 3W remains, which is excessively large (compared to other systems I've worked with, where the CPU would go far below 1W while suspended).&lt;/P&gt;&lt;P&gt;What's using all that static power? And how can we diagnose and reduce it?&lt;/P&gt;</description>
      <pubDate>Mon, 12 Aug 2024 10:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1027-reduce-static-power-consumption/m-p/1930126#M14725</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-08-12T10:05:19Z</dc:date>
    </item>
    <item>
      <title>Re: ls1027 reduce static power consumption</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1027-reduce-static-power-consumption/m-p/1938990#M14815</link>
      <description>&lt;P&gt;A significant amount is used by the PCIe interfaces - we're using 2x 2 lane Gen3.&lt;/P&gt;&lt;P&gt;It seems that the LS1027 doesn't support PCI link power states, is that correct or is there something we should do to enable that?&lt;/P&gt;</description>
      <pubDate>Fri, 23 Aug 2024 05:59:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1027-reduce-static-power-consumption/m-p/1938990#M14815</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-08-23T05:59:18Z</dc:date>
    </item>
    <item>
      <title>Re: ls1027 reduce static power consumption</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1027-reduce-static-power-consumption/m-p/1940781#M14820</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;A significant amount is used by the PCIe interfaces - we're using 2x 2 lane Gen3.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;SPAN&gt;How do you test&lt;/SPAN&gt;&lt;SPAN&gt; and ananyse&lt;/SPAN&gt;&lt;SPAN&gt; the PCIe interfaces power consumption?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Thanks&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Aug 2024 01:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1027-reduce-static-power-consumption/m-p/1940781#M14820</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2024-08-27T01:39:45Z</dc:date>
    </item>
  </channel>
</rss>