<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1027A Cannot reboot</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928093#M14718</link>
    <description>&lt;P&gt;We did some more digging with the scope.&lt;/P&gt;&lt;P&gt;On the LS1028ARDB, the RESET_nREQ pin goes to an FPGA. On our board it only has a o pull-up as the datasheet suggested.&lt;/P&gt;&lt;P&gt;When I attempt to reboot, the RESET_nREQ asserts low and nothing else happens.&lt;/P&gt;&lt;P&gt;On the LS1028ARDB, the RESET_nREQ asserts low and then the FPGA pulls the nPORESET low, which causes the reboot.&lt;/P&gt;&lt;P&gt;So we attempted the obvious and tied these two pins together. This caused the board to no longer boot at all.&lt;/P&gt;&lt;P&gt;Next thing we tried was route the RESET_nREQ to an input of the power-supply monitor chip that controls the nPORESET signal, so that when RESET_nREQ asserts, the monitor chip will assert the nPORESET signal for several milliseconds.&lt;/P&gt;&lt;P&gt;This appears to work in our testing.&lt;/P&gt;&lt;P&gt;Question to NXP engineers is now, is this how it's supposed to work?&lt;/P&gt;&lt;P&gt;Is the maybe some application note on this reset signal that explains how these signals are supposed to work? The datasheet is rather vague about it.&lt;/P&gt;</description>
    <pubDate>Thu, 08 Aug 2024 08:45:26 GMT</pubDate>
    <dc:creator>mikelooijmans</dc:creator>
    <dc:date>2024-08-08T08:45:26Z</dc:date>
    <item>
      <title>LS1027A Cannot reboot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1927282#M14707</link>
      <description>&lt;P&gt;We have a custom board with LS1027A CPU on it.&lt;/P&gt;&lt;P&gt;When I attempt to reboot the board from Linux, the system doesn't actually reboot, all it does is write this on the serial terminal and then hangs:&lt;/P&gt;&lt;P&gt;reboot: Restarting system&lt;BR /&gt;Unable to restart system&lt;/P&gt;&lt;P&gt;Out board looks so much like the LS1028ARDB board, it will actually boot the same image, and on that board, the reset works as expected.&lt;/P&gt;&lt;P&gt;Same issue with u-boot, if I type "reset", nothing happens and the prompt just returns.&lt;/P&gt;&lt;P&gt;What did we miss?&lt;/P&gt;</description>
      <pubDate>Wed, 07 Aug 2024 10:14:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1927282#M14707</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-08-07T10:14:19Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A Cannot reboot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928055#M14716</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Would you kindly share the logs? Both Linux and U-Boot.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 08 Aug 2024 07:59:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928055#M14716</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2024-08-08T07:59:08Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A Cannot reboot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928089#M14717</link>
      <description>&lt;P&gt;What logs are you referring to?&lt;/P&gt;&lt;P&gt;u-boot doesn't output anything (when I type "reset").&lt;/P&gt;&lt;P&gt;Kernel only outputs those two lines.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Aug 2024 08:38:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928089#M14717</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-08-08T08:38:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A Cannot reboot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928093#M14718</link>
      <description>&lt;P&gt;We did some more digging with the scope.&lt;/P&gt;&lt;P&gt;On the LS1028ARDB, the RESET_nREQ pin goes to an FPGA. On our board it only has a o pull-up as the datasheet suggested.&lt;/P&gt;&lt;P&gt;When I attempt to reboot, the RESET_nREQ asserts low and nothing else happens.&lt;/P&gt;&lt;P&gt;On the LS1028ARDB, the RESET_nREQ asserts low and then the FPGA pulls the nPORESET low, which causes the reboot.&lt;/P&gt;&lt;P&gt;So we attempted the obvious and tied these two pins together. This caused the board to no longer boot at all.&lt;/P&gt;&lt;P&gt;Next thing we tried was route the RESET_nREQ to an input of the power-supply monitor chip that controls the nPORESET signal, so that when RESET_nREQ asserts, the monitor chip will assert the nPORESET signal for several milliseconds.&lt;/P&gt;&lt;P&gt;This appears to work in our testing.&lt;/P&gt;&lt;P&gt;Question to NXP engineers is now, is this how it's supposed to work?&lt;/P&gt;&lt;P&gt;Is the maybe some application note on this reset signal that explains how these signals are supposed to work? The datasheet is rather vague about it.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Aug 2024 08:45:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928093#M14718</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-08-08T08:45:26Z</dc:date>
    </item>
    <item>
      <title>Re: LS1027A Cannot reboot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928804#M14720</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;SPAN&gt;You could refer to &lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LS1028ARM" target="_blank"&gt;&lt;SPAN&gt;LS1028A Reference Manual&lt;/SPAN&gt;&lt;/A&gt;&lt;SPAN&gt; and &lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN12028&amp;amp;location=null" target="_blank"&gt;&lt;SPAN&gt;AN12028_QorIQ LS1028A Design Checklist&lt;/SPAN&gt;&lt;/A&gt;&lt;SPAN&gt; for the RESET_REQ_B detail information.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Once asserted, RESET_REQ_B does not negate until PORESET_B is asserted.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;SPAN&gt;But another thing need to confirm, when assert PORESET_B, please follow &lt;/SPAN&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LS1028A" target="_blank"&gt;&lt;SPAN&gt;LS1028A/LS1018A Data Sheet&lt;/SPAN&gt;&lt;/A&gt;&lt;SPAN&gt;, page 75, &lt;/SPAN&gt;&lt;SPAN&gt;Table 13. RESET initialization timing specifications&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;So when connect them directly, please confirm the different conditions.&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 09 Aug 2024 04:34:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1027A-Cannot-reboot/m-p/1928804#M14720</guid>
      <dc:creator>June_Lu</dc:creator>
      <dc:date>2024-08-09T04:34:44Z</dc:date>
    </item>
  </channel>
</rss>