<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LX2160 DDR training fail ISSUE in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160-DDR-training-fail-ISSUE/m-p/1923220#M14674</link>
    <description>&lt;P&gt;Hi have the similar issue.&lt;/P&gt;&lt;P&gt;Where I have to add these parameters?&lt;/P&gt;&lt;P&gt;Are you using LSDK for building the images or any other method?&lt;/P&gt;&lt;P&gt;Also, which all files I need to modify for DDR configurations?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 01 Aug 2024 16:54:43 GMT</pubDate>
    <dc:creator>Nikhiln</dc:creator>
    <dc:date>2024-08-01T16:54:43Z</dc:date>
    <item>
      <title>LX2160 DDR training fail ISSUE</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160-DDR-training-fail-ISSUE/m-p/1852197#M14205</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;We produce a board using LX2160&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;DDR CONTROLLER1: 4*16 + 1*16(ECC), all there ddr_module share one CS &amp;amp; CKE&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;CONTROLLER2: 4*16 + 1*16(ECC), all there ddr_module share one CS &amp;amp; CKE&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;DDR PLL freq is 3200MHz &amp;amp; DDR freq is 1600MHz&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;From bl2 log, it seems that ddr training is fail&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Is there anything I should check?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=13&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=13 and input nod=30&lt;BR /&gt;INFO: Index = 1 with loc_nod=30 and input nod=30&lt;BR /&gt;INFO: Index = 0 with loc_nod=4 and input nod=17&lt;BR /&gt;INFO: Index = 1 with loc_nod=7 and input nod=17&lt;BR /&gt;INFO: Index = 2 with loc_nod=10 and input nod=17&lt;BR /&gt;INFO: Index = 3 with loc_nod=17 and input nod=17&lt;BR /&gt;INFO: Index = 0 with loc_nod=4 and input nod=17&lt;BR /&gt;INFO: Index = 1 with loc_nod=7 and input nod=17&lt;BR /&gt;INFO: Index = 2 with loc_nod=10 and input nod=17&lt;BR /&gt;INFO: Index = 3 with loc_nod=17 and input nod=17&lt;BR /&gt;INFO: RCW BOOT SRC is SD&lt;BR /&gt;INFO: SoC workaround for Errata A050426 was applied&lt;BR /&gt;INFO: SoC workaround for DDR Errata A011396 was applied&lt;BR /&gt;INFO: SoC workaround for DDR Errata A050450 was applied&lt;BR /&gt;INFO: SoC workaround for DDR Errata A050958 was applied&lt;BR /&gt;INFO: RCW BOOT SRC is SD&lt;BR /&gt;INFO: esdhc_emmc_init&lt;BR /&gt;INFO: Card detected successfully&lt;BR /&gt;INFO: init done:&lt;BR /&gt;INFO: Flexspi driver: Version v1.0&lt;BR /&gt;INFO: Flexspi: Default MCR0 = 0xffff80c0, before reset&lt;BR /&gt;INFO: Flexspi: After MCR0 = 0xffff0000,&lt;BR /&gt;INFO: Flexspi: Init done!!&lt;BR /&gt;INFO: F_SECTOR_ERASE_SZ: 0x00020000, num_sector: 1&lt;BR /&gt;INFO: In [fspi_sec_er][755] Erase address 0xc0000&lt;BR /&gt;NOTICE: BL2: v2.4(release):LSDK-21.08-1-g3875a8de3-dirty&lt;BR /&gt;NOTICE: BL2: Built : 14:09:43, Apr 23 2024&lt;BR /&gt;INFO: platform clock 750000000&lt;BR /&gt;INFO: DDR PLL1 3200000000&lt;BR /&gt;INFO: DDR PLL2 3200000000&lt;BR /&gt;INFO: frequency = 1600MHz&lt;BR /&gt;INFO: Vref_phy = 75 percent&lt;BR /&gt;INFO: Initializing input adv data structure&lt;BR /&gt;INFO: mr[0] = 0x210&lt;BR /&gt;INFO: mr[1] = 0x101&lt;BR /&gt;INFO: mr[2] = 0x0&lt;BR /&gt;INFO: mr[3] = 0x0&lt;BR /&gt;INFO: mr[4] = 0x0&lt;BR /&gt;INFO: mr[5] = 0x0&lt;BR /&gt;INFO: mr[6] = 0x0&lt;BR /&gt;INFO: input-&amp;gt;cs_d0 = 0x3&lt;BR /&gt;INFO: input-&amp;gt;cs_d1 = 0x0&lt;BR /&gt;INFO: input-&amp;gt;mirror = 0x0&lt;BR /&gt;INFO: PHY ODT impedance = 48 ohm&lt;BR /&gt;INFO: PHY DQ driver impedance = 48 ohm&lt;BR /&gt;INFO: PHY Addr driver impedance = 30 ohm&lt;BR /&gt;INFO: odt[0] = 0x1&lt;BR /&gt;INFO: odt[1] = 0x2&lt;BR /&gt;INFO: odt[2] = 0x0&lt;BR /&gt;INFO: odt[3] = 0x0&lt;BR /&gt;INFO: Initializing message block&lt;BR /&gt;INFO: msg_blk-&amp;gt;dram_type = 0x2&lt;BR /&gt;INFO: msg_blk-&amp;gt;sequence_ctrl = 0x31f&lt;BR /&gt;INFO: msg_blk-&amp;gt;phy_cfg = 0x0&lt;BR /&gt;INFO: msg_blk-&amp;gt;x16present = 0x3&lt;BR /&gt;INFO: msg_blk-&amp;gt;dramfreq = 0xc80&lt;BR /&gt;INFO: msg_blk-&amp;gt;pll_bypass_en = 0x0&lt;BR /&gt;INFO: msg_blk-&amp;gt;dfi_freq_ratio = 0x2&lt;BR /&gt;INFO: msg_blk-&amp;gt;phy_odt_impedance = 0x0&lt;BR /&gt;INFO: msg_blk-&amp;gt;phy_drv_impedance = 0x0&lt;BR /&gt;INFO: msg_blk-&amp;gt;bpznres_val = 0x0&lt;BR /&gt;INFO: msg_blk-&amp;gt;enabled_dqs = 0x40&lt;BR /&gt;INFO: msg_blk-&amp;gt;acsm_odt_ctrl0 = 0x1&lt;BR /&gt;INFO: msg_blk-&amp;gt;acsm_odt_ctrl1 = 0x2&lt;BR /&gt;INFO: msg_blk-&amp;gt;acsm_odt_ctrl2 = 0x0&lt;BR /&gt;INFO: msg_blk-&amp;gt;acsm_odt_ctrl3 = 0x0&lt;BR /&gt;INFO: rx2d_train_opt 0, tx2d_train_opt 0&lt;BR /&gt;INFO: Initialize PHY 0 config&lt;BR /&gt;INFO: pll_ctrl2 = 0x19&lt;BR /&gt;INFO: SOC_SI_REV = 2&lt;BR /&gt;INFO: dll_lck_param = 0x212&lt;BR /&gt;INFO: dll_gain_ctl = 0x61&lt;BR /&gt;INFO: prog_acx4_anib_dis 0x0&lt;BR /&gt;INFO: Initialize PHY 1 config&lt;BR /&gt;INFO: pll_ctrl2 = 0x19&lt;BR /&gt;INFO: SOC_SI_REV = 2&lt;BR /&gt;INFO: dll_lck_param = 0x212&lt;BR /&gt;INFO: dll_gain_ctl = 0x61&lt;BR /&gt;INFO: prog_acx4_anib_dis 0x0&lt;BR /&gt;NOTICE: DDR PMU Hardware version-0x1210&lt;BR /&gt;INFO: Load 1D firmware&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: Loading image id=33 at address 0x18003000&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: Image id=33 loaded: 0x18003000 - 0x18009bd0&lt;BR /&gt;INFO: Loaded Imaged id 33 of size 6bd0 at address 18003000&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: Loading image id=35 at address 0x18003000&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: Image id=35 loaded: 0x18003000 - 0x180036d0&lt;BR /&gt;INFO: Loaded Imaged id 35 of size 6d0 at address 18003000&lt;BR /&gt;INFO: Execute firmware&lt;BR /&gt;INFO: Applying PLL optimal settings&lt;BR /&gt;INFO: pll_ctrl2 = 0x19&lt;BR /&gt;INFO: pll_ctrl1 = 0x21&lt;BR /&gt;INFO: pll_test_mode = 0x24&lt;BR /&gt;INFO: pll_ctrl4 = 0x17f&lt;BR /&gt;NOTICE: DDR PMU Firmware vision-0x1001 (vA-2019.04)&lt;BR /&gt;INFO: End of initialization&lt;BR /&gt;INFO: End of read enable training&lt;BR /&gt;INFO: End of fine write leveling&lt;BR /&gt;INFO: 1D Training failure&lt;BR /&gt;INFO: Applying PLL optimal settings&lt;BR /&gt;INFO: pll_ctrl2 = 0x19&lt;BR /&gt;INFO: pll_ctrl1 = 0x21&lt;BR /&gt;INFO: pll_test_mode = 0x24&lt;BR /&gt;INFO: pll_ctrl4 = 0x17f&lt;BR /&gt;INFO: End of initialization&lt;BR /&gt;INFO: 1D Training failure&lt;BR /&gt;ERROR: Execution FW failed (error code -5)&lt;BR /&gt;Error - Invalid cs_in_use value&lt;BR /&gt;INFO: CDD rrmax 7 wwmax 7 rwmax f wrmax 7&lt;BR /&gt;INFO: Time before programming controller 357 ms&lt;BR /&gt;INFO: Program controller registers&lt;BR /&gt;PHY handshake timeout, ddr_dsr2 = 0&lt;BR /&gt;INFO: total size 16 GB&lt;BR /&gt;INFO: Need to wait up to 2680 ms&lt;BR /&gt;ERROR: Found training error(s): 0x100&lt;BR /&gt;ERROR: Error: Waiting for D_INIT timeout.&lt;BR /&gt;ERROR: Writing DDR register(s) failed&lt;BR /&gt;ERROR: Programing DDRC error&lt;BR /&gt;ERROR: DDR init failed.&lt;BR /&gt;NOTICE: Incorrect DRAM0 size is defined in platform_def.h&lt;BR /&gt;INFO: DDR Controller 1.&lt;BR /&gt;INFO: Configuring TrustZone Controller&lt;BR /&gt;INFO: Configuring TrustZone Controller&lt;BR /&gt;INFO: DDR Controller 2.&lt;BR /&gt;INFO: Configuring TrustZone Controller&lt;BR /&gt;INFO: Configuring TrustZone Controller&lt;BR /&gt;INFO: BL2: Doing platform setup&lt;BR /&gt;INFO: BL2: Loading image id 3&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: sd-mmc read done.&lt;BR /&gt;INFO: Loading image id=3 at address 0xfbe00000&lt;BR /&gt;INFO: sd-mmc read done.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 07:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160-DDR-training-fail-ISSUE/m-p/1852197#M14205</guid>
      <dc:creator>zeeetor</dc:creator>
      <dc:date>2024-04-23T07:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160 DDR training fail ISSUE</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160-DDR-training-fail-ISSUE/m-p/1852883#M14211</link>
      <description>&lt;P&gt;Problem solved!&lt;/P&gt;&lt;P&gt;CONFIG_STATIC_DDR = 0&lt;/P&gt;&lt;P&gt;CONFIG_DDR_NODIMM = 1&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Fill in&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;ddr_raw_timing with parameters according to ddr spec.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Apr 2024 01:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160-DDR-training-fail-ISSUE/m-p/1852883#M14211</guid>
      <dc:creator>zeeetor</dc:creator>
      <dc:date>2024-04-24T01:26:53Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160 DDR training fail ISSUE</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160-DDR-training-fail-ISSUE/m-p/1923220#M14674</link>
      <description>&lt;P&gt;Hi have the similar issue.&lt;/P&gt;&lt;P&gt;Where I have to add these parameters?&lt;/P&gt;&lt;P&gt;Are you using LSDK for building the images or any other method?&lt;/P&gt;&lt;P&gt;Also, which all files I need to modify for DDR configurations?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 01 Aug 2024 16:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160-DDR-training-fail-ISSUE/m-p/1923220#M14674</guid>
      <dc:creator>Nikhiln</dc:creator>
      <dc:date>2024-08-01T16:54:43Z</dc:date>
    </item>
  </channel>
</rss>