<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021A USB 3.0 problem</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562323#M1464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ufedor"&gt;ufedor&lt;/A&gt;,&lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do I need some specific software settings? Should I use usb2.0 driver instead of the default usb3.0 driver?&lt;/P&gt;&lt;P&gt;I found there is something like "usb 2.0 only mode" in RM, but I cannot find any details.&lt;/P&gt;&lt;P&gt;The error from kernel log:&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 2 using xhci-hcd&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 2, error -71&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to set USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE] to 0 but it didn't change. Should I change some extra register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Jul 2016 20:17:40 GMT</pubDate>
    <dc:creator>hwei</dc:creator>
    <dc:date>2016-07-12T20:17:40Z</dc:date>
    <item>
      <title>LS1021A - USB 3.0 controller as USB 2.0 problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562321#M1462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a question about the USB3.0 controller.&lt;/P&gt;&lt;P&gt;Can I just connect the USB2.0 part &lt;SPAN style="text-decoration: underline;"&gt;(just USB1_D_M/P)&lt;/SPAN&gt;of the USB3.0 PHYs and treat the USB3.0 controller as an USB2.0 one? Is it a possible/right method?&lt;/P&gt;&lt;P&gt;We &lt;SPAN style="text-decoration: line-through;"&gt;follow&lt;/SPAN&gt; did some design like this and it seems the USB3.0 controller cannot work properly. Do I need any special setting to make it work as an USB2.0 controller?&lt;/P&gt;&lt;P&gt;It prompts:&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 2 using xhci-hcd&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 2, error -71&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 3 using xhci-hcd&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 3, error -71&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 15:45:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562321#M1462</guid>
      <dc:creator>hwei</dc:creator>
      <dc:date>2016-07-12T15:45:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A USB 3.0 problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562322#M1463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; We follow this and it seems the USB3.0 controller cannot work properly.&lt;/P&gt;&lt;P&gt;What you have done?&lt;/P&gt;&lt;P&gt;What are the results?&lt;/P&gt;&lt;P&gt;Is USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE]=0? (to disable the USB3 PHY)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 17:52:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562322#M1463</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-07-12T17:52:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A USB 3.0 problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562323#M1464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ufedor"&gt;ufedor&lt;/A&gt;,&lt;SPAN class="jive-comment-meta font-color-meta-light"&gt;&lt;SPAN class="j-username-wrap"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do I need some specific software settings? Should I use usb2.0 driver instead of the default usb3.0 driver?&lt;/P&gt;&lt;P&gt;I found there is something like "usb 2.0 only mode" in RM, but I cannot find any details.&lt;/P&gt;&lt;P&gt;The error from kernel log:&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 2 using xhci-hcd&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: Device not responding to set address.&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 2, error -71&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to set USB_GHWPARAMS3[DWC_USB3_SSPHY_INTERFACE] to 0 but it didn't change. Should I change some extra register?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jul 2016 20:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562323#M1464</guid>
      <dc:creator>hwei</dc:creator>
      <dc:date>2016-07-12T20:17:40Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A USB 3.0 problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562324#M1465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please check whether a USB 3.0 device is properly recognized in your system?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Jul 2016 04:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-USB-3-0-controller-as-USB-2-0-problem/m-p/562324#M1465</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-07-14T04:45:56Z</dc:date>
    </item>
  </channel>
</rss>