<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Yocto build vpp in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Yocto-build-vpp/m-p/1919515#M14628</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes&amp;nbsp; it is normal because is the dependencies of yocto and your apps. if you are in yocto, you have to build the whole package once it added to it.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
    <pubDate>Mon, 29 Jul 2024 14:36:26 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-07-29T14:36:26Z</dc:date>
    <item>
      <title>Yocto build vpp</title>
      <link>https://community.nxp.com/t5/Layerscape/Yocto-build-vpp/m-p/1919316#M14627</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I refer to section 8.3.4.2 of the LLDP_6.1.55_2.2.0 documentation for the build vpp，used command:bitbake vpp，a very large number of rpm packages related to vpp have been generated in the following folder。&lt;/P&gt;&lt;P&gt;1、is this normal?Because in lsdk21.08, vpp will only generate 9 relevant deb package files.&lt;/P&gt;&lt;P&gt;2、How do I install vpp?&lt;/P&gt;&lt;P&gt;/root/yocto/build_lx2160ardb-rev2/tmp/work/aarch64-fsl-linux/vpp/2302-r0/deploy-rpms/aarch64&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="stupid_0-1722246315024.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/290711iAEBB774929C6A806/image-size/medium?v=v2&amp;amp;px=400" alt="stupid_0-1722246315024.png" title="stupid_0-1722246315024.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jul 2024 09:58:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Yocto-build-vpp/m-p/1919316#M14627</guid>
      <dc:creator>Blue_Sky1</dc:creator>
      <dc:date>2024-07-29T09:58:46Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto build vpp</title>
      <link>https://community.nxp.com/t5/Layerscape/Yocto-build-vpp/m-p/1919515#M14628</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes&amp;nbsp; it is normal because is the dependencies of yocto and your apps. if you are in yocto, you have to build the whole package once it added to it.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jul 2024 14:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Yocto-build-vpp/m-p/1919515#M14628</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-07-29T14:36:26Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto build vpp</title>
      <link>https://community.nxp.com/t5/Layerscape/Yocto-build-vpp/m-p/1919872#M14630</link>
      <description>Hi,Bio_TICFSL&lt;BR /&gt;&lt;BR /&gt;Yes,i build vpp in yocto system,and i just run this command：bitbake vpp.&lt;BR /&gt;&lt;BR /&gt;How do I take the compiled vpp and install it on the lx2160?&lt;BR /&gt;&lt;BR /&gt;Thanks</description>
      <pubDate>Tue, 30 Jul 2024 01:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Yocto-build-vpp/m-p/1919872#M14630</guid>
      <dc:creator>Blue_Sky1</dc:creator>
      <dc:date>2024-07-30T01:48:44Z</dc:date>
    </item>
  </channel>
</rss>