<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LLDP pakcages maintenance problem based on LX2160ARDB?</title>
    <link>https://community.nxp.com/t5/Layerscape/LLDP-pakcages-maintenance-problem-based-on-LX2160ARDB/m-p/1908234#M14548</link>
    <description>&lt;P&gt;You are using Ubuntu images, therefore root file system update should be done based on Ubuntu package manager.&lt;/P&gt;
&lt;P&gt;IMAGE_INSTALL:append = " ..." should be used for packages that don't have Ubuntu equivalent, which is for example nxp repositories&lt;/P&gt;
&lt;P&gt;&amp;nbsp;APTGET_EXTRA_PACKAGES += "nvmi-cli" should be used for Ubuntu to install nvmi-cli based on apt-get install nvmi-cli.&lt;/P&gt;
&lt;P&gt;So, please only use&amp;nbsp;APTGET_EXTRA_PACKAGES to add packages in&amp;nbsp;&lt;SPAN&gt;ls-image-main rootfs.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jul 2024 03:39:03 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2024-07-15T03:39:03Z</dc:date>
    <item>
      <title>LLDP pakcages maintenance problem based on LX2160ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/LLDP-pakcages-maintenance-problem-based-on-LX2160ARDB/m-p/1903747#M14533</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We use LLDP 5.15.71 based on LX2160ardb platform&lt;/P&gt;&lt;P&gt;About&amp;nbsp; meta-nxp-deskop layer, it has below describe:&lt;/P&gt;&lt;P&gt;# Note that we have a tight dependency to ubuntu-main&lt;BR /&gt;# and that we cannot just install arbitrary Yocto packages to avoid&lt;BR /&gt;# rootfs pollution or destruction.&lt;/P&gt;&lt;P&gt;What does this description mean?&lt;/P&gt;&lt;P&gt;How do we add packages with the below parameters on ls-image-main.bb file?&lt;/P&gt;&lt;P&gt;Yocto: IMAGE_INSTALL&lt;/P&gt;&lt;P&gt;Ubuntu :&amp;nbsp;APTGET_EXTRA_PACKAGES&lt;/P&gt;&lt;P&gt;Can I install some package from yocto and some from ubuntu apt?&lt;/P&gt;&lt;P&gt;Is it may cause package&amp;nbsp;conflict, how to avoid it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Jack&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Jul 2024 07:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LLDP-pakcages-maintenance-problem-based-on-LX2160ARDB/m-p/1903747#M14533</guid>
      <dc:creator>jackho</dc:creator>
      <dc:date>2024-07-09T07:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: LLDP pakcages maintenance problem based on LX2160ARDB?</title>
      <link>https://community.nxp.com/t5/Layerscape/LLDP-pakcages-maintenance-problem-based-on-LX2160ARDB/m-p/1908234#M14548</link>
      <description>&lt;P&gt;You are using Ubuntu images, therefore root file system update should be done based on Ubuntu package manager.&lt;/P&gt;
&lt;P&gt;IMAGE_INSTALL:append = " ..." should be used for packages that don't have Ubuntu equivalent, which is for example nxp repositories&lt;/P&gt;
&lt;P&gt;&amp;nbsp;APTGET_EXTRA_PACKAGES += "nvmi-cli" should be used for Ubuntu to install nvmi-cli based on apt-get install nvmi-cli.&lt;/P&gt;
&lt;P&gt;So, please only use&amp;nbsp;APTGET_EXTRA_PACKAGES to add packages in&amp;nbsp;&lt;SPAN&gt;ls-image-main rootfs.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jul 2024 03:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LLDP-pakcages-maintenance-problem-based-on-LX2160ARDB/m-p/1908234#M14548</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-07-15T03:39:03Z</dc:date>
    </item>
  </channel>
</rss>