<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1088ARDB - Ethernet Link Status in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1891582#M14459</link>
    <description>&lt;P&gt;try to use the command&lt;/P&gt;
&lt;PRE&gt;&lt;CODE class="language-text"&gt;$ ip monitor all&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;it is used to&amp;nbsp;&lt;SPAN&gt;get real time link state.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;please check the info in the next link, it could help with your objetive&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/offlinehacker/NCD" target="_blank"&gt;https://github.com/offlinehacker/NCD&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 20 Jun 2024 16:56:31 GMT</pubDate>
    <dc:creator>LFGP</dc:creator>
    <dc:date>2024-06-20T16:56:31Z</dc:date>
    <item>
      <title>LS1088ARDB - Ethernet Link Status</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1889728#M14450</link>
      <description>&lt;P&gt;Hi NXP Support,&lt;/P&gt;&lt;P&gt;I am struggling with the LS1088ARDB development board. Using the default configuration for the yocto build for the board I can get networking operational. However, ETHTOOL Reports the link status as yes always regardless if an ethernet cable is plugged in or not.&lt;/P&gt;&lt;P&gt;- Boot Up&lt;/P&gt;&lt;P&gt;- Run `ethtool eth0`, link detected reports yes with no ethernet port plugged in.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Settings for eth0:
        Supported ports: [  ]
        Supported link modes:   Not reported
        Supported pause frame use: No
        Supports auto-negotiation: No
        Supported FEC modes: Not reported
        Advertised link modes:  Not reported
        Advertised pause frame use: No
        Advertised auto-negotiation: No
        Advertised FEC modes: Not reported
        Speed: 1000Mb/s
        Duplex: Full
        Auto-negotiation: off
        Port: Twisted Pair
        PHYAD: 0
        Transceiver: internal
        MDI-X: Unknown
        Link detected: yes&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We need a way to know what ports have physical cables plugged in, as well as udev rules that trigger when cables are plugged in and removed. udev is not reporting any driver state changes on cables being plugged in.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 18:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1889728#M14450</guid>
      <dc:creator>mloder</dc:creator>
      <dc:date>2024-06-18T18:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088ARDB - Ethernet Link Status</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1891582#M14459</link>
      <description>&lt;P&gt;try to use the command&lt;/P&gt;
&lt;PRE&gt;&lt;CODE class="language-text"&gt;$ ip monitor all&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;it is used to&amp;nbsp;&lt;SPAN&gt;get real time link state.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;please check the info in the next link, it could help with your objetive&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/offlinehacker/NCD" target="_blank"&gt;https://github.com/offlinehacker/NCD&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Jun 2024 16:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1891582#M14459</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2024-06-20T16:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088ARDB - Ethernet Link Status</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1894423#M14485</link>
      <description>&lt;P&gt;Hi LFGP,&lt;/P&gt;&lt;P&gt;Thank you for the help, however, I tried the command, it only works with DPMAC2 this is also the only port ethtool works on. DPMAC3-10 does not report at all with that command there is no output.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Wed, 26 Jun 2024 12:50:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1894423#M14485</guid>
      <dc:creator>mloder</dc:creator>
      <dc:date>2024-06-26T12:50:35Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088ARDB - Ethernet Link Status</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1897728#M14508</link>
      <description>&lt;P&gt;you can check it at MAC level, please use the next command:&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;restool dpmac info dpmac.&amp;lt;mac number&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;To determine what macs you have execute:&lt;BR /&gt;&lt;BR /&gt;ls-listni&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;please let me know the results&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 18:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/1897728#M14508</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2024-07-02T18:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: LS1088ARDB - Ethernet Link Status</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/2180439#M16170</link>
      <description>I have same issue, and here is my results:&lt;BR /&gt;&lt;BR /&gt;root@OpenWrt:~# restool dpmac info dpmac.3&lt;BR /&gt;dpmac version: 4.10&lt;BR /&gt;dpmac object id/portal id: 3&lt;BR /&gt;plugged state: plugged&lt;BR /&gt;endpoint state: 1&lt;BR /&gt;endpoint: dpni.2, link is up&lt;BR /&gt;DPMAC link type: DPMAC_LINK_TYPE_FIXED&lt;BR /&gt;DPMAC ethernet interface: DPMAC_ETH_IF_QSGMII&lt;BR /&gt;MAC address: 00:04:9f:06:12:05&lt;BR /&gt;maximum supported rate 1000 Mbps&lt;BR /&gt;Counters:&lt;BR /&gt;rx all frames: 0&lt;BR /&gt;rx frames ok: 0&lt;BR /&gt;rx frame errors: 0&lt;BR /&gt;rx frame discards: 0&lt;BR /&gt;rx u-cast: 0&lt;BR /&gt;rx b-cast: 0&lt;BR /&gt;rx m-cast: 0&lt;BR /&gt;rx 64 bytes: 0&lt;BR /&gt;rx 65-127 bytes: 0&lt;BR /&gt;rx 128-255 bytes: 0&lt;BR /&gt;rx 256-511 bytes: 0&lt;BR /&gt;rx 512-1023 bytes: 0&lt;BR /&gt;rx 1024-1518 bytes: 0&lt;BR /&gt;rx 1519-max bytes: 0&lt;BR /&gt;rx frags: 0&lt;BR /&gt;rx jabber: 0&lt;BR /&gt;rx align errors: 0&lt;BR /&gt;rx oversized: 0&lt;BR /&gt;rx pause: 0&lt;BR /&gt;rx bytes: 0&lt;BR /&gt;tx frames ok: 65&lt;BR /&gt;tx u-cast: 0&lt;BR /&gt;tx m-cast: 65&lt;BR /&gt;tx b-cast: 0&lt;BR /&gt;tx frame errors: 0&lt;BR /&gt;tx undersized: 0&lt;BR /&gt;tx b-pause: 0&lt;BR /&gt;tx bytes: 11742&lt;BR /&gt;root@OpenWrt:~#&lt;BR /&gt;root@OpenWrt:~# ls-listni&lt;BR /&gt;dprc.1/dpni.8 (interface: eth8, end point: dpmac.9)&lt;BR /&gt;dprc.1/dpni.7 (interface: eth7, end point: dpmac.8)&lt;BR /&gt;dprc.1/dpni.6 (interface: eth6, end point: dpmac.7)&lt;BR /&gt;dprc.1/dpni.5 (interface: eth5, end point: dpmac.6)&lt;BR /&gt;dprc.1/dpni.4 (interface: eth4, end point: dpmac.5)&lt;BR /&gt;dprc.1/dpni.3 (interface: eth3, end point: dpmac.4)&lt;BR /&gt;dprc.1/dpni.2 (interface: eth2, end point: dpmac.3)&lt;BR /&gt;dprc.1/dpni.1 (interface: eth1, end point: dpmac.2)&lt;BR /&gt;dprc.1/dpni.0 (interface: eth0, end point: dpmac.1)&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203371"&gt;@LFGP&lt;/a&gt;&amp;nbsp; or&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235126"&gt;@mloder&lt;/a&gt;&amp;nbsp;, could you help me resolve this one?&lt;BR /&gt;&lt;BR /&gt;Thanks a lot</description>
      <pubDate>Mon, 06 Oct 2025 08:46:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1088ARDB-Ethernet-Link-Status/m-p/2180439#M16170</guid>
      <dc:creator>ZuzuBiek</dc:creator>
      <dc:date>2025-10-06T08:46:35Z</dc:date>
    </item>
  </channel>
</rss>