<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックOCRAM</title>
    <link>https://community.nxp.com/t5/Layerscape/OCRAM/m-p/1890528#M14454</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm wondering if it is possible to boot BL31 in OCRAM using LX2160A-RDB board. I'm doing nasty things obviously (not even ashamed !...).&amp;nbsp;It's a 2MB memory, 256kB are used and BL31 is not oversized.&lt;/P&gt;&lt;P&gt;I tried to r/w in the free space but custom memcpy() function from driver is blocking at the very first byte to write.&lt;/P&gt;&lt;P&gt;Any clue ?&lt;/P&gt;</description>
    <pubDate>Wed, 19 Jun 2024 16:02:32 GMT</pubDate>
    <dc:creator>VL38</dc:creator>
    <dc:date>2024-06-19T16:02:32Z</dc:date>
    <item>
      <title>OCRAM</title>
      <link>https://community.nxp.com/t5/Layerscape/OCRAM/m-p/1890528#M14454</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm wondering if it is possible to boot BL31 in OCRAM using LX2160A-RDB board. I'm doing nasty things obviously (not even ashamed !...).&amp;nbsp;It's a 2MB memory, 256kB are used and BL31 is not oversized.&lt;/P&gt;&lt;P&gt;I tried to r/w in the free space but custom memcpy() function from driver is blocking at the very first byte to write.&lt;/P&gt;&lt;P&gt;Any clue ?&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jun 2024 16:02:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OCRAM/m-p/1890528#M14454</guid>
      <dc:creator>VL38</dc:creator>
      <dc:date>2024-06-19T16:02:32Z</dc:date>
    </item>
    <item>
      <title>Re: OCRAM</title>
      <link>https://community.nxp.com/t5/Layerscape/OCRAM/m-p/1893860#M14482</link>
      <description>&lt;P&gt;Hello, it isn't possible, BL31 uses DDR memory space, not OCRAM.&lt;/P&gt;
&lt;P&gt;Please refer to the following in plat/nxp/common/include/default/plat_default_def.h&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;#define BL31_BASE NXP_SECURE_DRAM_ADDR&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Jun 2024 20:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OCRAM/m-p/1893860#M14482</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-06-25T20:20:42Z</dc:date>
    </item>
  </channel>
</rss>