<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Building and debugging in LS1028ARDB (vs T1040D4-RDB) in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Building-and-debugging-in-LS1028ARDB-vs-T1040D4-RDB/m-p/1888744#M14441</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have had some experience with MPC and QorIQ PowerPC-based MCUs/processors and I intend to give a try to the newer ARM-based families.&lt;/P&gt;&lt;P&gt;When working with QorIQ devices, I used to do some basic testing either by calling my applications directly from U-boot (uploading it via serial or Ethernet having built it with the GHS compiler) or by running it from the GHS debugging envionment, uploading it and debugging it with the GHS probe.&lt;/P&gt;&lt;P&gt;Are these two scenarios available in the LS1028A evaluation board? I.e., can I 1) run some bare-metal application by simply using the "go" U-boot command; 2) Use the GHS environment for more detailed debugging?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;</description>
    <pubDate>Mon, 17 Jun 2024 13:21:46 GMT</pubDate>
    <dc:creator>ricardofranca</dc:creator>
    <dc:date>2024-06-17T13:21:46Z</dc:date>
    <item>
      <title>Building and debugging in LS1028ARDB (vs T1040D4-RDB)</title>
      <link>https://community.nxp.com/t5/Layerscape/Building-and-debugging-in-LS1028ARDB-vs-T1040D4-RDB/m-p/1888744#M14441</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have had some experience with MPC and QorIQ PowerPC-based MCUs/processors and I intend to give a try to the newer ARM-based families.&lt;/P&gt;&lt;P&gt;When working with QorIQ devices, I used to do some basic testing either by calling my applications directly from U-boot (uploading it via serial or Ethernet having built it with the GHS compiler) or by running it from the GHS debugging envionment, uploading it and debugging it with the GHS probe.&lt;/P&gt;&lt;P&gt;Are these two scenarios available in the LS1028A evaluation board? I.e., can I 1) run some bare-metal application by simply using the "go" U-boot command; 2) Use the GHS environment for more detailed debugging?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 17 Jun 2024 13:21:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Building-and-debugging-in-LS1028ARDB-vs-T1040D4-RDB/m-p/1888744#M14441</guid>
      <dc:creator>ricardofranca</dc:creator>
      <dc:date>2024-06-17T13:21:46Z</dc:date>
    </item>
    <item>
      <title>Re: Building and debugging in LS1028ARDB (vs T1040D4-RDB)</title>
      <link>https://community.nxp.com/t5/Layerscape/Building-and-debugging-in-LS1028ARDB-vs-T1040D4-RDB/m-p/1889585#M14449</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;1) Yes you can run baremetal code&lt;/P&gt;
&lt;P&gt;2) you have to go with Greenhills for detail on it, it's supported.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 18 Jun 2024 14:12:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Building-and-debugging-in-LS1028ARDB-vs-T1040D4-RDB/m-p/1889585#M14449</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-06-18T14:12:20Z</dc:date>
    </item>
  </channel>
</rss>