<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Using IRQ00 - IRQ02 pins as a peripheral interrupt</title>
    <link>https://community.nxp.com/t5/Layerscape/Using-IRQ00-IRQ02-pins-as-a-peripheral-interrupt/m-p/1879192#M14387</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221133"&gt;@mehdi-cubic&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Regarding to the question "So, is it possible to use the IRQ00 - IRQ03 (external INT) pins for this purpose like a normal GPIO interrupt?"&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Yes, It possible to use just the IRQ03 as a GPIO interrupt.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regarding to the question "Looking at the LS1043ARM.pdf (Table B-1 - p2500 in Rev6), my impression is that these pins are designed for an external wake-up (only?)."&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The pins IRQ00 to IRQ02 is only for external wake up, the only one that can be possible to use as a GPIO is IRQ03.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regarding to the question "The example device-tree in the above link is using a GPIO address like this: 'gpio99: gpio@22', but is this possible with IRQ00, or should this line be rewired to a different GPIO?"&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;In the next response I will response this question&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Sebastian&lt;/P&gt;</description>
    <pubDate>Fri, 31 May 2024 22:28:26 GMT</pubDate>
    <dc:creator>SebastianG</dc:creator>
    <dc:date>2024-05-31T22:28:26Z</dc:date>
    <item>
      <title>Using IRQ00 - IRQ02 pins as a peripheral interrupt</title>
      <link>https://community.nxp.com/t5/Layerscape/Using-IRQ00-IRQ02-pins-as-a-peripheral-interrupt/m-p/1876245#M14364</link>
      <description>&lt;P&gt;I am using LS1043A (on a custom board), where IRQ00 is connected to the INT line of a GPIO expander chip (PCA9506).&amp;nbsp;&lt;BR /&gt;In this scenario, I am not sure if it is possible to have a device-tree node for the existing Kernel driver&amp;nbsp;&lt;A href="https://www.kernel.org/doc/Documentation/devicetree/bindings/gpio/gpio-pca953x.txt" target="_self"&gt;pca953x&lt;/A&gt;&lt;/P&gt;&lt;P&gt;So, is it possible to use the&amp;nbsp;IRQ00 -&amp;nbsp;IRQ03 (external INT) pins for this purpose like a normal GPIO interrupt?&lt;BR /&gt;Looking at the LS1043ARM.pdf (Table B-1 - p2500 in Rev6), my impression is that these pins are designed for an external wake-up (only?).&lt;BR /&gt;The example device-tree in the above link is using a GPIO address like this: 'gpio99:&amp;nbsp; gpio@22&lt;A href="mailto:gpio@22'," target="_blank"&gt;',&lt;/A&gt;&amp;nbsp;but is this possible with&amp;nbsp;IRQ00, or should this line be rewired to a different GPIO?&lt;BR /&gt;If this is possible, could you please suggest a device-tree entry.&lt;BR /&gt;I have also seen this&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/LS1043a-IRQ00-IRQ01-IRQ02-interruption-handler/m-p/1198040" target="_self"&gt;post&lt;/A&gt;&amp;nbsp;on the subject.&lt;BR /&gt;&lt;BR /&gt;Your help is appreciated.&lt;/P&gt;</description>
      <pubDate>Tue, 28 May 2024 10:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Using-IRQ00-IRQ02-pins-as-a-peripheral-interrupt/m-p/1876245#M14364</guid>
      <dc:creator>mehdi-cubic</dc:creator>
      <dc:date>2024-05-28T10:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: Using IRQ00 - IRQ02 pins as a peripheral interrupt</title>
      <link>https://community.nxp.com/t5/Layerscape/Using-IRQ00-IRQ02-pins-as-a-peripheral-interrupt/m-p/1879192#M14387</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221133"&gt;@mehdi-cubic&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Regarding to the question "So, is it possible to use the IRQ00 - IRQ03 (external INT) pins for this purpose like a normal GPIO interrupt?"&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Yes, It possible to use just the IRQ03 as a GPIO interrupt.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regarding to the question "Looking at the LS1043ARM.pdf (Table B-1 - p2500 in Rev6), my impression is that these pins are designed for an external wake-up (only?)."&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The pins IRQ00 to IRQ02 is only for external wake up, the only one that can be possible to use as a GPIO is IRQ03.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regarding to the question "The example device-tree in the above link is using a GPIO address like this: 'gpio99: gpio@22', but is this possible with IRQ00, or should this line be rewired to a different GPIO?"&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;In the next response I will response this question&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Sebastian&lt;/P&gt;</description>
      <pubDate>Fri, 31 May 2024 22:28:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Using-IRQ00-IRQ02-pins-as-a-peripheral-interrupt/m-p/1879192#M14387</guid>
      <dc:creator>SebastianG</dc:creator>
      <dc:date>2024-05-31T22:28:26Z</dc:date>
    </item>
  </channel>
</rss>