<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1875298#M14347</link>
    <description>&lt;P&gt;&lt;SPAN&gt;During HRESET_B, SoC follows exactly the same procedure as PORESET_B. But additional sampling of POR configuration pins occurs at the rising edge of PORESET_B signal (when PORESET_B is de-asserted) to determine the RCW source. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When SoC is out of reset, default value of PORESET_B &amp;amp; HRESET_B is high.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On setting WDOG3 active with timeout value of 3s, system reset after 3s =&amp;gt; mw.w 0x2a70000 0534&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WDOG3_WRSR register should indicate that the reset was due to watchdog timeout via the TOUT bit. Bit 14 should be 1 =&amp;gt; md.w 0x2a70004 would show 0012&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Further, register DCFG_CCSR_RSTRQSR1 should show 1 for bit 0, the CORE_WDOG3_RST_RR field, to indicate that WDOG reset request from WDOG3 is active. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The bit 0 of DCFG_CCSR_RSTRQSR1 register will restore its value to 1 if RESET_REQ_B is connected to HRESET_B. If RESET_REQ_B is connected to PORESET_B, then bit 0 of DCFG_CCSR_RSTRQSR1 register will restore its value to 0. &lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 27 May 2024 07:13:33 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2024-05-27T07:13:33Z</dc:date>
    <item>
      <title>LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1847180#M14180</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear&lt;/SPAN&gt;；&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; We set WDOG3 active and timeout value 3s,&amp;nbsp;It works and system was reset after 3S;See Figure 1.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;But we found that there's no change in&amp;nbsp;&lt;STRONG&gt;DCFG_CCSR_RSTRQSR1&amp;nbsp;&lt;/STRONG&gt;register.See Figure 2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;According the the LS1043ARM, the reset reason should be record in the bit 0, but it did not.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;What are the conditions that trigger a change in the DCFG_CCSR_RSTRQSR1 register at reset? How do I read the value of the DCFG_CCSR_RSTRQSR1 register to be a valid value?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 13:58:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1847180#M14180</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2024-04-15T13:58:03Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1854424#M14219</link>
      <description>&lt;P&gt;&lt;SPAN&gt;To which reset signal(PORESET_B or HRESET_B), the RESET_REQ_B pin is connected? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DCFG_CCSR_RSTRQSR1 register stores the status bits to record how reset occured last time the LS1043A device is working. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If RESET_REQ_B pin is connected to HRESET_B, then no change in value will be seen at bit 0(CORE_WDOG3_RST_RR). &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If connected to POREST_B, bit 0 will be set to 1. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;You can also refer/check section 13.3.14 Reset Request Status Register (DCFG_CCSR_RSTRQSR1) in LS1043ARM for its description and usage.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 25 Apr 2024 07:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1854424#M14219</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-04-25T07:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1860870#M14257</link>
      <description>&lt;P&gt;Dear Yingping;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; It&amp;nbsp;&lt;SPAN&gt;connected to POREST_B, bit 0&amp;nbsp; still is 0.&amp;nbsp;&amp;nbsp;What are the conditions for wdog3 to fire? Thank you!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 May 2024 23:28:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1860870#M14257</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2024-05-07T23:28:12Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1861117#M14260</link>
      <description>&lt;P&gt;Please refer to the following update from the AE team.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;If customer has any provision to connect RESET_REQ_B signal to HRESET_B, do that and observe the bit 0. Do let us know if any change occurs.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 May 2024 06:31:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1861117#M14260</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-08T06:31:39Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1861132#M14261</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Apologies for my last response. Some confusion occurs on understanding the issue. If customer has any provision to connect RESET_REQ_B signal to HRESET_B, do that and observe the bit 0. Do let us know if any change occurs.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;RESET_REQ_B is an internal block request that asserts HRESET_B or PORESET_B. In your case, it is asserting PORESET_B, which resets the register to its default or initial state. To see the source of the output reset assertion in DCFG_CCSR_RSTRQSR1 , RESET_REQ_B&amp;nbsp; should be connected to HRESET_B.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 08 May 2024 06:45:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1861132#M14261</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-08T06:45:41Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1863773#M14271</link>
      <description>&lt;P&gt;Dear Yiping；&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;Motherboard measured RESET_REQ connected to HRSET, can not achieve reset? And then it goes down and it stays down. Please check the attached schematic to see what the reason is.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;FYI!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 11 May 2024 03:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1863773#M14271</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2024-05-11T03:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1866153#M14289</link>
      <description>&lt;P&gt;&lt;SPAN&gt;1) R5587 is marked as "DNI", I am not sure if output from 4th pin of buffer IC U5021 is connected to HRESET_N.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) Similarly, R5049 is marked as "DNI", I am not sure if RESET_REQ_N signal is connected to HRESET_N through this resistor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3) We can also see at a point where R5446 is connected, RESET_REQ_N is also directly connected to POR_B through R5586 which is wrong because it does not meet the timing requirement of POR_B.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4) PORESET_B and HRESET_B have a minimum assertion time of 1ms and 32 SYSCLKs respectively which can be fulfilled if RESET_REQ_B is provided as an input to the reset block IC U5001. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;RESET_REQ_B causes assertion of either PORESET_B or HRESET_B. If PORESET_B is asserted, it initializes all registers to its default state and most I/O drivers are released to high impedance means RESET_REQ_B will behave as an input now. You can refer section 4.4.1 Power-on reset sequence of LS1043ARM for detail information. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;At this time, PORESET_B assertion causes RESET_REQ_B to go down but due to its high impedance state, it again pulled up within a short period of time which inhibits PORESET_B to meet its minimum assertion time. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Therefore, the RESET_REQ_B signal should be provided as an input to external reset IC which converts any short pulse detected to a bigger one through some internal logic and PORESET_B and HRESET_B timing requirement can be fulfilled.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 09:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1866153#M14289</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-15T09:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1870142#M14322</link>
      <description>&lt;P&gt;Dear Yiping；&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;HRESET_B and PORESET_B are currently described in the NXP LS1043ARM manual as follows:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;PORESET_B ：Power on reset. Causes the chip to abort all current internal and external&lt;BR /&gt;transactions and set all registers to their default values. PORESET_B may be&lt;BR /&gt;asserted completely asynchronously with respect to all other signals.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;HRESET_B：Hard reset. Causes the chip to abort all current internal and external transactions&lt;BR /&gt;and set all registers to their default values. HRESET_B may be asserted completely&lt;BR /&gt;asynchronously with respect to all other signals. HRESET_B is driven as an output&lt;BR /&gt;during the first part of the power on reset sequence, after which, it becomes an&lt;BR /&gt;input, allowing external devices to stall/hold the reset sequence. See Hard reset&lt;BR /&gt;sequence for more information.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;2 reset will be auses the chip to abort all current internal and external&lt;BR /&gt;transactions and set all registers to their default values.&amp;nbsp;What is the difference between HRESET_B and PORESET_B? Is default values&amp;nbsp; “0”?&amp;nbsp;Does HRESET_B restore the DCFG_CCSR_RSTRQSR1 register to 0?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; Thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 May 2024 02:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1870142#M14322</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2024-05-22T02:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1870153#M14323</link>
      <description>&lt;P&gt;Will back to you.&lt;/P&gt;</description>
      <pubDate>Wed, 22 May 2024 02:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1870153#M14323</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-22T02:46:39Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1875097#M14343</link>
      <description>&lt;P&gt;Dear yiping;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;Did you get any results on this question? Thank you!&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 02:14:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1875097#M14343</guid>
      <dc:creator>jack_huang1</dc:creator>
      <dc:date>2024-05-27T02:14:09Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1875104#M14344</link>
      <description>&lt;P&gt;Confirming with the AE team now.&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 02:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1875104#M14344</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-27T02:34:57Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A DCFG_CCSR_RSTRQSR1 register does not change</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1875298#M14347</link>
      <description>&lt;P&gt;&lt;SPAN&gt;During HRESET_B, SoC follows exactly the same procedure as PORESET_B. But additional sampling of POR configuration pins occurs at the rising edge of PORESET_B signal (when PORESET_B is de-asserted) to determine the RCW source. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When SoC is out of reset, default value of PORESET_B &amp;amp; HRESET_B is high.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;On setting WDOG3 active with timeout value of 3s, system reset after 3s =&amp;gt; mw.w 0x2a70000 0534&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;WDOG3_WRSR register should indicate that the reset was due to watchdog timeout via the TOUT bit. Bit 14 should be 1 =&amp;gt; md.w 0x2a70004 would show 0012&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Further, register DCFG_CCSR_RSTRQSR1 should show 1 for bit 0, the CORE_WDOG3_RST_RR field, to indicate that WDOG reset request from WDOG3 is active. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The bit 0 of DCFG_CCSR_RSTRQSR1 register will restore its value to 1 if RESET_REQ_B is connected to HRESET_B. If RESET_REQ_B is connected to PORESET_B, then bit 0 of DCFG_CCSR_RSTRQSR1 register will restore its value to 0. &lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 07:13:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-DCFG-CCSR-RSTRQSR1-register-does-not-change/m-p/1875298#M14347</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-05-27T07:13:33Z</dc:date>
    </item>
  </channel>
</rss>