<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1028 Newer kernel version than 5.10</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1875206#M14345</link>
    <description>&lt;P&gt;Wow, yet another NXP overlay for OpenEmbedded. Just how many are there?&lt;/P&gt;</description>
    <pubDate>Mon, 27 May 2024 05:56:37 GMT</pubDate>
    <dc:creator>mikelooijmans</dc:creator>
    <dc:date>2024-05-27T05:56:37Z</dc:date>
    <item>
      <title>LS1028 Newer kernel version than 5.10</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1868104#M14301</link>
      <description>&lt;P&gt;Even the current "master" of meta-freescale builds a 5.10 kernel for linux-qoriq.&lt;/P&gt;&lt;P&gt;This is ancient - even Yocto itself complains about it as it expects at least 5.15 (for glibc) in scarthgap and master.&lt;/P&gt;&lt;P&gt;Also, we're attaching an NVME to the PCIe port, and I really want some fairly recent kernel changes (6.1) that improve power management for us.&lt;/P&gt;&lt;P&gt;As we will not be using any GPU or network, no firmware blobs are needed, and reportedly, the LS1028 should work with mainline.&lt;/P&gt;&lt;P&gt;I tried building the 6.6 linux-fslc kernel instead, with some recipe modifications, and got the ls1028ardb board to boot a bit into the kernel. However, the DMA controller won't load properly so there's not much that works. I'm digging into what prevents the kernel from accessing the SD device, as it gets stuck waiting for that (and loading the rootfs).&lt;/P&gt;&lt;P&gt;Has anyone made any progress into making the LS1028 kernel slightly less outdated?&lt;/P&gt;</description>
      <pubDate>Fri, 17 May 2024 13:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1868104#M14301</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-05-17T13:58:30Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 Newer kernel version than 5.10</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1868801#M14306</link>
      <description>&lt;P&gt;Here you have &lt;A href="https://github.com/nxp-qoriq/meta-qoriq" target="_blank"&gt;https://github.com/nxp-qoriq/meta-qoriq&lt;/A&gt; a repo where there are more recent kernels available. From what I know the new meta-qoriq Yocto release scarthgap will be available at the end of June so once it's done I guess they will change it also in the meta-freescale.&lt;/P&gt;</description>
      <pubDate>Mon, 20 May 2024 10:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1868801#M14306</guid>
      <dc:creator>pb3</dc:creator>
      <dc:date>2024-05-20T10:08:17Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 Newer kernel version than 5.10</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1870250#M14325</link>
      <description>&lt;P&gt;Indeed, there's a 6.6 kernel recipe in there too.&lt;/P&gt;&lt;P&gt;The mainline kernel also works, it's just a matter of driver selection that made it fail to boot properly. It's a pain to find all the required drivers, found them by taking "compatible" strings from the devicetree, then grep on that to find the related code files, and then grep the Makefile in that directory to get to the required Kconfig item that enables it.&lt;/P&gt;</description>
      <pubDate>Wed, 22 May 2024 05:42:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1870250#M14325</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-05-22T05:42:14Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 Newer kernel version than 5.10</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1874858#M14340</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The latest supported version is&amp;nbsp;Kernel v6.1.55, You can refer to the following link for more information:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/meta-nxp-desktop/blob/lf-6.1.55-2.2.0-mickledore/README.md" target="_blank"&gt;https://github.com/nxp-imx/meta-nxp-desktop/blob/lf-6.1.55-2.2.0-mickledore/README.md&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 19:48:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1874858#M14340</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-05-24T19:48:57Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 Newer kernel version than 5.10</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1875206#M14345</link>
      <description>&lt;P&gt;Wow, yet another NXP overlay for OpenEmbedded. Just how many are there?&lt;/P&gt;</description>
      <pubDate>Mon, 27 May 2024 05:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-Newer-kernel-version-than-5-10/m-p/1875206#M14345</guid>
      <dc:creator>mikelooijmans</dc:creator>
      <dc:date>2024-05-27T05:56:37Z</dc:date>
    </item>
  </channel>
</rss>