<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1043A reset reason</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-reset-reason/m-p/1855798#M14224</link>
    <description>&lt;P&gt;Thanks for your explain Mr. Wang,&lt;/P&gt;&lt;P&gt;what I want is get the reason of last time reset, then I will do somthing according to it.&lt;/P&gt;&lt;P&gt;So could this register store the reset reson till next time start up after RESET_REQ_B asserted and then I can read the register in, u-boot for example, and get the reset reason?&lt;/P&gt;&lt;P&gt;If not, how can I get the reset reason of last time reset?&lt;/P&gt;</description>
    <pubDate>Fri, 26 Apr 2024 15:12:40 GMT</pubDate>
    <dc:creator>zillnk_wufan</dc:creator>
    <dc:date>2024-04-26T15:12:40Z</dc:date>
    <item>
      <title>LS1043A reset reason</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-reset-reason/m-p/1847770#M14184</link>
      <description>&lt;P&gt;Hi NXP experts:&lt;/P&gt;&lt;P&gt;I connect the RESET_REQ_B signal to the PORESET_B, and test the watchdog(wdog 3) function in my board, the watch dog works fine and the board reset, but when I try to figure out the reset reason by register&amp;nbsp;&lt;SPAN&gt;DCFG_CCSR_RSTRQSR1(0x01ee00c8), the register did not record the reset reason in relevant bit as the LS1043ARM documentation described.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zillnk_wufan_0-1713248861040.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/273937iF5093F2DE3C974EC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zillnk_wufan_0-1713248861040.png" alt="zillnk_wufan_0-1713248861040.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;zillnk_wufan_0-1713248861040.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;So I want to know is the PORESET_B cause the register not work? should I connect RESET_REQ_B to HRESET_B if I want to collect the reset reason? If not, what should I do?&lt;/P&gt;&lt;P&gt;Thanks a lot&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 06:31:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-reset-reason/m-p/1847770#M14184</guid>
      <dc:creator>zillnk_wufan</dc:creator>
      <dc:date>2024-04-16T06:31:26Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A reset reason</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-reset-reason/m-p/1851495#M14201</link>
      <description>&lt;P&gt;First of all, if RESET_REQ is asserted, when - there is a condition requiring the assertion of reset. I mean, the internal state of the processor core may be fatal and further code execution may not be possible, if reset is requested.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If the processor can still execute the code, when RESET_REQ is signaled, than yes - you can try to read re reset reason is DCFG_CCSR_RSTRQSR1. Note that most of the reset reasons, indicated in this register, may be masked in DCFG_CCSR_RSTRQMR1 (except watchdog reset and software-initiated reset)。&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The register DCFG_CCSR_RSTRQPBLSR is related to pre-boot loader and indicates pre-boot loader errors. If the core fails, when it already up and running, than this register is not related.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 09:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-reset-reason/m-p/1851495#M14201</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2024-04-22T09:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A reset reason</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-reset-reason/m-p/1855798#M14224</link>
      <description>&lt;P&gt;Thanks for your explain Mr. Wang,&lt;/P&gt;&lt;P&gt;what I want is get the reason of last time reset, then I will do somthing according to it.&lt;/P&gt;&lt;P&gt;So could this register store the reset reson till next time start up after RESET_REQ_B asserted and then I can read the register in, u-boot for example, and get the reset reason?&lt;/P&gt;&lt;P&gt;If not, how can I get the reset reason of last time reset?&lt;/P&gt;</description>
      <pubDate>Fri, 26 Apr 2024 15:12:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-reset-reason/m-p/1855798#M14224</guid>
      <dc:creator>zillnk_wufan</dc:creator>
      <dc:date>2024-04-26T15:12:40Z</dc:date>
    </item>
  </channel>
</rss>