<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: is there PCI configuration difference between LX2160XC72029B and LX2160XE72029B?</title>
    <link>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1839889#M14147</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We had got the information from our local distribute and can be resolved the issue with the patch file.&lt;/P&gt;&lt;P&gt;-----&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;Please try to upgrade to LSDK21.08, our LSDK uses the SVR to identify the correct LX2160 SoC silicon revision and then load the correct PCIe controller driver accordingly since Rev 1 and Rev 2 silicon use different PCIe controller IP cores from two different IP vendors. Unfortunately, due to oversight, the LSDK 20.xx version (up to LSDK 20.12) has a mistake when checking the CAN-FD bits.&amp;nbsp;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 03 Apr 2024 06:19:05 GMT</pubDate>
    <dc:creator>shinhakang</dc:creator>
    <dc:date>2024-04-03T06:19:05Z</dc:date>
    <item>
      <title>is there PCI configuration difference between LX2160XC72029B and LX2160XE72029B?</title>
      <link>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1838936#M14140</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We had changed LX2160A part-number&amp;nbsp;LX2160XE72029B from&amp;nbsp;LX2160XC72029B,&lt;/P&gt;&lt;P&gt;But PCI looks not working with the uboot and kernel which are working in&amp;nbsp;LX2160XC72029B.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any difference? on our understanding the difference whether CAN support or not.&lt;/P&gt;&lt;P&gt;If any needed for&amp;nbsp;LX2160XE72029B for PCI, let me know..&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shinha.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 05:19:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1838936#M14140</guid>
      <dc:creator>shinhakang</dc:creator>
      <dc:date>2024-04-02T05:19:09Z</dc:date>
    </item>
    <item>
      <title>Re: is there PCI configuration difference between LX2160XC72029B and LX2160XE72029B?</title>
      <link>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1839537#M14142</link>
      <description>&lt;P&gt;Hello, your understanding is correct, it should work in the same way for both devices for PCIe interfaces.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 15:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1839537#M14142</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-04-02T15:27:22Z</dc:date>
    </item>
    <item>
      <title>Re: is there PCI configuration difference between LX2160XC72029B and LX2160XE72029B?</title>
      <link>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1839764#M14144</link>
      <description>&lt;P&gt;Hi, thank for your comments. Then what should be checked in our case? when replaced with&amp;nbsp;&lt;SPAN&gt;LX2160XC72029B in the same board &amp;nbsp;it works, but&amp;nbsp;LX2160XE72029B not work... we are using LSDK 2004 version. Thanks.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 02:19:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1839764#M14144</guid>
      <dc:creator>shinhakang</dc:creator>
      <dc:date>2024-04-03T02:19:18Z</dc:date>
    </item>
    <item>
      <title>Re: is there PCI configuration difference between LX2160XC72029B and LX2160XE72029B?</title>
      <link>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1839889#M14147</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We had got the information from our local distribute and can be resolved the issue with the patch file.&lt;/P&gt;&lt;P&gt;-----&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;Please try to upgrade to LSDK21.08, our LSDK uses the SVR to identify the correct LX2160 SoC silicon revision and then load the correct PCIe controller driver accordingly since Rev 1 and Rev 2 silicon use different PCIe controller IP cores from two different IP vendors. Unfortunately, due to oversight, the LSDK 20.xx version (up to LSDK 20.12) has a mistake when checking the CAN-FD bits.&amp;nbsp;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;---&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 06:19:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/is-there-PCI-configuration-difference-between-LX2160XC72029B-and/m-p/1839889#M14147</guid>
      <dc:creator>shinhakang</dc:creator>
      <dc:date>2024-04-03T06:19:05Z</dc:date>
    </item>
  </channel>
</rss>