<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1021ATWR - U-BOOT- UART - LPUART</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021ATWR-U-BOOT-UART-LPUART/m-p/550889#M1402</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess I was not clear in my question. &lt;/P&gt;&lt;P&gt;Before I had a ls1021a Rev1.0 and UART by default. The console was on ttyS0 and the connection to RS485 on TWR-SER2 board was ttyS1 and I used both. Now in ls1021a Rev2.0 the RS485 is connected to ttyLP0 and the console as well.&lt;/P&gt;&lt;P&gt;What to do in order to have RS485 and console on separate tty's?&lt;/P&gt;&lt;P&gt;I couldn't find where is ttyLP1 going from TWR-ls1021a reference manual which I could use as console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Zoran Stoilov&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 Jul 2016 07:22:57 GMT</pubDate>
    <dc:creator>zoranstoilov</dc:creator>
    <dc:date>2016-07-29T07:22:57Z</dc:date>
    <item>
      <title>LS1021ATWR - U-BOOT- UART - LPUART</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021ATWR-U-BOOT-UART-LPUART/m-p/550887#M1400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a LS1021atwr Rev2.0 connected with TWR-SER2. I want to use RS485 functionality of TWR-SER2.&lt;/P&gt;&lt;P&gt;But RS485 is connected to LPUART1 pins.&lt;/P&gt;&lt;P&gt;If I enable LPUART in "&lt;SPAN class="p_header"&gt;include/configs/ls1021atwr.h", the console from UART1/USB is gone and I can see it on LPUART1. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="p_header"&gt;J19 and J20&amp;nbsp; before were shorting 2-3 when uart used and now they are shortening 1-2 when LPUART enabled.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="p_header"&gt;My question is how to configure u-boot so I can have console and I can use LPUART1(/dev/ttyLP0)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="p_header"&gt;I have enabled ttyLP1 in device tree(&amp;amp;lpuart1) but I don't know if/where it is connected to TWR-SER2 board!?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="p_header"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="p_header"&gt;I use SDK1.9 for u-boot building with sdk2.0 for openwrt rootfs and I boot from SD_CARD only.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 16:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021ATWR-U-BOOT-UART-LPUART/m-p/550887#M1400</guid>
      <dc:creator>zoranstoilov</dc:creator>
      <dc:date>2016-07-28T16:18:20Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021ATWR - U-BOOT- UART - LPUART</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021ATWR-U-BOOT-UART-LPUART/m-p/550888#M1401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;Find the following setting in the u-boot configuration file for TWR-LS1021A board (ls1021atwr.h file)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;#ifdef CONFIG_LPUART&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;#define CONFIG_EXTRA_ENV_SETTINGS \&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "bootargs=root=/dev/ram0 rw console=ttyLP0,115200\0" \&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "initrd_high=0xcfffffff\0"&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; \&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "fdt_high=0xcfffffff\0"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2016 03:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021ATWR-U-BOOT-UART-LPUART/m-p/550888#M1401</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-07-29T03:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021ATWR - U-BOOT- UART - LPUART</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021ATWR-U-BOOT-UART-LPUART/m-p/550889#M1402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I guess I was not clear in my question. &lt;/P&gt;&lt;P&gt;Before I had a ls1021a Rev1.0 and UART by default. The console was on ttyS0 and the connection to RS485 on TWR-SER2 board was ttyS1 and I used both. Now in ls1021a Rev2.0 the RS485 is connected to ttyLP0 and the console as well.&lt;/P&gt;&lt;P&gt;What to do in order to have RS485 and console on separate tty's?&lt;/P&gt;&lt;P&gt;I couldn't find where is ttyLP1 going from TWR-ls1021a reference manual which I could use as console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Zoran Stoilov&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Jul 2016 07:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021ATWR-U-BOOT-UART-LPUART/m-p/550889#M1402</guid>
      <dc:creator>zoranstoilov</dc:creator>
      <dc:date>2016-07-29T07:22:57Z</dc:date>
    </item>
  </channel>
</rss>