<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LS1043ARDB-PD preboot issue in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-preboot-issue/m-p/1794645#M13901</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am struggling with some problems with LS1043ARDB-PD.&lt;/P&gt;&lt;P&gt;I did some preboots to execute "help" command in teraterm with connection in this Evaluation Board.&lt;/P&gt;&lt;P&gt;And I followed getting started guide to this.&lt;/P&gt;&lt;P&gt;But while i was using this board, i had changed&amp;nbsp;k22fx512_if_mbed.bin file's connection properties into notepad++ file, because of curiosity.&lt;/P&gt;&lt;P&gt;But now the board won't get to the preboot even i follow steps even thought i reset the connection properties.&lt;/P&gt;&lt;P&gt;How can i solve this case?&lt;/P&gt;&lt;P&gt;@LS1043ARDB-PD&lt;/P&gt;</description>
    <pubDate>Wed, 24 Jan 2024 12:14:39 GMT</pubDate>
    <dc:creator>TJAhn</dc:creator>
    <dc:date>2024-01-24T12:14:39Z</dc:date>
    <item>
      <title>LS1043ARDB-PD preboot issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-preboot-issue/m-p/1794645#M13901</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am struggling with some problems with LS1043ARDB-PD.&lt;/P&gt;&lt;P&gt;I did some preboots to execute "help" command in teraterm with connection in this Evaluation Board.&lt;/P&gt;&lt;P&gt;And I followed getting started guide to this.&lt;/P&gt;&lt;P&gt;But while i was using this board, i had changed&amp;nbsp;k22fx512_if_mbed.bin file's connection properties into notepad++ file, because of curiosity.&lt;/P&gt;&lt;P&gt;But now the board won't get to the preboot even i follow steps even thought i reset the connection properties.&lt;/P&gt;&lt;P&gt;How can i solve this case?&lt;/P&gt;&lt;P&gt;@LS1043ARDB-PD&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jan 2024 12:14:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-preboot-issue/m-p/1794645#M13901</guid>
      <dc:creator>TJAhn</dc:creator>
      <dc:date>2024-01-24T12:14:39Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043ARDB-PD preboot issue</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-preboot-issue/m-p/1797067#M13915</link>
      <description>&lt;P&gt;Hello, Please follow the steps below:&lt;/P&gt;
&lt;P&gt;Plug in power to LS board. Hold down Reset button while plugging the PC USB cable into the CSAM USB connector on the board.&lt;BR /&gt;On Windows, the board will be mapped as a Mass Storage Device under a volume labelled 'BOOTLOADER'.&lt;BR /&gt;LED for MBED status will blink in green on the board to acknowledge it is in bootloader mode.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;1. Copy the attached binary into the 'BOOTLOADER’&lt;BR /&gt;2. Wait the binary copy to finish; LED for MBED status will blink with higher rate on finish;&lt;BR /&gt;3. Unplug the USB cable from the board, then plug it back in to power cycle the module&lt;BR /&gt;4. The board should be ready to connect to CodeWarrior&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, there is a known issue with MBED operation under Win10.&lt;/P&gt;
&lt;P&gt;This is the work around we have confirmed to fix the mbed issue on Win10 PC's:&lt;BR /&gt;- Go to the "Start" option on the PC and type the command&amp;nbsp; "Services"&lt;BR /&gt;- Than you should see the following "Services" window open&lt;BR /&gt;- Select the "Storage Services" and on the left-hand side of the window click the "Stop the service"&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Oswalag_0-1706551932143.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/260606iF854B04799C413A9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Oswalag_0-1706551932143.jpeg" alt="Oswalag_0-1706551932143.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Oswalag_0-1706551932143.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 18:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-preboot-issue/m-p/1797067#M13915</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-01-29T18:12:58Z</dc:date>
    </item>
  </channel>
</rss>