<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: can I deploy customized bootpartition, rootfs etc. using flex-installer?</title>
    <link>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1758082#M13663</link>
    <description>&lt;P&gt;so, I need to run flex-installer with working directory to be the directory that has customized rootfs file. right?&lt;BR /&gt;&lt;BR /&gt;thanks&lt;/P&gt;</description>
    <pubDate>Thu, 16 Nov 2023 05:51:02 GMT</pubDate>
    <dc:creator>Taeyoon</dc:creator>
    <dc:date>2023-11-16T05:51:02Z</dc:date>
    <item>
      <title>can I deploy customized bootpartition, rootfs etc. using flex-installer?</title>
      <link>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1756063#M13625</link>
      <description>&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;I have bootpartition, composite firmware, rootfs(ls-image-main.xxx.tar.gz) files customized with yocto build.&lt;/P&gt;&lt;P&gt;I confuse whether flex-installer command is used only when deploying&amp;nbsp;default ones or also used for deploying customized ones.&amp;nbsp;&lt;/P&gt;&lt;P&gt;for example, if I have updated version(with customized kernel) ls-image-main-lx2160ardb-rev2.tar.gz in ~/yocto-sdk/build_lx2160ardb-rev2/tmp/deploy/images/lx2160ardb-rev2 directory, and run the command that $flex-installer -r ls-image-main-lx2160ardb-rev2.tar.gz -d /dev/sdx, then is updated rootfs in my host deployed to the SDcard connected to host?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks,&lt;/P&gt;</description>
      <pubDate>Mon, 13 Nov 2023 07:19:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1756063#M13625</guid>
      <dc:creator>Taeyoon</dc:creator>
      <dc:date>2023-11-13T07:19:17Z</dc:date>
    </item>
    <item>
      <title>Re: can I deploy customized bootpartition, rootfs etc. using flex-installer?</title>
      <link>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1757360#M13650</link>
      <description>&lt;P&gt;Yes,&amp;nbsp;&lt;SPAN&gt;flex-installer command can be used to deploy customized rootfs filesystem.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 06:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1757360#M13650</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-11-15T06:51:46Z</dc:date>
    </item>
    <item>
      <title>Re: can I deploy customized bootpartition, rootfs etc. using flex-installer?</title>
      <link>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1758082#M13663</link>
      <description>&lt;P&gt;so, I need to run flex-installer with working directory to be the directory that has customized rootfs file. right?&lt;BR /&gt;&lt;BR /&gt;thanks&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 05:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1758082#M13663</guid>
      <dc:creator>Taeyoon</dc:creator>
      <dc:date>2023-11-16T05:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: can I deploy customized bootpartition, rootfs etc. using flex-installer?</title>
      <link>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1758861#M13670</link>
      <description>&lt;P&gt;Yes.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Nov 2023 07:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/can-I-deploy-customized-bootpartition-rootfs-etc-using-flex/m-p/1758861#M13670</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-11-17T07:24:42Z</dc:date>
    </item>
  </channel>
</rss>