<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Yocto Image BLUEBOX 3.0 Error in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Yocto-Image-BLUEBOX-3-0-Error/m-p/1757545#M13653</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;We are getting the following error after following the given documentation from NXP while generating Yocto Image for LX2160ARDB-REV2 for Bluebox 3.0 .&lt;/P&gt;&lt;P&gt;(We are using the documentation under NDA)&lt;BR /&gt;Command:&lt;BR /&gt;user@1234:/Layerscape/build_lx2160ardb-rev2$ bitbake ls-image-lite&lt;BR /&gt;ERROR:Nothing PROVIDES 'ls-image-lite'&lt;/P&gt;&lt;P&gt;We can see the .bb file at location '/Layerscape/sources/meta-nxp-desktop/recipes-fsl/images/ls-image-lite.bb'&lt;BR /&gt;Could we get some help to resolve this??&lt;/P&gt;</description>
    <pubDate>Wed, 15 Nov 2023 10:11:05 GMT</pubDate>
    <dc:creator>AnanyaJamwal</dc:creator>
    <dc:date>2023-11-15T10:11:05Z</dc:date>
    <item>
      <title>Yocto Image BLUEBOX 3.0 Error</title>
      <link>https://community.nxp.com/t5/Layerscape/Yocto-Image-BLUEBOX-3-0-Error/m-p/1757545#M13653</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;We are getting the following error after following the given documentation from NXP while generating Yocto Image for LX2160ARDB-REV2 for Bluebox 3.0 .&lt;/P&gt;&lt;P&gt;(We are using the documentation under NDA)&lt;BR /&gt;Command:&lt;BR /&gt;user@1234:/Layerscape/build_lx2160ardb-rev2$ bitbake ls-image-lite&lt;BR /&gt;ERROR:Nothing PROVIDES 'ls-image-lite'&lt;/P&gt;&lt;P&gt;We can see the .bb file at location '/Layerscape/sources/meta-nxp-desktop/recipes-fsl/images/ls-image-lite.bb'&lt;BR /&gt;Could we get some help to resolve this??&lt;/P&gt;</description>
      <pubDate>Wed, 15 Nov 2023 10:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Yocto-Image-BLUEBOX-3-0-Error/m-p/1757545#M13653</guid>
      <dc:creator>AnanyaJamwal</dc:creator>
      <dc:date>2023-11-15T10:11:05Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Image BLUEBOX 3.0 Error</title>
      <link>https://community.nxp.com/t5/Layerscape/Yocto-Image-BLUEBOX-3-0-Error/m-p/1762925#M13687</link>
      <description>&lt;P&gt;If you are using documentation under NDA please open a new technical case to review it.&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 20:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Yocto-Image-BLUEBOX-3-0-Error/m-p/1762925#M13687</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2023-11-23T20:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: Yocto Image BLUEBOX 3.0 Error</title>
      <link>https://community.nxp.com/t5/Layerscape/Yocto-Image-BLUEBOX-3-0-Error/m-p/1786486#M13854</link>
      <description>&lt;P&gt;So I am running into the same problem now, with public documentation:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/LLDPUG_RevL6.1.22_2.0.0.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/LLDPUG_RevL6.1.22_2.0.0.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Following the instructions from chapter 4.5 leads to this problem.&amp;nbsp; I see why this is the case, i.e. the mentioned "meta-nxp-desktop" layer is not enabled by default.&amp;nbsp; Instead, the "setup-env" script suggests building "fsl-image-networking" or "fsl-image-networking-full".&lt;/P&gt;&lt;P&gt;So I manually enabled the layer and bitbake starts running, but fails with this error:&lt;/P&gt;&lt;P&gt;ERROR: ParseError at /media/dzu/hd01-xfs/nxp/yocto-sdk-6.1.22-2.0.0/sources/meta-nxp-desktop/recipes-graphics/libgpuperfcnt/libgpuperfcnt_6.4.11.p1.2.1d.bb:8: Could not inherit file classes/fsl-eula-unpack2.bbclass&lt;BR /&gt;ERROR: Parsing halted due to errors, see error messages above&lt;/P&gt;&lt;P&gt;So I believe there are multiple problems here that need fixing by NXP, correct?&lt;/P&gt;</description>
      <pubDate>Wed, 10 Jan 2024 21:35:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Yocto-Image-BLUEBOX-3-0-Error/m-p/1786486#M13854</guid>
      <dc:creator>laodzu</dc:creator>
      <dc:date>2024-01-10T21:35:02Z</dc:date>
    </item>
  </channel>
</rss>