<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Codewarrior TAP does not connect to target hardware under Ubuntu in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Codewarrior-TAP-does-not-connect-to-target-hardware-under-Ubuntu/m-p/1755089#M13618</link>
    <description>&lt;P&gt;My configuration:&lt;/P&gt;&lt;P&gt;Target: NXP LS1046ARDB&lt;/P&gt;&lt;P&gt;JTAG Probe: CodeWarrior TAP (USB)&lt;/P&gt;&lt;P&gt;Host PC: Ubuntu 22.04 with CodeWarrior Development Studio 11.5.12&lt;/P&gt;&lt;P&gt;I am not able to perform a target connection under Ubuntu. I attach one screenshot of the Connection Server and one of the Diagnostic Output. Both Ubuntu and CodeWarrior have been updated.&lt;/P&gt;&lt;P&gt;I made a test with the Windows version of the&amp;nbsp;CodeWarrior Development Studio and&amp;nbsp; the connection establishes without problems, so the hardware is working. Needless to say that I need to use Ubuntu so I need to find a solution&lt;/P&gt;</description>
    <pubDate>Thu, 09 Nov 2023 16:49:54 GMT</pubDate>
    <dc:creator>DaT63</dc:creator>
    <dc:date>2023-11-09T16:49:54Z</dc:date>
    <item>
      <title>Codewarrior TAP does not connect to target hardware under Ubuntu</title>
      <link>https://community.nxp.com/t5/Layerscape/Codewarrior-TAP-does-not-connect-to-target-hardware-under-Ubuntu/m-p/1755089#M13618</link>
      <description>&lt;P&gt;My configuration:&lt;/P&gt;&lt;P&gt;Target: NXP LS1046ARDB&lt;/P&gt;&lt;P&gt;JTAG Probe: CodeWarrior TAP (USB)&lt;/P&gt;&lt;P&gt;Host PC: Ubuntu 22.04 with CodeWarrior Development Studio 11.5.12&lt;/P&gt;&lt;P&gt;I am not able to perform a target connection under Ubuntu. I attach one screenshot of the Connection Server and one of the Diagnostic Output. Both Ubuntu and CodeWarrior have been updated.&lt;/P&gt;&lt;P&gt;I made a test with the Windows version of the&amp;nbsp;CodeWarrior Development Studio and&amp;nbsp; the connection establishes without problems, so the hardware is working. Needless to say that I need to use Ubuntu so I need to find a solution&lt;/P&gt;</description>
      <pubDate>Thu, 09 Nov 2023 16:49:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Codewarrior-TAP-does-not-connect-to-target-hardware-under-Ubuntu/m-p/1755089#M13618</guid>
      <dc:creator>DaT63</dc:creator>
      <dc:date>2023-11-09T16:49:54Z</dc:date>
    </item>
    <item>
      <title>Re: Codewarrior TAP does not connect to target hardware under Ubuntu</title>
      <link>https://community.nxp.com/t5/Layerscape/Codewarrior-TAP-does-not-connect-to-target-hardware-under-Ubuntu/m-p/1757972#M13660</link>
      <description>&lt;P&gt;There are some issues regarding CWTAP under Ubuntu,&amp;nbsp;&lt;SPAN&gt;Please refer to the attached workaround and let me know if it works on your side.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 16 Nov 2023 01:58:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Codewarrior-TAP-does-not-connect-to-target-hardware-under-Ubuntu/m-p/1757972#M13660</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2023-11-16T01:58:25Z</dc:date>
    </item>
  </channel>
</rss>