<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1028A  RDB USB interface</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028A-RDB-USB-interface/m-p/1748642#M13562</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218921"&gt;@mkraj&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Please refer to Table 32 in the AN12028 for pin termination details if the USB interface is unused.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
    <pubDate>Mon, 30 Oct 2023 10:22:53 GMT</pubDate>
    <dc:creator>mrudangshelat-13</dc:creator>
    <dc:date>2023-10-30T10:22:53Z</dc:date>
    <item>
      <title>LS1028A  RDB USB interface</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-RDB-USB-interface/m-p/1747873#M13554</link>
      <description>&lt;P&gt;Dear Expert&lt;/P&gt;&lt;P&gt;We are doing USB interface modifications of LS1028A RDB by connecting both usb3.0 interfaces to the M.2 connecctors for connecting 4g modem and we are not using any USB connector.&lt;/P&gt;&lt;P&gt;we are not using below usb interface pins&lt;/P&gt;&lt;P&gt;1. R_USB1_VBUS- not using&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;USB1_ID -connecting to ground with 1K&lt;/P&gt;&lt;P&gt;3.USB_DRVVBUS-not using&lt;/P&gt;&lt;P&gt;4.USB_PWRFAULT-not using&lt;/P&gt;&lt;P&gt;5.USB2_VBUS-not using&lt;/P&gt;&lt;P&gt;6.&amp;nbsp;USB2_ID-connecting to ground with 1K&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it ok? Please comment.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;P&gt;With Regards&lt;/P&gt;&lt;P&gt;Krishnam Raju M&lt;/P&gt;</description>
      <pubDate>Fri, 27 Oct 2023 13:00:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-RDB-USB-interface/m-p/1747873#M13554</guid>
      <dc:creator>mkraj</dc:creator>
      <dc:date>2023-10-27T13:00:24Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A  RDB USB interface</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028A-RDB-USB-interface/m-p/1748642#M13562</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/218921"&gt;@mkraj&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Please refer to Table 32 in the AN12028 for pin termination details if the USB interface is unused.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Mon, 30 Oct 2023 10:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028A-RDB-USB-interface/m-p/1748642#M13562</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-10-30T10:22:53Z</dc:date>
    </item>
  </channel>
</rss>