<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Building QorIQ Linux SDK 2.0 for LS2085ARDB in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544018#M1355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , &lt;/P&gt;&lt;P&gt;I intend to develop a high performance user space packet processing application using DPAA2.&lt;/P&gt;&lt;P&gt;ls2080 doesn't have AIOP, if sdk is built for ls2080ardb, would I be able to use AIOP of ls2085A SoC?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Swati&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jul 2016 12:47:23 GMT</pubDate>
    <dc:creator>swatideshpande</dc:creator>
    <dc:date>2016-07-28T12:47:23Z</dc:date>
    <item>
      <title>Building QorIQ Linux SDK 2.0 for LS2085ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544015#M1352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I would like to build QorIQ Linux SDK&amp;nbsp; 2.0 for LS2085ARDB. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Installed below sdks.&lt;/P&gt;&lt;P&gt;QorIQ Linux SDK v2.0 AARCH64 Yocto Cache.iso&lt;/P&gt;&lt;P&gt;QorIQ Linux SDK v2.0 SOURCE.iso&lt;/P&gt;&lt;P&gt; and ran . /fsl-setup-env -h and observe that only below platforms are supported&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Supported machines:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; b4420qds-64b b4420qds b4860qds-64b b4860qds c293pcie ls1021atwr ls1043aqds ls1043ardb ls2080ardb p2041rdb p3041ds p4080ds p5020ds-64b p5020ds p5040ds-64b p5040ds t1023rdb-64b t1023rdb t1024rdb-64b t1024rdb t1040d4rdb-64b t1040d4rdb t1042d4rdb-64b t1042d4rdb t2080qds-64b t2080qds t2080rdb-64b t2080rdb t4160qds-64b t4160qds t4240qds-64b t4240qds t4240rdb-64b t4240rdb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you Please let me know what target should I use to build image for LS2085ARDB ? Am I using the right sdk?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Swati&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 09:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544015#M1352</guid>
      <dc:creator>swatideshpande</dc:creator>
      <dc:date>2016-07-27T09:31:30Z</dc:date>
    </item>
    <item>
      <title>Re: Building QorIQ Linux SDK 2.0 for LS2085ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544016#M1353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You should use ls2080ardb as target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 09:36:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544016#M1353</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-07-27T09:36:47Z</dc:date>
    </item>
    <item>
      <title>Re: Building QorIQ Linux SDK 2.0 for LS2085ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544017#M1354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the quick answer Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jul 2016 14:25:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544017#M1354</guid>
      <dc:creator>swatideshpande</dc:creator>
      <dc:date>2016-07-27T14:25:47Z</dc:date>
    </item>
    <item>
      <title>Re: Building QorIQ Linux SDK 2.0 for LS2085ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544018#M1355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi , &lt;/P&gt;&lt;P&gt;I intend to develop a high performance user space packet processing application using DPAA2.&lt;/P&gt;&lt;P&gt;ls2080 doesn't have AIOP, if sdk is built for ls2080ardb, would I be able to use AIOP of ls2085A SoC?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Swati&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 12:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544018#M1355</guid>
      <dc:creator>swatideshpande</dc:creator>
      <dc:date>2016-07-28T12:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: Building QorIQ Linux SDK 2.0 for LS2085ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544019#M1356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LS2080a is the same as LS2085a, but without AIOP. Please contact a NXP FAE, to get the sdk for LS2085. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jul 2016 13:07:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Building-QorIQ-Linux-SDK-2-0-for-LS2085ARDB/m-p/544019#M1356</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2016-07-28T13:07:00Z</dc:date>
    </item>
  </channel>
</rss>