<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS2085A Console is not coming</title>
    <link>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393311#M135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anandha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you say : "Everything is fine except the console&lt;/P&gt;&lt;P&gt;prints are not coming,, i have checked the uart cables&lt;/P&gt;&lt;P&gt;also.. even probed the signals too.. it is fine"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mean you know u-boot is working fine but&lt;/P&gt;&lt;P&gt;just nothing is coming to your terminal connection ?&lt;/P&gt;&lt;P&gt;If you are not sure that u-boot is running properly&lt;/P&gt;&lt;P&gt;use your JTAG debugger and RESET HALT first to&lt;/P&gt;&lt;P&gt;see if you can properly come out of reset then&lt;/P&gt;&lt;P&gt;single step couple times to make sure u-boot is&lt;/P&gt;&lt;P&gt;being executed at the correct address.&lt;/P&gt;&lt;P&gt;Also, you mentioned you probed the signals,&lt;/P&gt;&lt;P&gt;do you see activity on the uart pins when you&lt;/P&gt;&lt;P&gt;watch them with a scope ? If this is the case then&lt;/P&gt;&lt;P&gt;there might be a problem in your terminal program&lt;/P&gt;&lt;P&gt;settings (baud rate, flow control etc). Just make sure&lt;/P&gt;&lt;P&gt;your board is coming out of reset properly by halting&lt;/P&gt;&lt;P&gt;early on using your JTAG debugger. Perhaps you &lt;/P&gt;&lt;P&gt;can also stop at a later point and check the register&lt;/P&gt;&lt;P&gt;contents for serial port.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2015 14:48:50 GMT</pubDate>
    <dc:creator>sinanakman</dc:creator>
    <dc:date>2015-07-29T14:48:50Z</dc:date>
    <item>
      <title>LS2085A Console is not coming</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393308#M132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using LS2085A QDS board, board is booting properly but it is not giving the console prints. I have flashed all the necessary default images in the NOR flash using JTAG in the corresponding partition. All the settings are fine. FPGA and all clock initialization are fine. We have confirmed this using the corresponding LED in the board, any clues what might went wrong. ????&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: Everything is fine except the console prints are not coming,, i have checked the uart cables also.. even probed the signals too.. it is fine,, but why the console is not coming ??iif&lt;/P&gt;&lt;P&gt;Please let me know if anybody faced similar kind of problem ??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 13:18:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393308#M132</guid>
      <dc:creator>anandhakumarm</dc:creator>
      <dc:date>2015-07-29T13:18:07Z</dc:date>
    </item>
    <item>
      <title>Re: LS2085A Console is not coming</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393309#M133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check if you're using the correct UART port, UART cable and if the RCW is located at 0x0 offset and u-boot at 0x0010_0000 offset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 13:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393309#M133</guid>
      <dc:creator>marius_grigoras</dc:creator>
      <dc:date>2015-07-29T13:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: LS2085A Console is not coming</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393310#M134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marius,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;yes, im using the correct UART port, UART cable is fine, RCW and Uboot also placed in the correct offset..&amp;nbsp; Still the problem persists..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 14:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393310#M134</guid>
      <dc:creator>anandhakumarm</dc:creator>
      <dc:date>2015-07-29T14:22:37Z</dc:date>
    </item>
    <item>
      <title>Re: LS2085A Console is not coming</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393311#M135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Anandha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you say : "Everything is fine except the console&lt;/P&gt;&lt;P&gt;prints are not coming,, i have checked the uart cables&lt;/P&gt;&lt;P&gt;also.. even probed the signals too.. it is fine"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mean you know u-boot is working fine but&lt;/P&gt;&lt;P&gt;just nothing is coming to your terminal connection ?&lt;/P&gt;&lt;P&gt;If you are not sure that u-boot is running properly&lt;/P&gt;&lt;P&gt;use your JTAG debugger and RESET HALT first to&lt;/P&gt;&lt;P&gt;see if you can properly come out of reset then&lt;/P&gt;&lt;P&gt;single step couple times to make sure u-boot is&lt;/P&gt;&lt;P&gt;being executed at the correct address.&lt;/P&gt;&lt;P&gt;Also, you mentioned you probed the signals,&lt;/P&gt;&lt;P&gt;do you see activity on the uart pins when you&lt;/P&gt;&lt;P&gt;watch them with a scope ? If this is the case then&lt;/P&gt;&lt;P&gt;there might be a problem in your terminal program&lt;/P&gt;&lt;P&gt;settings (baud rate, flow control etc). Just make sure&lt;/P&gt;&lt;P&gt;your board is coming out of reset properly by halting&lt;/P&gt;&lt;P&gt;early on using your JTAG debugger. Perhaps you &lt;/P&gt;&lt;P&gt;can also stop at a later point and check the register&lt;/P&gt;&lt;P&gt;contents for serial port.&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sinan Akman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 14:48:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393311#M135</guid>
      <dc:creator>sinanakman</dc:creator>
      <dc:date>2015-07-29T14:48:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS2085A Console is not coming</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393312#M136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sinan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your valuable reply man.. Actually it is coming out of reset sequence... that is why we are getting the blue LED ON.. that indicates Successful FPGA initialization; correct processor orientation and all on-board voltage is in good condition;&amp;nbsp; All reset configuration and sequencer passed.. Also i can able to see the uart activity in scope, that is also fine.. Uboot is also fine,, terminal minicom settings also following the standards (baud rate 115200, no flow contrl)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Still the problem remains..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 09:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393312#M136</guid>
      <dc:creator>anandhakumarm</dc:creator>
      <dc:date>2015-07-30T09:03:25Z</dc:date>
    </item>
    <item>
      <title>Re: LS2085A Console is not coming</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393313#M137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, if you see UART activity by scope, why do you think console output is not coming? Have you tried to another PC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 15:11:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2085A-Console-is-not-coming/m-p/393313#M137</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2015-07-30T15:11:53Z</dc:date>
    </item>
  </channel>
</rss>