<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックOTPMK fusing on Freeway LS1046ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1734888#M13437</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I want to know what are the additional steps that need to be performed for fuse programming on Freeway LS1046ARDB board.&lt;/P&gt;&lt;P&gt;The Freeway manual doesn't seem to include any instructions regarding jumper settings to connect 1.8V for fuse programming. Instead, it mentions the use of GPIO for this purpose. I have a couple of questions:&lt;/P&gt;&lt;P&gt;i) To program fuses on the Freeway LS1046, is it necessary to manually short anything, or is configuring the GPIOs sufficient?&lt;/P&gt;&lt;P&gt;ii) If GPIOs are involved, should the direction of GPIOs be set as input or output?&lt;/P&gt;&lt;P&gt;I would greatly appreciate it if someone could provide me with &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;the steps to carry out fuse programming on the Freeway Board. Because Fusing on LS1046ARDB and fusing on Freeway LS1046ARDB seems to be different.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Faizan&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 06 Oct 2023 14:12:09 GMT</pubDate>
    <dc:creator>Faizanbaig</dc:creator>
    <dc:date>2023-10-06T14:12:09Z</dc:date>
    <item>
      <title>OTPMK fusing on Freeway LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1734888#M13437</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I want to know what are the additional steps that need to be performed for fuse programming on Freeway LS1046ARDB board.&lt;/P&gt;&lt;P&gt;The Freeway manual doesn't seem to include any instructions regarding jumper settings to connect 1.8V for fuse programming. Instead, it mentions the use of GPIO for this purpose. I have a couple of questions:&lt;/P&gt;&lt;P&gt;i) To program fuses on the Freeway LS1046, is it necessary to manually short anything, or is configuring the GPIOs sufficient?&lt;/P&gt;&lt;P&gt;ii) If GPIOs are involved, should the direction of GPIOs be set as input or output?&lt;/P&gt;&lt;P&gt;I would greatly appreciate it if someone could provide me with &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;the steps to carry out fuse programming on the Freeway Board. Because Fusing on LS1046ARDB and fusing on Freeway LS1046ARDB seems to be different.&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Faizan&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Oct 2023 14:12:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1734888#M13437</guid>
      <dc:creator>Faizanbaig</dc:creator>
      <dc:date>2023-10-06T14:12:09Z</dc:date>
    </item>
    <item>
      <title>Re: OTPMK fusing on Freeway LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1736010#M13450</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;As seen in board's reference manual:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Connects to the 1x2 PROG_SFP header (J74). The GPIO_FUSE_PROG signal controls the power supply to the TA_PROG_SFP pin of the processor:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;• When GPIO_FUSE_PROG is low, power to TA_PROG_SFP pin is 1.8 V (fuse programming enable)&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;LI-WRAPPER&gt;&lt;SPAN class="fontstyle0"&gt;• When GPIO_FUSE_PROG is high, power to TA_PROG_SFP pin is 0 V (fuse programming disable) (default value)&lt;/SPAN&gt; &lt;BR style="font-style: normal; font-variant: normal; font-weight: normal; letter-spacing: normal; line-height: normal; orphans: 2; text-align: -webkit-auto; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-size-adjust: auto; -webkit-text-stroke-width: 0px;" /&gt;&lt;/LI-WRAPPER&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;I've seen that they're either one or another, please check the schematic, you can use GPIO to saturate the transistor or directly short with the NP J74.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="josephlinares_0-1696880807371.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244158i09D3D78ADC55AB82/image-size/large?v=v2&amp;amp;px=999" role="button" title="josephlinares_0-1696880807371.png" alt="josephlinares_0-1696880807371.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;josephlinares_0-1696880807371.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;If you want to use GPIO, you should probably need a workaround, I'd request your board revision to check on that.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 09 Oct 2023 19:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1736010#M13450</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-10-09T19:47:40Z</dc:date>
    </item>
    <item>
      <title>Re: OTPMK fusing on Freeway LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1736725#M13457</link>
      <description>Hi,&lt;BR /&gt;Thanks for the response.&lt;BR /&gt;But I am still in confusion. I would like you to provide me clarity on whether the steps/process for Fuse programming same for LS1046ARDB and Freeway LS1046A or is it different?&lt;BR /&gt;If Different what is it ? What are the detailed steps to be followed?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Faizan</description>
      <pubDate>Tue, 10 Oct 2023 16:40:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1736725#M13457</guid>
      <dc:creator>Faizanbaig</dc:creator>
      <dc:date>2023-10-10T16:40:31Z</dc:date>
    </item>
    <item>
      <title>Re: OTPMK fusing on Freeway LS1046ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1737860#M13466</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Sure thing, as the fuses are inside the chip we'd expect that the fuses are burnt in the same way but there should be another way to enable POVDD, for everything else, I'm attaching a presentation based on LS1043A RDB that solves almost every question in implementing secure boot; you'll see is also another way to enable POVDD.&lt;/P&gt;
&lt;P&gt;Regarding that, let's refer to &lt;A href="https://www.nxp.com/docs/en/user-guide/LLDPUG_RevL6.1.22_2.0.0.pdf" target="_self"&gt;latest LDP release&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;For LS1043ARDB in&amp;nbsp;6.1.1.5.2.1 is told:&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Put J13 to enable PWR_PROG_SFP&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;J13 is a 2x2 jumper that connects 1.8V to TA_PROG_SFP.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;For LS1046ARDB:&lt;/SPAN&gt;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt; Put J21 to enable PWR_PROG_SFP &lt;BR style="font-style: normal; font-variant: normal; font-weight: normal; letter-spacing: normal; line-height: normal; orphans: 2; text-align: -webkit-auto; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-size-adjust: auto; -webkit-text-stroke-width: 0px;" /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;J21 is a 2x2 jumper that connects 1.8V to TA_PROG_SFP.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;For FRWY LS1046A REV B is missing, but in schematics is a NP 1x2 header &lt;STRONG&gt;J74&lt;/STRONG&gt; that can short OVDD to TA_PROG_SFP pin, it's &lt;STRONG&gt;ored&lt;/STRONG&gt; with a MOSFET that can be triggered with a GPIO as FRWY LS1046A Reference Manual States.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="josephlinares_0-1697051275971.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/244594i471D1E59BC3EE928/image-size/medium?v=v2&amp;amp;px=400" role="button" title="josephlinares_0-1697051275971.png" alt="josephlinares_0-1697051275971.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;josephlinares_0-1697051275971.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;So for slide 45 I think you can populate J74 or create this situation:&lt;/SPAN&gt;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt; GPIO_FUSE_PROG is High, Q3 is ON= PROG_SFP=1.8V {Fuse programming Enable} &lt;BR style="font-style: normal; font-variant: normal; font-weight: normal; letter-spacing: normal; line-height: normal; orphans: 2; text-align: -webkit-auto; text-indent: 0px; text-transform: none; white-space: normal; widows: 2; word-spacing: 0px; -webkit-text-size-adjust: auto; -webkit-text-stroke-width: 0px;" /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN class="fontstyle0"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 19:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/OTPMK-fusing-on-Freeway-LS1046ARDB/m-p/1737860#M13466</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2023-10-11T19:11:09Z</dc:date>
    </item>
  </channel>
</rss>