<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1012A LSDK 21.08 boot failed. in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1733687#M13431</link>
    <description>&lt;P&gt;Hi&amp;nbsp;Oswalag,&lt;/P&gt;&lt;P&gt;I am currently conducting a boot test using an SD card after QSPI Flash.&lt;BR /&gt;The system is displaying the message mentioned above during the SD card boot process and then freezing.&lt;/P&gt;&lt;P&gt;I successfully booted the system by copying the ls1012afrwy_boot.scr file generated in LSDK 18.12 to the SD card boot partition, instead of using the lsdk 21.08 generated file.&lt;/P&gt;&lt;P&gt;Why isn't it working when I try to use the scr file generated in LSDK 21.08?&lt;/P&gt;&lt;P&gt;Thank you.&lt;BR /&gt;Best Regards,&lt;BR /&gt;Gyosun.&lt;/P&gt;</description>
    <pubDate>Wed, 04 Oct 2023 11:01:21 GMT</pubDate>
    <dc:creator>Gyosun</dc:creator>
    <dc:date>2023-10-04T11:01:21Z</dc:date>
    <item>
      <title>LS1012A LSDK 21.08 boot failed.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1729792#M13388</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are porting LSDK 21.08 to a custom board similar to ls1012afrwy.&lt;BR /&gt;The SD card was made as follows.&lt;/P&gt;&lt;P&gt;flex-installer -i auto -m ls1012afrwy -d /dev/sdc -r rootfs_lsdk2108_buildroot_devel_arm64.tgz -b boot_LS_arm64_lts_5.10.tgz -p 3P=100M:2G:-1&lt;/P&gt;&lt;P&gt;It seems that the rootfs mount is not working properly during booting.&lt;/P&gt;&lt;P&gt;&lt;A href="https://drive.google.com/file/d/12Nw3fHoyluaPnK9L3DaD9B0UPRvBlBpN/view?usp=sharing" target="_self"&gt;LSDK2108_boot_fail.txt&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need help urgently.&lt;/P&gt;&lt;P&gt;Thank you,&lt;BR /&gt;Best Regards.&lt;BR /&gt;Gyosun.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Sep 2023 14:08:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1729792#M13388</guid>
      <dc:creator>Gyosun</dc:creator>
      <dc:date>2023-09-26T14:08:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A LSDK 21.08 boot failed.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1730776#M13405</link>
      <description>&lt;P&gt;ls1012a cannot boot from SD card, you can boot from qspi flash.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 21:01:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1730776#M13405</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2023-09-27T21:01:22Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A LSDK 21.08 boot failed.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1733687#M13431</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Oswalag,&lt;/P&gt;&lt;P&gt;I am currently conducting a boot test using an SD card after QSPI Flash.&lt;BR /&gt;The system is displaying the message mentioned above during the SD card boot process and then freezing.&lt;/P&gt;&lt;P&gt;I successfully booted the system by copying the ls1012afrwy_boot.scr file generated in LSDK 18.12 to the SD card boot partition, instead of using the lsdk 21.08 generated file.&lt;/P&gt;&lt;P&gt;Why isn't it working when I try to use the scr file generated in LSDK 21.08?&lt;/P&gt;&lt;P&gt;Thank you.&lt;BR /&gt;Best Regards,&lt;BR /&gt;Gyosun.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Oct 2023 11:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1733687#M13431</guid>
      <dc:creator>Gyosun</dc:creator>
      <dc:date>2023-10-04T11:01:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A LSDK 21.08 boot failed.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1734399#M13436</link>
      <description>&lt;P&gt;Take a look on the flash layout, you cannot boot from sd&amp;nbsp; (ls1012), you can use the SD card to deploy only the linux image and ubuntu userland (if it is the case).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Oswalag_0-1696530653134.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/243723i5B11D9F984B775E8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Oswalag_0-1696530653134.png" alt="Oswalag_0-1696530653134.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Oswalag_0-1696530653134.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Oct 2023 18:36:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-LSDK-21-08-boot-failed/m-p/1734399#M13436</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2023-10-05T18:36:35Z</dc:date>
    </item>
  </channel>
</rss>