<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1043ARDB_PD evaluation board  IFC  interface to 16 bit NOR FLASH</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-evaluation-board-IFC-interface-to-16-bit-NOR-FLASH/m-p/1731216#M13416</link>
    <description>&lt;P&gt;&lt;EM&gt;In&amp;nbsp; LS1043A RDB-PD , 16 Bit NOR FLASH is connected to IFC interface of LS1043A.&amp;nbsp; &amp;nbsp;As per this&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;IFC_ADDR[1:15] is connected to A[25:11] of NOR FLASH&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;IFC_ADDR[16:26] is connected to A[10: 0] of&amp;nbsp; NOR FLASH&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;But as per LS1043ARM&amp;nbsp; Fig:25-9, IFC_AD0&amp;nbsp; after address decoding should get connect to A25 address line of NOR FLASH. I&lt;/EM&gt;&lt;EM&gt;&amp;nbsp;am confusing while co-relating&amp;nbsp;LS1043ARM&amp;nbsp; Fig:25-9 with 16 Bit NOR FLASH&amp;nbsp; connectivity in&amp;nbsp;LS1043A RDB-PD evaluation board. Please clarify.&lt;/EM&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 28 Sep 2023 10:22:30 GMT</pubDate>
    <dc:creator>Pamid</dc:creator>
    <dc:date>2023-09-28T10:22:30Z</dc:date>
    <item>
      <title>LS1043ARDB_PD evaluation board  IFC  interface to 16 bit NOR FLASH</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-evaluation-board-IFC-interface-to-16-bit-NOR-FLASH/m-p/1731216#M13416</link>
      <description>&lt;P&gt;&lt;EM&gt;In&amp;nbsp; LS1043A RDB-PD , 16 Bit NOR FLASH is connected to IFC interface of LS1043A.&amp;nbsp; &amp;nbsp;As per this&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;IFC_ADDR[1:15] is connected to A[25:11] of NOR FLASH&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;IFC_ADDR[16:26] is connected to A[10: 0] of&amp;nbsp; NOR FLASH&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;But as per LS1043ARM&amp;nbsp; Fig:25-9, IFC_AD0&amp;nbsp; after address decoding should get connect to A25 address line of NOR FLASH. I&lt;/EM&gt;&lt;EM&gt;&amp;nbsp;am confusing while co-relating&amp;nbsp;LS1043ARM&amp;nbsp; Fig:25-9 with 16 Bit NOR FLASH&amp;nbsp; connectivity in&amp;nbsp;LS1043A RDB-PD evaluation board. Please clarify.&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 10:22:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043ARDB-PD-evaluation-board-IFC-interface-to-16-bit-NOR-FLASH/m-p/1731216#M13416</guid>
      <dc:creator>Pamid</dc:creator>
      <dc:date>2023-09-28T10:22:30Z</dc:date>
    </item>
  </channel>
</rss>