<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ls1043a  interface with 16bit NOR FLASH dual die in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1043a-interface-with-16bit-NOR-FLASH-dual-die/m-p/1731069#M13409</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/47848"&gt;@Pamid&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Please refer to section#&amp;nbsp;25.4.1.2.1 mentioned in the LS1043ARM for the connection details.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
    <pubDate>Thu, 28 Sep 2023 06:53:03 GMT</pubDate>
    <dc:creator>mrudangshelat-13</dc:creator>
    <dc:date>2023-09-28T06:53:03Z</dc:date>
    <item>
      <title>ls1043a  interface with 16bit NOR FLASH dual die</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1043a-interface-with-16bit-NOR-FLASH-dual-die/m-p/1730981#M13406</link>
      <description>&lt;P&gt;We want to use LS1043A in our application with 16 Bit NOR FLASH 256MB (MT28FW02GBBA1HPC). NORFLASH is a dual die device. In this regard &amp;nbsp;how address and data bus will be connected&amp;nbsp; from LS1043A to NORFLASH&amp;nbsp; using&amp;nbsp; mode 0 pin muxing.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 05:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1043a-interface-with-16bit-NOR-FLASH-dual-die/m-p/1730981#M13406</guid>
      <dc:creator>Pamid</dc:creator>
      <dc:date>2023-09-28T05:07:45Z</dc:date>
    </item>
    <item>
      <title>Re: ls1043a  interface with 16bit NOR FLASH dual die</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1043a-interface-with-16bit-NOR-FLASH-dual-die/m-p/1731069#M13409</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/47848"&gt;@Pamid&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Please refer to section#&amp;nbsp;25.4.1.2.1 mentioned in the LS1043ARM for the connection details.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 06:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1043a-interface-with-16bit-NOR-FLASH-dual-die/m-p/1731069#M13409</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-09-28T06:53:03Z</dc:date>
    </item>
  </channel>
</rss>